Sealing Shielding

3 Advantages of a Double Chamfer Radial Seal

Radial Male and Female Rubber SealMore often than not, an O-ring makes for a great sealing element. They seal over a wide range of pressure, temperature and tolerance. Normally they require very little room, are readily available, and easily sourced. However, there are specific applications that may be better suited for an alternate type of seal, such as a double chamfer radial seal. 

First, let’s clarify what exactly a radial seal is. Radial implies the seal is being compressed from inside to outside. Sometimes this type of sealing is called inner or outer sealing. It may also be called a rod or female seal, or a piston or male seal.

In essence, a radial seal is placed in a groove either around a piston, or in a groove inside a bore. Double chamfer radial seals will fit in both a male groove, around a piston, or in a female groove (inside a bore). 

Unlike an O-ring, the cross section of the double chamfer radial seal has two flat sealing surfaces, and opposite of the groove, they are angled for easier installation.

 

3 Advantages of a Double Chamfer Radial Seal_Male&FemaleDC_Parker O-Ring & Engineered Seals Division

 

Advantages of double chamfer radial seals:

1. When the O-ring fails by spiraling in a reciprocating application or during installation, the double chamfer seal is a good alternative. The wide, flat base of the double chamfer makes it resistant to rolling, and therefore, a solution for O-ring spiral failure. The FEA below demonstrates the O-ring rolling in a gland. 

O-ring FEA of seal rolling in groove

 

2. High pressure or large clearance gap applications can result in an extruded O-ring. A common solution is to add a back-up ring as a support to the O-ring. The back-up ring is a great solution, however this can add complexity in several ways. One, it adds another item to the bill of materials. Second, the back-up can be difficult to install, resulting in damage. Finally if the back-up is forgotten or incorrectly assembled during installation, the O-ring will leak. A high pressure high temperature double chamfer radial seal replaces the O-ring and back-up combination with a single sealing solution. In addition, known issues with scarf cut back-up rings are the chance of the angled edge damaging the O-ring. By eliminating the scarfed back-up, we are eliminating a possible failure mode. 

 

3. A third advantage has to do with available groove space on the hardware. Standard O-rings require a specific groove depth and width, which can be difficult in tight locations or with limited hardware space. Since double chamfer radial seals are easily customized, they can be designed for a more shallow groove, and seal just as well as an O-ring. Double chamfer radial seals are easily customized in both size and material for most any application. For example, since the product is extruded rather than molded, the custom sizes will likely not need a costly mold and instead, use existing extrusion tooling configured for the desired size. And since the double chamfer radial seal is extruded rather than molded, there is no parting line on the finished product. This can be an advantage for gaseous or vacuum applications when even the smallest change in sealing surface finish will create a leak path.

 

Another feature of the double chamfer radial seal is the ability to color code the outer diameter (O.D.) or inner diameter (I.D.) for visibility of proper installation. This helps operators to easily see the seal is installed, which can be beneficial when a black O-ring is in a black housing. Double chamfer radial seals can have an inner diameter as small as .500” or have an outer diameter as large as 18” which means most every groove can retrofit from an O-ring. The seal height, also called wall, and width, also called cut, can also be adjusted.

To learn more about sizing a double chamfer radial seal for your application, download our Radial Seal Design Guide , speak to one of our Applications Engineers at 859-335-5101, or chat with us online via our website.

 

 

A Simple Guide to Radial Seals | Sealing Fundamentals

How to Enhance Performance and Safety of Static Radial Seals

Avoid Seal Extrusion with a Robust Gland Design

 

 

This article was contributed by:

Dorothy Kern, Applications Engineer Lead, Parker O-Ring Division

Dorothy Kern, applications engineer lead, O-Ring & Engineered Seals Division

Have a question about Parker products or services? We can help: Contact Us!

Comments for 3 Advantages of a Double Chamfer Radial Seal


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha