Sealing Shielding

3 Guidelines to Ensure Proper Seal Installation

Parker O-Lube, Parker Super O-LubeIncorrect O-ring installation can lead to assembly damage causing leakage during the first pressure test. If the system does not pressurize properly, the entire piece of equipment should be disassembled and seals must be replaced. Depending on when this test occurs, multiple manufacturing steps could be in between the seal installation and the first step where leakage can be identified. If O-ring damage happens with high frequency, you could be wasting time and money on seal replacement. Luckily, there are some easy steps that can be followed to help prevent this from occurring. Parker’s recommended guidelines for installation include always using lubrication, good gland design, and ensuring correct sizing.

Lubrication makes installation easier

Using lubrication is an essential facet of proper installation. Lubrication reduces surface friction between the O-ring and mating surfaces, allowing the O-ring to seat in the groove with very little difficulty. In male and female radial seals, lubrication will reduce installation force and create a smooth transition as the piston is inserted in the bore. 

Choosing the proper lubricant requires careful consideration of your system. You must ensure the lubricant choice is compatible with the O-ring material being used, suitable for the temperature range of the application, compatible with the system fluids, capable of producing a high surface tension film, and does not clog system filters. 

Parker offers two lubricants, O-Lube and Super-O-Lube. The O-Lube is an outstanding general-purpose grease intended for O-ring and elastomer seal types used in hydrocarbon service. O-Lube has a recommended service temperature of -20°F to 180°F (-29°C to 82°C). On the other hand, Super-O-Lube is an ideal all-purpose O-ring lubricant. Rather than a grease, the Super-O-Lube is a high viscosity silicone oil. It is an extremely effective seal lubricant, useful from -65°F to 400°F (-54°C to 204°C). 

For more information on Parker O-Lube and Super-O-Lube and how to choose a lubricant, refer to section 3 of the O-Ring Handbook

Good design principles

chamfers for lubricantOne of the easiest ways to ensure care-free installation is by following good design practice as recommended in the Parker O-Ring Handbook. The dimensions listed in the O-Ring Handbook put good compression on the O-ring while preventing the groove from exceeding 100% fill. In radial seal applications Parker recommends using a lead in chamfer at an angle of 15-20 degrees with an opening which exceeds the maximum height of the O-ring in the groove. 

Want to know more about installation of specific groove types?  Parker has produced easy to follow videos showing how to install O-rings in dovetail grooves, face seals, and male and female radial seals. 

 

sizing cone, sizing tapeProper sizing is key

Putting the wrong sized O-ring into an application can also lead to damage, making it important to verify O-ring sizing to ensure the right O-ring was selected. Unfortunately, measuring O-rings in the field or in a warehouse is not easily done without the proper tools. Parker offers a unique solution to this problem by offering measuring cones and circumference “Pi” tape to help provide quick and easy O-ring sizing information. These tools will help ensure that the proper Parker standard size is chosen during assembly.

Applications help for further assistance

By following the above recommendations you can be at ease during manufacturing your product. If you do encounter issues during your assembly that fall outside our recommendations, Parker can help troubleshoot your situation. Parker O-Ring Division application engineers can assist with your particular application. Our engineers can be reached a variety of ways, via telephone, email, and even online chat. With this additional help you can be sure that you will find success using Parker O-Rings. 

 

How to Avoid Critical Component Failure in the Oil & Gas Industry - Eric Uehlein Parker Hannifin O-Ring Division

 

 

This article was contributed by Eric Uehlein, Applications Engineer, Parker Hannifin O-Ring Division

 

 

 

Be sure to check out our video demonstrating the various ways to apply Parker lubricants in your applications.

 

Related content:

How to Lubricate an O-Ring 

Proper Installation of an O-Ring: Standard Male Gland

Proper Installation of an O-Ring: Standard Female Gland

Proper Installation of an O-Ring: Face Seal Gland

Proper Installation of an O-Ring: Full and Half Dovetails

 

 

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for 3 Guidelines to Ensure Proper Seal Installation

parker o ring lube
The O-Lube is an outstanding general-purpose grease intended for O-ring and elastomer seal types used in hydrocarbon service.
parker o ring lube
making it important to verify O-ring sizing to ensure the right O-ring was selected. Unfortunately, measuring O-rings in the field or in a warehouse is not easily done without the proper tools.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha