Pneumatics

3 Things to Consider for Machine Tools and IIoT

3 Things to Consider for Machine Tools and IoTAs Industry 4.0 and the Industrial Internet of Things (IIoT) continue to grow and evolve, they promise numerous benefits for a leaner enterprise. In the realm of machine tools, the IIoT can certainly offer chances for improvements in monitoring and maintenance. There are, however, some concerns that must be addressed before this becomes a reality.
 

1. The need for more “smart” devices and machine components that communicate with each other and the factory

Machine tool manufacturers seek to use such components to make their products more reliable and productive, without increasing initial machine cost. This situation is driving a trend of increased cooperation between end users, machine design engineers and their engineering partners in electro-mechanical and pneumatic motion components. 

The end goal is to offer useful information to factory managers who can act on the data that machines collect. Considering this, all partners must work together to set up effective IIoT-capable systems. End users know what information they need for their businesses. Machine designers know the unique concerns and opportunities present in a particular application. Automation component suppliers know how to get data from edge devices to factory software and the internet. Together these engineers can create systems that help factories achieve a leaner, more automated business.

These alliances work to find automation solutions that cost-effectively incorporate better connectivity, control, and intelligence into machine tools. Engineering partners can make sure that all collected data is accurate and that it represents important parameters relevant in the real world. They can specify which components to use and which communications protocols make sense for a given application.

 

3 Things to Consider for Machine Tools and IIoT - IO-Link Image - Pneumatic DivisionTake, for example, a pneumatic tool used to grasp blank parts and load them into position on a cutting machine. Its pneumatic valves are controlled by solenoids, and the voltage of the coils can be monitored for signs of impending failure. To make this data actionable, machine designers need a means of acquiring that information. Open-standard protocols such as IO Link provide affordable serial communication with low-level edge devices, connecting them to motion controllers which in turn connect to the factory network and, if desired, to an internet gateway. Motion component manufacturers are starting to offer IO Link modules for their pneumatic valves, providing an easily integrated, cost-effective solution.

 

2. IIoT goes beyond merely connecting together sensors and factory management software

Rather, it is an approach that allows the collection and effective interpretation of data. So far, the status quo in industrial equipment and machine tools has been to monitor one or two aspects of a system, such as position or speed. However, tracking the number of cycles could supply business managers with data that is important for measuring production, service life and total cost of ownership. 

Other parameters such as thermal warning may allow engineers to spot when equipment is not operating correctly or as efficiently as it could. Managers can then schedule maintenance predictably and prevent small problems from becoming big headaches.

3 Things to Consider for Machine Tools and IIoT - PAC Controller - Pneumatic Division EuropeA good example is a motor that powers the position of a cutting tool. In the past, the motion controller or PLC received only speed and position information from the motor and its encoder. Now it must be able to receive information about errors, temperature and power factor. Most PACs (programmable automation controllers) are able to handle these inputs and provide the logic that determines when to send a maintenance alert. Some PACs even have internet gateways as part of their embedded HMIs (human-machine interfaces). This greatly simplifies the programming required to connect machines to the internet.

 

3. Marry the muscles of machines with intelligent motion control 

As industries continue to move into the 21st century, the demand for automated, intelligent equipment and controls is sure to expand into machine tool applications, as well as transportation, energy, food and beverage, and life sciences. 

Each of these applications has its own set of unique requirements. For example, food and beverage applications require absolute cleanliness and frequent, periodic maintenance, whereas transportation applications require long operating times and harsh, continually varying environments. For machine tools, the approach marries the muscles of machines with intelligent motion control and then shares information about machine health and production with the entire enterprise.

As mentioned, the IIoT is a highly integrated approach to industrial applications, machine tools, and operations. It requires collaboration on many levels between machine tool builders, motion control suppliers, sensor manufacturers, infrastructure vendors, and machine end users. When each partner offers the essential expertise needed, then machine intelligence can be applied to many different kinds of processes and business goals.

Categories
Recent Posts by Author

Central Tire Inflation System for Off-highway Vehicles

Parker's Central Tire Inflation System (CTIS) offers improved mobility when operating vehicles in severe off-road or soft soil conditions. Ideally suited for the agriculture and military markets, this...

What are the Challenges for Pneumatics in the Food Industry?

Starting from agriculture and food processing arriving to the packaging operation, automation is everywhere in the modern food plants and plays a fundamental role to address the required...

What is End Position Cushioning in Rodless Cylinders and How To Adjust

In the world of industrial automation, pneumatic rodless cylinders can now be found just about anywhere; from food and beverage packaging to pharmaceutical and chemical production lines. They have a...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for 3 Things to Consider for Machine Tools and IIoT


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha