Sealing Shielding

5 Factors to Consider When Determining Compressive Load of a Seal

5 Factors to Consider When Determining Compressive Load of a Seal_hollow O-rings_Parker O-Ring & Engineered Seals DivisionClosure force requirements are an important consideration for sealing applications, and the Applications Engineering team is often asked for guidance as to how to minimize or predict the amount of force it will take to close a properly-designed face seal groove.  

There are several factors to consider when trying to determine the compressive load. The most important of those considerations are:
 

 

Hardness of the rubber

It is correct to assume that as the hardness of the rubber increases so too does the compressive load.  Parker’s O-Ring and Engineered Seals Division offers materials that cover a range of 40-95 durometers (Shore A scale).

Below is an example of compressive load for a 0.139” CS O-ring made from NBR (Buna-N) materials at different measures of hardness (60, 70, and 90):
 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 1 Compressive force of .139" CS NBR of diff durometers_Parker O-Ring & Engineered Seals Division

Figure 1: Measure of compressive force requirements of a 0.139” CS, NBR material at different hardness levels.

 

Cross-sectional thickness

Another intuitive thought is that as cross-section diameter increases, so does the compressive load requirement.  

Below is a plot of compressive load requirements per linear inch for the standard cross-sections (0.070”, 0.103”, 0.139”, 0.210”, and 0.275”), and it follows that logic.
 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 2 Compressive load req at diff CS thicknesses on NBR 70 duro_Parker O-Ring & Engineered Seals Division

Figure 2: Compressive load requirements at different cross-sectional thicknesses on a 70 durometer NBR material.

 

Groove width

Groove width impacts compressive load because of how it changes the amount of gland-fill in a given application. If a groove is narrow, the O-ring is likely to make sidewall contact once compressed. When sidewall contact occurs, it results in higher compressive load requirements because of how the part is being constricted in the groove. If there is an application that has high gland fill, adding a draft angle can significantly reduce the compressive load requirements, as shown in Figure 3.  Figures 4, 5, and 6 show the impact of groove width and draft angle on gland fill.
 

 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 3 Compressive force for .070" NBR 70 duro_Parker O-Ring & Engineered Seals Division

Figure 3: Compressive force for 0.070" CS 70 Durometer NBR at 99.8% nominal gland fill when fully compressed. The graph shows the impact of the draft angle on the compressive load for grooves that have very high gland fill.

 

 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 4_Parker O-Ring & Engineered Seals Division

Figure 4: This image shows an O-Ring being compressed with no sidewall contact.

 

 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 5_Parker O-Ring & Engineered Seals Division

Figure 5: This image shows an O-Ring being compressed the same amount as in Figure 4, but with a narrower groove.  The result is a very high gland fill.

 

 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 6 FEA_Parker O-Ring & Engineered Seals Division

Figure 6: This is the same amount of compression as in Figure 5, but with a 3-degree draft angle added. The result is lower gland fill and lower stress on the O-Ring. 

 

Material family 

A common myth in the sealing industry is that there is a correlation between material family and compressive load requirements, but as seen in the graphic below, that is not necessarily the case. The only truly accurate statement is that silicone materials have lower compressive load requirements than that of other materials. Otherwise, many material families have a significant overlap in the amount of compressive load they generate for the same amounts of the squeeze.

Below is a plot of compressive load requirements per linear inch for various 70 durometer materials.

 

5 Factors to Consider When Determining Compressive Load of a Seal_Fig 7 Compression load req per linear inch for 70 duro materials_Parker O-Ring & Engineered Seals Division

Figure 7:  Compressive load requirements by a material family with hardness held at 70 durometers.

 

In summary, here are some ways to mitigate high compressive loads without sacrificing the amount of squeeze applied to the seal:
•    Use a softer (lower durometer) material.
•    Use a thinner cross-sectional diameter.
•    If gland fill is very high, widen the groove.  If that is not possible, consider adding a draft angle.
•    If appropriate for the application, switch to a silicone seal material.
•    If the application is conducive, consider using a hollow cross-section from our extruded product line.
 

 

 


William Pomeroy, applications engineer, O-Ring & Engineered Seals DivisionThis article was contributed by William Pomeroy, applications engineer, Parker O-Ring & Engineered Seals Division

 

 

 

 

 

TetraSeal: An Alternate Sealing Solution When An O-Ring Isn't Working

Sealing Fundamentals | Face Seal

Press-in-Place Seals for Axial Sealing Applications

Why is Shore A Hardness Important?

A Simple Guide to Radial Seals | Sealing Fundamentals

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for 5 Factors to Consider When Determining Compressive Load of a Seal


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha