Food Beverage Filtration

9 Benefits of Sterile Filtration Over Flash Pasteurisation of Beer

9 Benefits of Cold Stabilisation over Pasteurisation of Beer_Parker Bioscience_Beer bottlesThe shelf-life of beer is a key consideration for any brewing business – and there are multiple ways of extending this. It can be achieved through ingredient selection, packaging, or the brewing methods used during production.

The overall stabilisation of beer is of critical importance for the shelf-life of beers. As producers target new and faraway emerging markets, it is critical that the beer reaches drinkers’ palates with the characteristics that its creators have spent so much time and resources developing intact.

9 Benefits of Cold Stabilisation Over Flash Pasteurisation of Beer_Parker Bioscience_Cold Stabilisation White Paper

 

 

 

Interested in learning more about the benefits of sterile filtration for beer flavour and its impact on product losses? 
Download our complete whitepaper, Reducing the cost of microbial stabilisation of beer.

 

 

 

Pasteurisation

Traditionally, this has been done on a large scale by flash pasteurisation, a process of heating the beer which removes spoilage organisms that can be present. The typical spoilage organisms within beer include yeast – both wild, and those used in the brewing process – as well as specific anaerobic bacterial strains (most commonly lactic acid and acetic acid species). Pasteurisation, though an effective means of removing microbials can, however, negatively impact the flavour profile of the end product, and often reduces the shelf-life.

 

Sterile filtration

Sterile filtration is an alternative to pasteurisation, which has many of the benefits, but fewer of the drawbacks. Sterile Filtration (or cold stabilisation) refers to the final microbial filtration of beer using a microporous membrane to remove yeasts and other spoilage organisms. More and more brewers are turning to sterile filtration as a reliable method to ensure a longer shelf-life of their packaged beer.

It has been shown that beer which has been filtered to achieve stabilisation retains its unique and desirable characteristics more efficiently than beer stabilised through flash pasteurisation. It can also be demonstrated that sterile filtration can have a beneficial effect on taste characteristics throughout the duration of the beer’s shelf-life.

Parker Bioscience’s BEVPOR BR microfiltration filter not only ensures the microbial stabilisation of beer, it also helps to protect its unique sensory characteristics. Utilising a PES (polyethersulphone) membrane, The BEVPOR BR minimises the adsorption of beer components when compared to alternatives.

 

Key benefits of sterile filtration over pasteurisation

1. Protects the unique characteristics of beer

The pasteurisation process is a much harsher technique than sterile filtration, which has a gentler impact on the beer.

 

2. Protects a beer’s unique flavour throughout its shelf life

Sterile filtration increases the shelf life of a product, whereas pasteurisation, even for short periods, can lead to a decrease in shelf life.

 

3. Can be easily integrity tested to verify performance

Because of the relative simplicity of cold stabilisation systems compared to pasteurisation equipment, the performance of sterile filtration can more easily be monitored.

 

4. Head retention is improved

The filters used in sterile filtration minimise adsorption of desirable components and help to protect beer head retention.

 

5. Lower beer losses

Differences in the mixing phase mean that beer losses when using sterile filtration can be significantly lower than flash pasteurisation. This is mostly due to losses caused when beer is dumped following a shutdown of a pasteurisation system if any abnormalities in pressure, temperature or flow rate occur.

 

6. Energy efficiency costs are significantly reduced

Sterile filtration does not require the huge amounts of energy needed to run the plate heat exchangers used in pasteurisation and does not necessitate a buffer tank, resulting in less water consumption than that which is typically seen in the pasteurisation process.

 

7. Effective against heat resistant stages such as spores and cysts

Sterile filtration works just as well in removing microbial growth as pasteurisation and generates fewer of the drawbacks.

 

8. Simplicity of day-to-day operations

Sterile filtration requires fewer parts, making it easier to operate. Filters can often be regenerated in-situ, resulting in a longer service life.

 

9. Lower initial expenditure vs. flash pasteurisation hardware

Pasteurisation hardware is large and expensive in comparison to the lower initial outlay for a sterile filtration setup.

 

In summary: flash pasteurisation vs. sterile filtration

9 Benefits of Cold Stabilisation over Flash Pasteurisation of Beer_Parker Bioscience_Flash Pasteurisation vs Cold Stabilisation Graphic

 

9 Benefits of Cold Stabilisation Over Flash Pasteurisation of Beer_Parker Bioscience_Cold Stabilisation White Paper

 

 

 

Interested in learning more about the benefits of sterile filtration for beer flavour and its impact on product losses? Download our complete whitepaper, Reducing the cost of microbial stabilisation of beer.

 

 

 

 

9 Benefits of Sterile Filtration Over Flash Pasteurisation of Beer _Parker Bioscience Division Food and Beverage Filtration Blog_Daniel Vecsey

This post was contributed by Daniel Vecsey, market development manager, Parker Bioscience Division, United Kingdom.

Parker Bioscience Division offers filtration solutions to protect the quality and taste of beverage products. By working with our application experts, manufacturers can develop a tailored solution to ensure their beverage is free from contamination, full of flavour and visibly clear.

 

 

Related content

How to Protect Beer Quality at the Lowest Cost

Important Reasons to Filter Culinary Steam 

The Importance of Maintaining CO2 Gas Quality in Bottling Applications | Case Study

Have a question about Parker products or services? We can help: Contact Us!

Comments for 9 Benefits of Sterile Filtration Over Flash Pasteurisation of Beer

Rom
I've come here to learn about filtration vs heat for my own brew and which i should choose. I appreciate the info but when i got to the bottom and realised the info has come from market development manager of a company that offers filtration i realised I'd never get an honest answer, also you didn't mention whether to use 1 micro or 0.45 ect. Cheers anyway

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha