Sealing Shielding

Advancements in Automotive Transmissions

Advancements in Automotive Transmissions - automotive transmission cut away - Parker HannifinPrecision timepieces operate much like the inner workings for automotive machines. Underneath the back cover lies a series of gears and springs designed to measure the passage of time. We are told how these inner workings are created with such precision that they are able to measure the time accurately over whatever time period that the name brand manufacturer wants to advertise.  

Think about these “precision components” within the watch necessary to create this “machine” whose fastest rotational output is one rotation per minute, compared to an automatic transmission that has components that rotate more than seven thousand RPM!

35 years ago, the world of automotive transmissions moved from three speed boxes to four speed transmissions. In the late 90’s, six speed transmissions were introduced into the market offering improvements in fuel economy and shift quality. In the past five years, many automotive OEM’s launched several eight speed designs. Today, nearly every OEM is either launching or developing nine and ten speed transmissions, with patents being applied for eleven speeds.

Drivers of change

The drivers for this progression in development of automotive transmissions is: 

  1. fuel economy 

  2. drivability, or shift quality

The goal is to make sure the vehicle is in the most optimum gear ratio for whatever speed and acceleration combination the vehicle may be in from zero to whatever the legal speed limit may be in your area. This provides the best fuel economy. The more gear ratios you have available to you; the better chance you have of being in an optimal condition which improves overall efficiency.

From a shift quality point of view, think of it like a staircase. A typical staircase has 11-13 steps in order for a person to comfortably climb. Imagine if you reduced that to six or four steps, each step would be a struggle to walk up making the climb slow and cumbersome. Perhaps you have heard concerns regarding the vehicle “constantly shifting” or driven some of these vehicles with the higher number of speeds. The experience is actually positive in that the shifts are so smooth; you don’t actually feel them.

Competing for space

Advancements in Automotive Transmissions, Nested ClutchIt is important to note that the vehicles are not becoming any smaller. If anything, the trend is for smaller vehicles for better fuel economy. Obviously, a ten speed transmission had many more components than that of a four or six speed, but all of these parts need to fit within the same size transmission case. 

All of the different component groups are therefore fighting for real estate. A typical rear wheel drive transmission is roughly a meter long. In design meetings an entire room full of people may be negotiating over a tenth of a millimeter. This is the average diameter of a human hair. Many of the component tolerances are in the range of a hundredth of a millimeter. We are not only talking about splitting hairs, but we are talking about splitting hairs into ten layers! 

It is inspiring to me to think about these new transmissions and what it takes to put together these precision components and rotate them at more than seven thousand times per minute with enough balance that it doesn’t vibrate the driver out of the vehicle. These machines are just as much a piece of art as the “Precision Timepieces” and Parker is proud to be part of this process.

 

For more information from the Engineered Materials Group, please visit the Parker Engineered Materials Group Landing page. 

 

Advancements in Automotive Transmissions, Scott Van Luvender, Applications Engineering Manager, Automotive

 

 

 

This blog was contributed by Scott Van Luvender, applications engineering manager, Automotive.

 

 

 

 

Related content: 

Custom Seals Provide Trusted Results for Automotive Industry Challenges

Seals and the Quest for MPG

O-Rings and Seals for Automotive Transmission Fluid

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Advancements in Automotive Transmissions


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha