ZoomLock MAX press-to-connect flame-free refrigerant fittings help
to improve productivity for HVACR contractors and technicians on
the job. Having the ZoomLock MAX complete system equipped with...
Posted On 10/08/2020
Read More ►
ZoomLock MAX press-to-connect refrigerant fittings are changing the
way HVACR professionals connect refrigerant lines. By using
ZoomLock MAX, you, the HVACR technician can connect refrigerant
lines in...
Posted On 09/25/2020
Read More ►
Parker Sporlan’s ZoomLock MAX press-to-connect refrigerant
fittings, designed for the air conditioning and refrigeration
markets, allows HVACR contractors to make secure leak-free
connections in...
Posted On 09/16/2020
Read More ►
As forward-looking city planners react to the news of climate
change by tightening building codes for heightened energy
efficiency and air quality, contractors and distributors are on the
front lines...
Posted On 11/04/2019
Read More ►
In today’s world where time is precious, doing the job right the
first time is critical. Your customers want reliability and
appreciate the attention to detail that will ensure their system
provides...
Posted On 10/02/2019
Read More ►
Parker Sporlan's new web-based product selection program,
Virtual Engineer, allows the user to size, select, and fully
configure products for Air Conditioning and Refrigeration
applications. Virtual...
Posted On 08/15/2019
Read More ►
To obtain long term system life, it is important to keep
contaminants to a minimum. This is particularly true of a heavy
duty application such as a heat pump. Therefore, all heat pumps
should have at...
Posted On 02/20/2019
Read More ►
The design and operation of Parker Sporlan Head Pressure Control
Valves are discussed thoroughly in Bulletin 90-30. Installation and
service is covered in Bulletin 90-31. This Climate Control...
Posted On 10/24/2018
Read More ►
Cleaning air conditioner condenser and evaporator coils is a basic
need for proper system maintenance. In fact, it is probably the
number one performed maintenance task by air conditioning...
Posted On 07/02/2018
Read More ►
The Suction Line Filter-Drier method of cleaning up a system after
a hermetic motor burnout is favored by service technicians and
recommended by manufacturers throughout the HVAC and...
Posted On 08/01/2017
Read More ►
A solenoid valve with a built-in check valve is designed to replace
a liquid line solenoid valve in parallel with a check valve for
reverse flow. This valve may be applied in the liquid line of...
Posted On 03/02/2017
Read More ►
With our recent introduction of the Smart Service Tool Kit, there
have been many questions asked and answered. Let's review the ones
pertaining to buying and general details here: Q1: When will
the...
Posted On 08/03/2016
Read More ►
To ensure peak performance, solenoid valves must be selected and
applied correctly; however, proper installation procedures are
equally important. Aside from correct installation, troubleshooting
the...
Posted On 07/19/2016
Read More ►
We all know that a properly charged refrigeration system utilizing
a receiver must have a liquid and vapor interface in the receiver.
And we also know that saturated pressure and temperature...
Posted On 07/05/2016
Read More ►
In air conditioning and refrigeration applications, the ability of
the thermostatic expansion valve (TEV) to match refrigerant flow to
the rate at which refrigerant can be vaporized in the...
Posted On 06/21/2016
Read More ►
Parker's HVACR Tech tips cover service tips for the HVACR
technician servicing commercial refrigeration systems as well as
HVAC for both commercial and home. The following are
service tips for...
Posted On 05/24/2016
Read More ►
Calculating Superheat and Subcooling requires cumbersome equipment,
writing down temperature and pressure readings, converting pressure
readings using a PT chart, and finally subtracting totals to...
Posted On 03/16/2015
Read More ►
Lubricant-refrigerant mixture breakdown causes sludge formation and
other corrosive materials that will hinder the normal operation of
compressor valves and control devices in refrigerant and...
Posted On 08/01/2014
Read More ►
Climate control is the technology of controlling fluids and gases
to vary temperature. Parker provides comfort, convenience and
control through refrigeration and air conditioning. Key
markets Air...
Posted On 07/01/2013
Read More ►