Electromechanical

All About Cache and Forward Buffering in InteractX

All About Cache and Forward Buffering in InteractX - ParkerMotion - Parker Hannifin Electromechanical North America DivisionCache and forward buffering is one of those topics that can challenge users of HMI software. One way we are using this this blog is to demystify product topics that appear complicated but aren't. Cache and forward buffering is a powerful feature of Interact Xpress (InteractX) HMI Visualization Software that is under utilized because people think it's complicated. It's not.

 

InteractXpress HMI software

By far, the most cost-effective way to support industrial machinery installations or remote stations across geographical distances is via the internet or other IP connections. InteractX takes full advantage of the internet and the wide availability of web browsers to design, publish, run and support your HMI applications without sophisticated Windows-based software and hardware. InteractX  can be accessed from either the HMI panel or any PC running Internet Explorer.
 

Cache and forward buffering

Cache and forward buffering is an efficient low cost method of increasing the reliability of and availability of your database logged data in InteractX. It is especially useful for applications in regulated industries where "the dog ate my homework" isn't an acceptable excuse to inspectors looking for data that wasn't logged due to a network failure or server downtime.

Cache and forward buffering performs 3 simple functions automatically by enabling a simple check box in InteractX:

1. It monitors the connection to a remote database and identifies any loss of communication.

2. If any disconnection is identified it stores all log data locally on the InteractX stations hard drive. (Cache)

3. When the database connection is re-established it copies all of the locally logged data back to the remote database. (Forward)

This process provides a level of data security that is only topped by redundant technologies at a considerably higher cost. This feature is appreciated in industries such as pharmaceutical, food and beverage, heat treating, and even military contractors. Essentially anyone who logs data that they don't want to lose to a Server shutdown, cable failure, network switch failure or other infrastructure problem. Isn't that everyone who logs data?

 

Enabling cache and forward buffering in InteractX

Enabling cache and forward buffering in InteractX is extremely simple:

  1. Open your remote database InteractX project in you development system and select "Databases" from the application browser.
  2. Select the database and table that you want to enable cache and forward buffering on right click and select "properties". This will launch the "Object Properties" window
  3. Select "Connection Management" from the object properties window and select the checkbox marked "Enabled" under the "Caching" Section.
  4. There are two properties that should be tied to tags and tools in your application:

a. Cache Exists is a binary property that will toggle true when InteractX is caching data rather than sending it to a remote database. This should be attached to a tag and displayed on an indicator to signal the operator that InteractX has lost its connection with the remote database.

b. Clear Cache is a binary input that will attempt to forward the cache data to the remote database. This should be assigned to a tag that is attached to a momentary push button. This will allow the operator to attempt to clear the local cache after re-connecting to the local database.

 

We hope you have some applications for cache and forward buffering, that this is of value, and with the help of this post, you can easily implement this feature. One thing to keep in mind is that there is no need or benefit to turning this feature on for a local database. We'd recommend against enabling caching when the database is stored on the same PC as InteractX.

 

All about Cache and Forwad Buffering in Interactx - Information Anywhere Whitepaper DownloadDownload our whitepaper to learn more how web-enabled devices can push valuable production information anywhere your plant needs it.

 

 

 

 

 

 

Andy Balderson Electromechanical Division Marketing Manager Parker Hannifin Andy Balderson, Division Marketing Manager, Parker Hannifin - Electromechanical Division North America 

 

 

 

 

 

 

 

 

 

Other articles covering automation topics:

How the “Information Anywhere” Revolution Helps Boost Production

How to Make Creating Tags for HMIs Easy

How to Remotely Control Your Plant With a Mobile App

How the “Information Anywhere” Revolution Helps Boost Production

Categories
Recent Posts by Author

Choosing the Right Rotary Servo Feedback Device - Part 3

This is the final of a three-part series that spoke to the various feedback devices that are provided as options on Parker Servo Motors. Part 1 & Part 2 provided the basic theory of operation for the...

Choose the Right Screw Drive Train With Actuator Performance Calculator

There is no “one size fits all” drive train linear actuator technology for every application. In reality, the selection of different types of linear motion systems depends entirely on what is most...

How Using Electric Linear Actuators Can Save You Money

It’s well documented that creating compressed air for use by pneumatic cylinders is not a particularly cost-effective process, largely as a result of generator and system inefficiencies. With accounts...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for All About Cache and Forward Buffering in InteractX


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha