Fluid Gas Handling

An Effective Way to Identify Hydraulic Fitting Orientation

Identifying Hydraulic Fitting Orientation - Parker Hose Products Division - Orientation VideoHow do you determine the necessary hydraulic hose fitting when your application involves connecting two bent hoses? When your fittings are at an angle, understanding their orientation is critical. They must be oriented to each other to ensure proper installation with minimal stress on the hose from twisting. 

Fitting orientation is determined by the number of degrees measured in a clockwise direction. The orientation angle tolerance should be ±3° for overall length (OAL) up to 24" or ±5° for OAL over 24" according to SAE J517. If the angle of the hose orientation is not correct in the construction of a hose assembly, the performance and life of the assembly will be greatly reduced. For more information about hydraulic fitting orientation, watch the video below.


To identify the angle of a hose end simply there are two different methods. There is a near end reference method and a far end reference method. Each set of directions is described below. Whether you are using the near or far end method, the key is to remain consistent. When ordering hose assemblies, specify which method was used to ensure correct orientation. 

Near end reference method:

  1. Hold the hose assembly as if you are looking into a telescope.
  2. Position the elbow fitting closest to you at the 6 o’clock position (straight down).
  3. Identify the position of the farthest fitting, reading counter-clockwise.

Identifying Hydraulic Fitting Orientation - Parker Hose Products Division - Near end reference method

Far End Reference Method (the method used by Parker’s Hose Products Division):

  1. Hold the hose assembly as if you are looking into a telescope.
  2. Position the elbow fitting farthest from you to 6 o’clock position (straight down).
  3. Identify the position of the closest fitting, reading clockwise.

Identifying Hydraulic Fitting Orientation - Parker Hose Products Division - Far end reference method

To avoid fitting orientation, do not use an angle fitting on both ends of a hose assembly. Use a straight fitting and an angle adapter on the other end. This method makes installation easier and eliminates the need for orientation. Hose Products Division offers a wide selection of fitting options, view our hydraulic hose fittings for more information.

 

Kyri McDonough, Hose Products Division, Parker HannifinArticle contributed by Kyri McDonough, marketing services manager at Hose Products Division, Parker Hannifin.

 

 

 

 

Other related topics on hydraulic hose, hose application, and selection criteria:

Measure and Specify Hydraulic Hose Length With Ease
The Love-Hate Relationship Between Hydraulic Hose and Chemical Compatibility
Step-By-Step Hydraulic Hose Assembly
Successful Hydraulic Hose Assembly Starts Here
Five Most Important Factors You Need to Consider for Hydraulic Fittings
Hydraulic Hose 101: Fast Facts

Have a question about Parker products or services? We can help: Contact Us!

Comments for An Effective Way to Identify Hydraulic Fitting Orientation


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha