Filtration

Are You Ready for an Audit? Is Your Plant Compressed Air in Compliance with GFSI, SQF, and BRC Codes? Part 1 of 6

Are you ready for an audit? Is your plan compressed air in compliance with GFSI, SQF, and BRC Codes? - Mold and Bacteria Growth Image - Parker Hannifin Gas Separation & Filtration DivisionLet’s cut to the chase: The auditor is going to show up on your doorstep very soon, and you need to pass your GFSI (Global Food Safety Initiative), SQF (Safe Quality Foods), and BRC (British Retail Consortium) certification audits. There is a “Compressed Air Quality” requirement that is hard to define. What will the Auditor be looking for? Are there any meaningful GMPs (Good Manufacturing Practices) or industry standards to reference?  How do we actually do this? In short, the Auditor will be looking to make sure that adequate point-of-use filtration is in place to reduce microbial contamination risks from compressed air where it contacts the food or food-contact-surfaces.

 

Are you ready for an audit? Is your plan compressed air in compliance with GFSI, SQF, and BRC Codes? - Read Good Manufacturing Practices White Paper - Parker Industrial Gas Filtration and Generation Division

This white paper benchmarks the current Good Manufacturing Practices from the most popular food safety standards and consolidates them into one easy to understand document. Download.

 

 

 

 

The risks:

In a risk-based food safety system, it’s all about identifying the sources of potential food contamination and eliminating them. In this case, the risk which must be managed is microbial contamination of the food from compressed air. Impurities such as particulates, oil carryover and moisture can be present in compressed air. However, the most serious risk associated with compressed air, particularly when it comes into contact with food is microbial contamination. Choosing the correct filtration is important for both food safety and compliance reasons. 

Where compressed air contacts food or food-contact-surfaces during processing, there is the potential for contamination in the form of microbial pathogens (as well as yeasts and molds that wreak havoc on shelf life). This means that point-of-use filtration that is capable of removing microbial contamination needs to be in place.

 

The dilemma:

Very soon the auditors will be showing up on your doorstep to make sure you are correctly managing the risk of microbial contamination from compressed air. The industry standards and food safety code GMPs related to cleanliness and filtration of compressed air coming in contact with food are nebulous at best and not prescriptive at all. How can you pass the audit? 

 

The answer:

Sterile air filtration is an effective and affordable answer to removing potential microbial contamination from your compressed air system. When sterile air filtration is installed at point-of-use, the risk of microbial sized contamination is reduced in excess of 5-log.

Below is a quick overview of the types of compressed air filtration available: 

  • Particulate/Moisture Removal Filters: 5 to 40 micron
    • Removes particulates and liquid water - microbial sized contamination passes right through.
  • Coalescing Filters: 0.7 down to 0.01 micron
    • Removes oil and water aerosols - 1-log to 2-log reduction of microbial sized contamination.
  • Commercial Sterile Air Filters:  0.01 micron
    • Minimum 5-log reduction of microbial sized contamination. 

Therefore, by installing sterile air filtration at the point-of-use, where it comes into contact with food or food-contact-surfaces, you will meet or exceed GFSI, 21 CFR and all published food safety codes relative to compressed air quality in a food processing plant. 

 

Are you ready for an audit? Is your plan compressed air in compliance with GFSI, SQF, and BRC Codes? - Read Good Manufacturing Practices White Paper - Parker Industrial Gas Filtration and Generation Division

Download the white paper and learn the best GMPs for food contact air from the most recent food safety standards.

 

 

 

 

This is Part 1 of a 6 Part series on Compressed Air Contamination in Food Plants. Below are links to the rest of the series.

What are the Risks of Contaminated Compressed Air in a Food Plant? Part 2 of 6

How to Manage the Risks of Food Product Contamination from Compressed Air. Part 3 of 6

What’s the Best Line of Defense against Microbial Contamination of Food? Part 6 of 6

What are the Risks of Contaminated Compressed Air in a Food Plant? Part 2 of 6

Is Your Food Product Safe from Microbial Contamination? Part 4 of 6

 

This series was written by Lee Scott, market development manager, Parker Hannifin

Have a question about Parker products or services? We can help: Contact Us!

Comments for Are You Ready for an Audit? Is Your Plant Compressed Air in Compliance with GFSI, SQF, and BRC Codes? Part 1 of 6

Electrical Maintenance Training
This is one of the better blogs i've seen for electrical safety with lots of information and tips.It is full of information.I really appreciate for this blog.Thanks....
Electrical Maintenance Training

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha