Electromechanical

Automated Bottle Sorting | Simplifying Returnable Assets

Automated Bottle Sorting Simplifying Returnable Assets-Mixed Bottles-VisionTec-Parker-R Bindner-Electromechanical Division EuropeMost people of a certain age have childhood memories of returning beverage bottles to their neighborhood store and getting back their deposit coins, which were usually just enough to invest in an extra piece of candy from the same retailer.

It’s a simple business model when viewed at the front end; but if you restrict your viewpoint of anything to only what happens in front of you, you’ll miss the sophisticated backend operations, which enable that simplicity.

Appreciating the intricacy of what makes any reverse supply chain work requires a logistics tour.

 

Bottle return process – a mixed crate

What separates the recirculation of beverage bottles from any other returnable asset is the sheer variety of shapes and sizes to be managed and the ability to do so with minimal loss and damage as the pace of business accelerates.

Let’s go back through the bottle return supply chain at the point we came in—the store.

When that retailer receives the bottles brought in by customers, it usually mixes bottle types in crates. Whatever business receives these crates from the retailer—whether a bottling company or a third party bottle management service provider—the receiver must be able to detect differences and sort accordingly.

 

Before automation, it would take 40-50 people to sort bottles by hand in some breweries. 

Olaf Zeiss, Linear Actuator Product Manager, Electromechanical Division - Europe

 

Automated Bottle Sorting Simplifying Returnable Assets-VisionTec Bottle Sorting System-View of facility through observation area Parker-R Bindner-Electromechanical Division EuropeIncreasingly, beverage producers are leaving the task of detecting, sorting and returning those bottles to companies that invest in automated systems and training.

 

When a subcontractor is sorting bottles, they want to go as fast as possible because they get paid for every bottle.                                                                 Zeiss

 

 

Automated bottle detection and sortation

In Fuldabrück, Germany, Vision-Tec has made a business out of providing the necessary technology to bottling service providers to help them generate a profit from the returns process.

Vision-Tec offers automated modular material handling systems for crate and bottle detection, combining flexible multi-camera capabilities with sortation. This technology uses vertical and oblique image capture as well as ultraviolet light to detect various shapes of bottles and labels. Even a bottle’s luminescence can be detected--and with ultrasound, bottle height can be checked—with or without a cap.

This is sophisticated technology, calling for machine intelligence to remove counterfeit bottles and then refill or complete boxes with like bottles.

 

Sophisticated products for sophisticated technology

Automated Bottle Sorting Simplifying Returnable Assets-Automated Rails VisionTec-Parker R Bindner-Electromechanical DivisionWe were pleased when Vision-Tec chose to work with Parker Hannifin to supply multiple components for their automated bottle handling and sortation systems.

For instance, our linear actuators provide the higher velocity and acceleration required to meet the performance requirements of beverage producers and bottlers. Further, our actuators withstand the fluctuating temperatures of European summers and winters and the corrosive environments of bottling plants.

 

In the summertime, these breweries and bottlers work 24 hours a day. These are wet environments, where the equipment is cleaned regularly and the plant doors are normally open because bottles are always coming in and going out. The actuators must withstand these temperature swings.

 Zeiss

 

That ruggedness extends to the motors and gears used in Parker’s drive combinations, which offer IP65 compliance (resistance to water and dust).

Vision-Tec’s sorting robots must be equally robust—not to mention scalable and expandable. Sort stations are equipped with two grab arms each, taking the wrong bottles out of the crates as they are fed into the line, and then filling in the right ones in continuous motion operation. By setting up intermediate storage/buffers, travel paths for the grab arms can be substantially reduced. Depending on the stage of extension, up to 1,200 boxes per hour can be sorted.

Automated Bottle Sorting Simplifying Returnable Assets-ServoController-VisionTec-Parker R Bindner-Electromechanical DivisionIn addition to their complex optical systems and control technology, Vision-Tec uses Parker Hannifin HPLA linear axes for controlling the mechanical longitudinal movements (in the running direction) of the sorting modules. In conjunction with intelligent Parker compax3 servo controllers, with their EtherCAT communication interface, these features are designed not only to meet the requirements of beverage bottlers but of textile engineering firms, process engineering companies, logistics service providers, warehouses and machine tool manufacturers, as well.

 

Parker’s complete drive packages contribute significantly to the high performance and reliability of our systems. Also significant [are] their support for the sizing process and configuration process of the drive systems, and the solution’s rapid availability. 

Knut Oppermann, Technical Manager, Vision-Tec

 

Vision-Tec is planning five to ten more bottling lines by the end of the year for other beverage companies, and Parker will help it customize system requirements to those different needs.

While bottle return processing will never be as simple as the front end transaction, with these automated systems, it may seem so. Just take a look at the video.

 

 

How to over come challenges linked to the new EU Rail Standard EN45545 - Case Study

Read more customer success stories here 

 

 

 

 

 

 

 

 

 

Learn more about our processing and packaging solutions here.

 

 

Rochus Bindner-Marketing Communications Manager-Electromechanical Division EuropeContributed by Rochus Bindner, marketing communications manager, Electromechanical Division Europe.

 

 

 

 

Related content:

Developing Custom Motion Control Solutions

Designing a Low-cost Actuator for Harsh Environments

Life and Linear Positioners

Take the Guesswork out of Choosing a Linear Drive Train

 

 
Categories

Have a question about Parker products or services? We can help: Contact Us!

Comments for Automated Bottle Sorting | Simplifying Returnable Assets


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha