Gas Generation

Benefits of Using a Hollow Fiber Membrane System to Generate Nitrogen

Benefits of Using a Hollow Fiber Membrane System to Generate Nitrogen - Hollow Fiber Membrane used in Nitrogen Gas Generation - Parker Industrial Gas Filtration and Generation DivisionFor many industrial and analytical applications, using an in-house generator to supply nitrogen (N2) offers multiple advantages over receiving the gas in tanks from a supplier. Those advantages include:

 

 

 


 

  • Less waste - The in-house system generates nitrogen at a pressure and flow rate required for the application, on-demand, so no gas is wasted.
     
  • Improved plant safety - The danger of handling high-pressure cylinders is eliminated.
     
  • Greater security of supply. Users don’t need to depend on outside vendors. An in-house system eliminates delivery delays, long-term contracts, and uncontrollable price increases.

Although situations vary, most users can expect a payback period of slightly more than one year when switching from bottled nitrogen to generating nitrogen in-house. That’s assuming conservatively that a facility uses a flow of 20 L/min (slpm) of N2 for four hours per day. Over the period of one year (250) days), 1,200,000 L of N2 will be consumed, equivalent to 186 standard 9x56 inch cylinders.

In addition to the direct benefits, there is also an environmental benefit to consider. Gas distillation is a highly energy-intensive process. The use of a hollow fiber membrane for the generation of nitrogen uses significantly less energy and hence produces much less greenhouse gas than does fractional distillation. Not only does the distillation process itself use significant energy, but so does transporting the gas cylinders from where the N2 is produced to where it is used, as well as transporting the empty cylinders back to the plant.

A Low-Energy Process

How does the in-house generator achieve these benefits?

How Membrane Separation Technology WorksRather than distill the N2 from the air, a process that requires significant cooling, a hollow fiber membrane separates oxygen and water vapor from the nitrogen at room temperature. First, compressed air flows through a high-efficiency coalescing filter to remove water vapor and particulate matter and then through an activated carbon scrubber to remove hydrocarbons. The air then passes through hollow fiber membranes that preferentially allow the oxygen and any remaining water vapor to escape while the N2 continues passing through the tube. From there, the nitrogen passes through a final filter containing activated sterile nitrogen filtration media.  Finally, the purified nitrogen passes directly to the application via the system’s output port.

For many applications, an in-house hollow fiber membrane system is a more convenient, safer, lower cost, more reliable and more energy-efficient way to generate a continuous supply of pure nitrogen. And it’s better for the environment.

 

 

Benefits of Using a Hollow Fiber Membrane System to Generate Nitrogen - Download the white paper - Parker Industrial Gas Filtration and Generation DivisionDownload the white paper and learn about the environmental and cost implications of fractional distillation and how it compares to in-house nitrogen generation

 

This is Part 2 of a 3 part series on a sustainable approach to the supply of nitrogen.  Following are links to the rest of the series: 

Nitrogen Generation using an In House Generator vs Fractional Distillation  Part 1 of 3

Pressure Swing Adsorption Technology as an Alternative to Conventional Air Separation Part 3 of 3

This series was contributed by David Connaughton, business development manager - nitrogen, Parker Industrial Gas Filtration and Generation Division.


 

Categories
Recent Posts by Author

Nitro Iced Coffee Uses Self-Contained Nitrogen Generators | Case Study

Battle Grounds Coffee is a small, community-oriented coffee shop in Haverhill, MA. The owners were challenged to find a more efficient and consistent way to deliver Nitro Coffee to their customers.  ...

How to Prevent Contamination & Corrosion in Demineralized Water Storage Tanks

Power generation plants rely heavily on demineralized and deionized water to maintain required levels of water purity during process operations. Managing the water supply is critical under...

Nitrogen Generation System Reduces Costs in Additive Manufacturing

Additive manufacturing or 3D printing is a relatively new rapid manufacturing technology that has become mainstream in recent years. It covers a wide variety of processes used to produce a multitude...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Benefits of Using a Hollow Fiber Membrane System to Generate Nitrogen


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha