Sealing Shielding

Best Conductive Plastics: Five Things to Look For

Best Conductive Plastics: Five Things to Look For, Parker Chomerics Division, Conductive plastic boxCan electrically conductive plastics really replace traditional metal electronics enclosures? The answer is a resounding yes! There are very effective electrically conductive plastics available today that provide excellent electromechanical properties that help shield portable electronics from the electromagnetic interference (EMI) noise that is proliferating our daily life. Smart phones, Bluetooth, Wi-Fi, radio, even your television are all susceptible to EMI. So here are the key points you may want to consider when evaluating electrically conductive plastics for your application:

#1: Shielding effectiveness

Every day we encounter EMI, and sometimes it happens at the most inopportune time. Maybe you’ve been put on hold for an hour and just when the customer service agent gets back to you, your cell phone drops the signal. Or perhaps you’re blasting the car radio listening to your favorite song, and just when the chorus comes on, static noise drowns out the tunes as you drive under high tension power lines. These are all examples of EMI interfering with our daily life, and electrically conductive plastics can help shield our portable devices from these interruptions.

#2 Manufacturing cost performance

When it comes to small portable electronics such as smart phones and other wireless devices, there is typically no more cost effective way to produce them than using injected molded conductive plastics. Metal housings often require additional rework after tooling, such as bending and threading, that injection molded plastics do not need.

#3: Weight

Nowadays, smart phones and other small portable electronics such as life science devices are routine. Electrically conductive plastics allow these devices to remain lightweight and compact, all while providing critical EMI shielding performance to not interfere with the device’s performance.

#4 Durability

Electrically conductive plastics can typically withstand everyday wear and tear better than many metal enclosures and metal PCB components. In a lab, conductive plastics can pass drop test after drop test with flying colors, which is not so easy to do with heavy metal enclosures.

#5: Corrosion resistance

Even if a conductive plastic housing gets dinged up, scuffs and scratches do not lead to corrosion susceptibility. Most conductive plastics can resist corrosion in harsh environments much better than metal can.

Benefits of conductive plastics

Conductive plastics are very effective given the correct applications. Given the shrinking nature of electronics devices, often you will save money going with conductive plastic over traditional metal because conductive plastics typically do not need additional machining such as adding threads, bending, etc. Given the right application, conductive plastics can be cost effective for smaller portable devices.

Be sure to work with a material provider that has extensive knowledge in the above areas and can support you on your design.

Discover the Parker Chomerics family of PREMIERTM Conductive Plastics for electronics enclosures today.

 

Jarrod Cohen, Best Conductive Plastics: Five Things to Look For, Parker Chomerics Division

 

 

This blog was contributed by Jarrod Cohen, marketing communications manager, Parker Chomerics Division.

 

 

 

 

Related Content:

Improved EMI Shielding Consistency of Single Pellet Conductive Plastics 

Design Decisions Relating to EMC Shielding

New Essential Handbook for EMI Shielding Applications

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Best Conductive Plastics: Five Things to Look For


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha