Compressed Air Gas Treatment

Best Way to Dry Compressed Air in Hazardous Areas

Best way to dry compressed air in hazardous areas - parker hannifinMany instruments and controls operating in hazardous industrial environments require instrument grade compressed air to ensure effective operation. Without clean, dry air, quality control and process control systems may be subject to damage from water and contaminants resulting in costly downtime and maintenance.

Examples of hazardous environments include refineries, chemical processing plants, mines, grain mills and other facilities that may have high concentrations of flammable gases, vapors, combustible dusts, or ignitable fibers. Even a small spark can lead to a horrific explosion that can be dangerous to both workers and equipment in the area.

 

Best way to dry compressed air in hazardous environments - Download Drying Compressed Air White Paper - Parker HannifinDownload our white paper and learn how to safely dry compressed air in hazardous environments.

 

 

 

 

While industrial plants typically have centralized instrument-grade air lines, the air is often contaminated with water and can benefit from a point-of-use drying system that guarantees clean, dry air to a specific dew point. Traditional drying systems that use PSA (Pressure Swing Adsorption) or refrigerant drying technologies require expensive modifications to operate within hazardous areas. However, compressed air dryers that use membrane technology operate without electricity, therefore, no modifications are necessary for them to operate in hazardous areas.

 

Equipment considerations

Electrically operated equipment that is located in hazardous areas must be specifically designed to prevent ignition and explosion. Electrical enclosures found on the various types of traditional compressed air drying equipment (refrigerated dryers, chemical dryers and desiccant dryers) must be strong enough to contain an explosion within the cabinet. Therefore the walls of the enclosure must be very thick and heavy. The internals in the cabinet must operate at temperatures below the ignition temperature of the hazardous material. The cabinet must also be designed so that any ignition inside the cabinet would not immediately exit the cabinet; in other words, the ignited gases must be quenched so that the escaping gases don’t cause an explosion outside the cabinet. The added weight and heavy-duty designs of such equipment increase the cost and space requirements.

 

Membrane technology as an effective alternative

Membrane dryers are designed with no moving parts and require no electricity, making them inherently explosion proof. Membrane dryers use specially formulated membrane microtubes that are selectively permeable to water vapor. The microtubes provide an excellent medium for producing dry air from standard compressed air. As the compressed air travels along the length of the membrane, water vapor diffuses through the membrane, producing clean, dry compressed air at the outlet. A small fraction of the dry air is then directed along the outside surface of the membrane to sweep the moisture-laden air away from the membrane (Figure 1). These dryers can reduce the dew point of compressed air to as low as -40°F/°C. They operate with very little noise output - just a small amount of purge air is emitted through small exhaust ports. To free up floor space, membrane dryers can be wall-mounted. They contain no refrigerants or freons, making them environmentally safe. Membrane compressed air dryers are ideal for remote areas, Class I, II or III hazardous locations, sub-freezing environments, and applications requiring water vapor removal and a consistent dew point.

Figure 1: How membrane technology works

Best way to dry compressed air in hazardous areas - membrane technology - Parker Hannfin

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Best Way to Dry Compressed Air in Hazardous Areas - Download Drying Compressed Air White Paper - ParkerDownload the white paper and get the facts on how to safely dry compressed air in hazardous environments.

 

This post was contributed by David Connaughton, product manager, Parker Industrial Gas Filtration & Separation Division.

 

 

 

Related posts:

Facts You Need to Know About Drying Compressed Air

Choosing the Right Compressed Air Dryer for Your Application

8 FAQs on Drying Electrical Cabinets with an Air Dryer

How to Keep Electrical Cabinets Dry in Food Processing Plants

 

 

Categories
Recent Posts by Author

Is Your Compressed Air Purity Validated?

Is your manufacturing plant's compressed air purity validated? Perhaps the methods you are employing to check the purity or quality of the air in your facility are only indicative? Is there...

Six Points to Consider When Applying ISO8573-1 in a Manufacturing Facility

ISO (International Standards Organization) is the world’s largest developer and publisher of international standards. There are three ISO standards that relate to compressed air quality and testing...

Air Preparation for High-Precision Manufacturing

Today's global industrial, industrial and electronics manufacturing environment is uncompromising. To remain at the forefront, suppliers must meet a multitude of demands - shortest lead time, highest...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Best Way to Dry Compressed Air in Hazardous Areas


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha