Not all BSPP 60° cone fittings are created equal, nor are they always interchangeable.
Questions often arise regarding compatibility and interchangeability between different kinds of BSPP 60° cone fittings, which typically serve as hose adapters on ‘low-cost’ hydraulic systems from Asia and Europe. This is similar to how NPSM pipe swivels are typically used in the U.S. on equipment such as log splitters and other low-end hydraulic farm machinery.

Figure 1: Two main styles of BSPP 60° fittings conform to either British or Japanese standards, such as Parker's K4 BSP (right) adapters and JIS fittings (left). While the designs are similar, they are not always interchangeable.
Comparing the two main styles:
There are two main styles of BSPP cone fittings that conform to either British Standard BS 5200 or Japanese Industrial Standard JIS B8363 (Figure 1). Both are designed as hose adapters rather than tube connections, and both seal by metal-to-metal line contact between the conical surface of the internal seat and a corresponding surface on the mating component. Although cone angles and threads are identical, there are instances when these fittings will not function properly if interchanged. Figure 2, below, illustrates where a gap exists between sealing surfaces, whereas Figure 3 shows an effective seal created by the combination of properly matched components.

Figure 2: Mating a BS 5200 body and JIS 8363 swivel nut results in a hydraulic assembly that will not seal.

Figure 3: A BSPP 60° cone fitting seals by metal-to-metal line of contact.
Identification: There is no standard for identifying these fittings. Some manufacturers mark JIS adapters with ‘JIS’ on the hex or forging flats for visual identification. BS 5200 adapters do not carry a specific identifying mark. Also, BS 5200 adapters may or may not have the tapered undercut at the end of the threads.
Compatibility with hose fittings: Both adapters connect to hose fittings if the connection meets the appropriate standard.
Interchangeability: BS 5200 adapters do not mate with JIS swivel connections. JIS adapters may mate with BS swivels, but these fittings should not be considered interchangeable because they were not designed as such.
Here is a review of the similarities, differences, and interchangeability of these two styles:
Similarities:
- The seat angle is 60° for both styles.
- Both use British Standard Pipe, Parallel (BSPP) thread.
- Both have an undercut at the end of the threads near the hex.
Differences:
- Each conforms to a different standard, British Standard BS 5200 or Japanese Industrial Standard JIS B8363.
- Thread lengths are shorter on BS 5200 adapters. (Dimension A, Table 1)
- The 60° cone diameter differs for each type. (Dimension B, Table 1)
- The BS 5200 can also be used as a port fitting. A tapered undercut on some version of the adapter helps locate a loose seal when used as a port fitting. The taper centers the port's bonded seal for proper sealing.
- BS 5200 adapters include size 10 (5/8 in.) and JIS adapters do not.

Table 1: Comparing dimensions
The International Standards Organization is developing a standard to replace BS 5200 and JIS, based mostly on the BS 5200 standard. In the meantime, while BS 5200 and JIS 8363 adapters are similar, in some instances they are not interchangeable. The best advice is to avoid mixing them.
Did you find this post helpful? Subscribe to TFD techConnect posts by email. TFD techConnect is a technically-focused monthly blog written for engineers specifically around motion and control engineering challenges.
If you have questions or comments, please post them and I’ll respond if warranted. If you want to talk to me directly, I can be reached at Parker Tube Fittings Division, 614.279.7070 or via email. Download a print-friendly version of BSPP 60° Cone Fittings: Looks Can Be Deceiving.
Do you want to receive new product announcements and technology updates from Parker Tube Fittings Division? Subscribe today and stay informed.

Burleigh Bailey, Research & Development - Engineering Manager, Parker Tube Fittings Division
Additional helpful content:
The Truth About Pressure Ratings for Hydraulic Fittings and Adapters
Turn vs. Torque? How Making the Right Choice Keeps Your Hydraulic Fitting Connections Leak-Free
Four Easy Steps to Identify Hydraulic Threads
Sizing Tube to Maximize Hydraulic System Efficiency
How Many Times Can I Reassemble a Hydraulic Fitting?




Comments for BSPP 60° Cone Fittings: Looks Can Be Deceiving
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.