Sealing Shielding

CamLock Seals Extend Seal Life with Innovative Dual Bead Design

DB CamLock Seal, semi fueling gas station with camlockCam and groove style couplings, commonly referred to as camlock fittings, are used across many industries due to their ability to quickly connect and disconnect from holding tanks, pumps, filters, or other equipment. Although the nature of the camlock design makes it economical and rather simple to use, Parker’s engineers have found a way to improve the design even further with the DB CamLock seal

The standard sealing element commonly used in a camlock fitting is a rectangular cross section flat gasket. Since these flat gaskets are a solid chunk of rubber, they can be extremely difficult to compress when using the cam and groove locking mechanism of the fitting. An abnormally high closure force can sometimes result in an incomplete connection which, many times, results in leakage. Also, when compressed, the flat gasket geometry provides a broad but very low seal pressure across the mating substrates.

Parker DB CamLock Seal design features:

  • Dual seal bead
  • Increased maximum seal pressure
  • Reduction of damaging seal stresses
  • Reduced compressive load
  • Excellent retention fit
  • Color-coded materials

Compared to the standard flat gasket, the innovative Parker DB CamLock seal offers several improved features starting with the dual bead design. The dual bead feature provides redundant seal points which can be useful if damage were to occur to the primary sealing bead during operation. Having that second sealing bead can keep the fitting leak free and operational until a replacement can be sourced. 

The DB CamLock design also increases maximum seal pressure on the fitting hardware by approximately 55%. This increase in seal pressure provides a much better barrier to potential fluid passing by the seal. Having a higher seal pressure acting on the substrates, while reducing areas of significant harmful stress, reduces the chances of seal damage, increasing your seal life. 

Upon use, one of the most evident features of Parker’s DB CamLock seal design is the reduction of clamping load required during connection of the fitting. Using state of the art Finite Element Analysis (FEA), you can expect a reduction of closure force around 40% over traditional flat gaskets. A lower clamping load helps to ensure a complete connection which is essential to preventing leaks with cam and groove couplings.  

Parker DB Camlock

Another necessity for eliminating leakage in camlock couplings is making sure the sealing element is present. The DB CamLock seal design provides an excellent retention fit and is available in all standard size camlock assemblies. Therefore, you don’t have to worry about the seal falling out during transport. 

Lastly, the DB CamLock seals are available in material families that are commonly used in many fluid handling applications with a color-coded format. This allows an operator to be able to easily identify the seal material being used in a coupling by simply identifying the color.  

Common seal compound offerings for the DB CamLock seals are:

Parker Camlock compounds

For more information on DB CamLock Seals or other Parker EMG products visit Parker's O-Ring & Engineered Seals Division website and chat with us online.  

 

Nathan Sowder

 

 

Article contributed by Nathan Sowder, Business Development Engineer, Parker O-Ring & Engineered Seals Division.

 

 

Sealing Fundamentals 

How to Properly Install a Parker Hollow O-ring How to Choose the Right Fluid Power Hose

Categories
Recent Posts by Author

Low Drag Dynamic Sealing for Hydraulic Clutch Applications

As automatic transmissions become more advanced as a system, the components within must evolve as well. Performance drives the design and there are many factors that must mesh together to achieve the...

Extend Seal Life and Reduce Maintenance Costs With Our Versatile FF156

We are coming up on two years since the birth of FF156-75 and this compound is one worth celebrating.  If you don’t know what FF156 is, thank you for taking a few minutes to read this blog. FF156 is...

Innovative Rod Seals Enhance Performance of Actuators in Aviation

Hydraulic sealing systems used in aviation technology applications are exposed to particularly challenging ambient influences such as extreme temperature fluctuations and aggressive pressure...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for CamLock Seals Extend Seal Life with Innovative Dual Bead Design


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha