Fluid Gas Handling

Check Valves Are the Unsung Heroes of Fluid Power

Check Valves Are the Unsung Heroes of Fluid Power_Check Valves_Parker Quick Coupling DivisionCheck valves are unseen and undervalued. These valves are found in just about every mobile and industrial hydraulic system on the planet. Simply put, if there’s a pump, most likely you will find a check valve. Check valves keep the fluids flowing in the desired direction to prevent damaging flow or pressure in the reverse direction. They can also be used in applications to maintain a system pressure for optimum system readiness and performance. Surprisingly, for a valve that performs such a critical function, a check valve incorporates very few components - the body, poppet, spring and retainer.

 

Give this essential valve its due

Considering its wide use, engineers, maintenance technicians and even end users should have a basic understanding of the function that this essential component serves in their systems. More often, however, that’s not the case. Generally, misunderstood in their function and importance, when you mention check valves, the responses range from “they just don’t work” to “never use them.” As stated earlier, a check valve exists to keep fluid flowing forward while helping to prevent reverse flow of fluids within a system. That makes them important for many reasons.       

 

Where and why to use a check valve

  • Pump protection: Systems with multiple pumps will experience extended service life when check valves are utilized to isolate and protect these components from system failure. Examples of this could be a high/low pump or even an emergency pump on a mobile system.
  • Cooler protection: Damaging pressure spikes can be avoided by diverting pressure/flow.  Examples are widespread in mobile and industrial applications with hydraulic and lubrication oil coolers.
  • Actuator flow control: Whenever speed control of an actuator is needed for operator safety, use a check valve in the lift and lower circuit. Examples are forklifts, aerial work platforms or hood systems on large equipment.
  • Keeping prime/pressure: Commonly used on fuel systems to maintain prime, for ease of maintenance and for quick start up.  Also, check valves are essential for use on hydraulic systems to prevent pump oil starvation at start up. 

 

The most innovative check valves on the market

Check Valves are the Unsung Heroes of Fluid Power_Check Valves in Open and Closed Position_Parker Quick Coupling DivisionLike any product out there, quality makes the difference. When that product is a check valve, you want the best on the market. There’s just too much at stake to consider anything else. That’s where Parker comes in. Parker’s check valves are engineered to perform under the most demanding circumstances. Offered in many configurations, our in-line style check valves are available in a variety of sizes, pressure ratings, flow capacities and crack pressures to satisfy most hydraulic system applications.

• The DT Series check valves cover the widest variety of applications. These hard seat check valves are offered in sizes from ¼” to 1-1/2” with the added benefit and convenience of compact design. Select sizes are also available in 45°, 90° and tee shape fittings which can help optimize system design by reducing labor and leak points. If you are unsure where to start looking for check valves, the DT Series is a great first option.

• The CV Series check valves are another hard seat check valve option for your application. Built using a rugged modular design that results in less pressure drop for increased performance in critical applications.

• The CPIFF Series check valves are a soft seat check valve option for your application. Soft seats are often used in applications where zero backflow is allowed.

 

Many standard configurations are available for purchase on parker.com. In stock items can ship within two business days. Learn more about Parker's complete line of check valves. Contact Quick Coupling Division for custom configuration options.

 

One of the most important valves for any system

Finally, a check valve is a relatively inexpensive component that protects significantly more expensive system components. A company can save thousands of dollars by implementing check valves and protecting these vital components. With so much on the line, it only makes sense to choose a reliable and high-quality product that can deliver under the most extreme conditions. And that’s what you can expect from Parker.

 

Check Valves Are the Unsung Heroes of Fluid Power_Matthew Walley_Parker Quick Coupling DivisionContributed by Matt Walley, product sales manager, Quick Coupling Division, Parker Hannifin.

 

 

 

 

 

Related links:

Avoid the Most Common Workplace Hazards with a New Way to Change Oil

Three Key Benefits of Using Non-Spill Quick Couplings

Screw-to-Connect Couplings Make Hard Work Easier

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Check Valves Are the Unsung Heroes of Fluid Power


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha