Chemical Handling

Theme Park Thrills Owe Much to Hydraulics and Accumulators

Most people enjoy theme parks as a place to get away from work, but for those in the hydraulics industry, they are a place to demonstrate their expertise. Behind many of the rides that make your...
On August 8, 2018

Point-of-Care Testing Requires Microfluidic Precision

Point-of-care testing (POCT) is a rapidly expanding segment of the healthcare industry, especially for at-home care and disease management. This expansion is driven by an increasingly diverse array of...
On August 7, 2018

How to Apply Conductive Foil Masking Tape Before Painting

EMI (electromagnetic interference) is the disruption of the operation of an electronic device when it is near an electromagnetic field in the radio frequency spectrum that is caused by another...
On July 31, 2018

How Oil Changes are Impacting your Bottom Line

It’s not an exaggeration to say oil is the lifeblood of all machines. Commercial fleet vehicles, heavy machinery and large-scale power generation equipment all rely on clean engine oil to lubricate,...
On May 24, 2018

Know Your Pneumatics: Continuous Position Sensing

The use of industrial networks to make sensors and actuators more intelligent has become common across modern factory environments, and the use of continuous position sensing is a pathway to achieving...
On February 20, 2018

Most Popular Filtration Technology Blogs of 2017

2017 saw economic growth accelerate and the indicators suggest that trend will continue. This puts productivity initiatives high on the list of manufacturers, keen on taking full advantage of...
On January 4, 2018

Metallurgy Makes or Breaks Tube Fittings

For over forty years, Parker has lead the development of the chemical hardening process ideal for ferrules designed to grip and seal stainless steel tubing. The process is called Suparcase. This...
On September 29, 2017

Convoluted Tubing: Flexible Tubing for Tight Spaces

PTFE convoluted tubing is used when customers need a very flexible tube that can withstand constant flexing, for high-temperature fluid handling applications and for applications where other wires and...
On August 31, 2017

Four Ways to Use Hose in a Wet Method Silica Dust Suppression System

If the excitement of the construction industry takes your breath away, congratulations! You’re in the right business. But construction workers may have shortness of breath for a far more serious...
On August 1, 2017

Use a Metal Seal for Those High Temperature or High Pressure Situations!

Parker Hannifin Engineered Materials Group has developed a wide variety of metal seals which can be formed or machined. A metal seal is a highly engineered sealing solution which provides...
On June 22, 2017

The Importance of Natural Gas Product Certifications

To stay at the forefront of the competitive transportation markets, fleet managers are turning to alternative fuels that meet the environmental and economic needs of today and in the future.  Natural...
On June 12, 2017

The Love-Hate Relationship Between Hydraulic Hose and Chemical Compatibility

Chemical compatibility in regards to hydraulic hose can be complicated, however it is necessary for the performance and hose life. When selecting a hose, you must consider the chemical compatibility...
On June 7, 2017

New 20,000 psi Coupler Takes Offshore Drilling Operations Deeper

Withstanding the high pressures of deepwater reservoirs has been a challenge for offshore drilling operations limited by the capabilities of their equipment. Going after deep reservoirs with higher...
On April 27, 2017

Certified Natural Gas Vehicle and Fueling System Products

As we move into the future, the need for transportation is merging with society’s concerns about pollution, climate change, depletion of natural resources and the long-term sustainability of our...
On April 21, 2017

Hydraulic Hose 101: Fast Facts

Hydraulic hose is more complicated than it seems. There are many factors that go into designing, manufacturing, and testing high-quality hydraulic hoses. At Parker Hannifin Hose Products Division, we...
On March 30, 2017

8 Simple Tips for Maintaining and Replacing Your Mast Hose

Does your mast hose look like this? Employees often overlook hoses during routine maintenance checks for material handling equipment, which inevitably leads to machine down time and lost...
On March 20, 2017

Modular Seal Kit for Pneumatic Cylinders Covers All Kinds of Applications

Parker Prädifa offers a large number of combined pneumatic seals and wipers for the open groove of the EU system. By installing the right type of seal, a wide range of applications can be covered with...
On February 8, 2017

Why Nitrogen Is Better than Argon for Wine Production

A question often asked in the wine and grape industry is: which is better for wine production, nitrogen or argon? Both are inert gases at room temperature, and both are used for blanketing wine...
On December 6, 2016

Solenoid Valve Selection for Harsh Outdoor Applications

Wherever water, chemical mixtures, oil and gases are transported through pipes, solenoid valves are instrumental in remotely or automatically controlling the flow and transfer of fluids. But...
On October 4, 2016

Going to Extremes: A Closer Look at Hydraulic Hoses

For many industrial and mobile applications, hydraulic hoses need to withstand extreme conditions, including aggressive liquids, scorching to freezing temperatures and ultra-high pressure. Do you have...
On September 15, 2016