Hydraulic Filtration

Clean Hydraulic Fluids Are the Key to Top Performance

Clean Hydraulic Fluids Are the Keys to Top Performance - Power Lines - Parker Hydraulic Filtration DivisionFor optimum renewable energy performance, power generation equipment including transmissions, EHC drives, turbines, and transformers depend on clean hydraulic fluids and oil. When a hydraulic system becomes contaminated with air, water, or suspended solids, performance begins to break down. Any of these contaminants can cause a lack of lubrication between component surfaces, which results in increased friction, leading to more wear debris and eventual failure.

Power generation is one of the few industries that replaces hydraulic fluids and oils only when it is absolutely necessary, adding new fluid when reservoirs become low. This makes it even more important that power generation engineers utilize high-quality filtration systems to keep fluids and lubricants as clean and long-lasting as possible.

Protect mission-critical equipment

Clean Hydraulic Fluids are the Key to Top Performance - Sentinel Fluid Purification System, Hydraulic Filtration division, Parker HannifinWater, entrained air, gases, and solid particulates contaminate turbine oil and hydraulic fluid and must be removed on a regular basis. Water is one of the most common contaminants in a fluid system and one of the most damaging. Therefore, it is especially important to protect mission-critical hydraulic and lubrication systems through the use of appropriate filtration.

With conventional purifiers, water cannot be removed until the hydraulic reservoir fluid reaches and maintains a temperature of 150 degrees F. This can take hours, if the ambient temperature is low and the reservoir volume is large, which slows down operations and drives up energy costs. In contrast, Parker’s Sentinel™ fluid purification system removes water and other contaminants from hydraulic fluid more efficiently, and at less cost.

The Sentinel treats contaminated hydraulic fluid in smaller volumes. Every two minutes a 6KW heater heats 4-5-gallon batches of fluid at a time, cleaning the fluid and then releasing it. This conserves power and saves time that would otherwise be spent heating the entire main system reservoir to the required temperature.

 

Other advantages include:

  • Optimized size, weight, and design for oil reservoirs up to 1,000 gallons
  • Up to 75 percent lighter and smaller than most traditional full-scale purifiers on the market
  • Easy to place, position, and move due to smaller overall footprint
  • Can be automated with customer-selected parameters within Parker's IQAN interface

Automatic monitoring

The Sentinel is the only purifier on the market with an automatic monitoring system. A Parker IQAN controller allows the operator to set the parameters of operation. Once the parameters are set and the unit is turned on, it operates until the low limit of water content has been attained. At this point, the timing setting takes over. The timer can be set from 1 hour up to 720 hours. Once the time setting is reached, the unit turns on, pulls a sample of the fluid and measures the water content. If the content is below the high setting, the unit goes back to the timing mode. If the water content is at or above the high setting for water, the unit goes back into operation and runs until it reaches the low setting again and repeats. The Sentinel can also be operated in standard mode—once the parameters are set and the unit starts, it will run until it reaches the low water setting and then turns off. It will not come back on until the operator restarts the unit.

Automatic filtration extends the usable life of fluids, minimizes energy consumption, and reduces costs. By keeping the hydraulic system as dry as possible, the Sentinel lessens the chance of destroying a bearing on a turbine and losing millions in revenue as a result of lost time and mechanical repair.  

Sentinel™  an efficient, portable unit designed for fluid purification and protecting hydraulic systems was awarded the title of "Product of the Year 2015" by the magazine "Inżynieria i Utrzymanie Ruchu” (“Engineering and Maintenance" in Poland) in the category of "Diagnostics, monitoring, and regulation." The Sentinel stretches maintenance budgets and boosts productivity, by streamlining the dehydration process and reducing costly, unscheduled downtime.

 

Attending the 2019 PowerGen International show?

Visit Booth #3119 at POWERGEN International 2019 to see how Parker offers the most comprehensive product and system solutions for today’s power generation environments. Learn more about our filtration products, sealing and shielding, sensors and diagnostics, heated enclosure system, combustion turbine and energy storage solutions.

 

Garry Moore_Inside Sales Technical Support - Parker Hannifin Hydraulic Filtration DivisionArticle contributed by Garry Moore. field technical services, Hydraulic Filter Division, Parker Hannifin

 

 

 

 

Other related content includes:

Innovative New Fluid Purifier Saves Time, Money in Hydroelectric Plants

Smart Cylinders Reduce Operational Costs

New Wireless Sensor Monitors Compressed Air Systems with Ease

Grid Tie Technology Makes the Most of Renewable Energy

Wireless Transmission of Performance Data Extends Equipment Life

Categories
Recent Posts by Author

How to Perform a Cold Corrosion Test for Cylinder Oil

The oil used to lubricate the cylinders of large 2-stroke marine diesel engines has to contend with high temperatures and acidic products formed during the combustion of sulphur-rich bunker...

Industrial Machine Vibration Analysis and Condition Monitoring

A condition monitoring system is concerned with the early detection of failure. Vibration monitoring systems, whether they use traditional techniques based on displacement or acoustic emission sensor...

Fuel Monitoring Matters

Whether you choose distillates, liquefied natural gas (LNG) or scrubbers to meet the new International Maritime Organization (IMO) fuel regulations in 2020, it will be even more critical to regularly...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Clean Hydraulic Fluids Are the Key to Top Performance


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha