Fluid Gas Handling

CNG Fuel Systems for Heavy Duty Vehicles

CNG Fuel Systems for Heavy Duty Vehicles - Heavy duty white truck - Parker Veriflo - Parker HannifinWhen we think about emissions, we usually think about our vehicles and the new wave of personal electric vehicles. The reality is that heavy-duty vehicles used for transportation of goods and passengers produce far more emissions and use a lot more fuel than personal vehicles.

Making a bigger impact on emissions

We can make a bigger impact in reducing emissions by replacing heavy-duty diesel vehicles, especially those that use a lot of fuel. We can also impact more lives by reducing emissions from transit and school buses and protect the health and our fragile environment. 

While some nations have already taken a leap, the USA is now accelerating its move to natural gas heavy-duty truck and transit buses. In fact with Cummins-Westport’s North America launch of the near-zero NOx ISL-G series engines, CNG/LNG now offer the cleanest way to go for medium and heavy-duty applications.

The largest limitations have been that our duty cycles are typically more demanding in terms of variations of temperature with deep negatives like -40F in the north to high 100’s in the deserts of Arizona and New Mexico. The current fuel system designs also limit the amount of recoverable fuel from the tanks to about 350-400 psi tank pressure. Further, no regulatory system in the market was certified to the nationally recognized to ANSI NGV3.1 standard. Existing systems also compromise the reliability of vehicles with poor filtration of contaminants and designs that include materials such as Buna, susceptible to failure in the local operating conditions.

Energy outlooks see growth

CNG Fuel Systems for Heavy Duty Vehicles - FM80 fuel regulation system - Parker Veriflo - Parker HannifinMost energy outlooks see a huge growth in the use of these vehicles in the coming years and thus OEMs and integrators have been looking for answers. Parker FM80 fuel regulation system answers all the needs of the market and delivers more.

Parker Hannifin’s FM80 Fuel Regulation Module, a fully integrated CNG (compressed natural gas) flow control and regulation system for medium and heavy-duty vehicles -

  • Withstands extreme variations in temperature, flow, vibration, supply pressure and gas composition. It is constructed of robust anodized aluminum, a high-grade low Sulphur “Vericlean” stainless steel poppet and extremely reliable Parker VG109 seals
  • Features advanced FM80 metal piston-style regulator, coalescent filters, pressure sensors, lock-off solenoid valve, heat exchanger, and low-pressure relief valve all in one compact body
  • Offers customizable levels of integration and more configuration options
  • Exceeds industry standards for leakage and safety and is certified to ANSI NGV3.1
  • Meets flow and regulation specifications of all leading OEMs with CNG options
  • Features technology which prevents freezing problems in the winter and eliminates leakage of gas into coolant from wear of soft diaphragms and seals over time 
  • Incorporation of a larger oil sump means longer times between filter drains, helping increase driver productivity and asset utilization
  • Optimized for advanced fuel handling performance in 5- to 12-liter engines
  • Piston-style regulator design offers stable pressure delivery and control of CNG throughout the full range of extreme engine and environmental operating conditions
  • Integrated internal regulator components, with fewer connections, work together to eliminate fuel line failures due to freezing, dampen flow-induced vibration, reduce drop in high flow, and extend cycle life
  • Manifold design of regulator system reduces chance of fuel line pressure increase due to reduced volume of fuel between solenoid valve and regulator seals
  • Achieves high nominal flow rate (175 lbs./hr, 80 kg/hr) and the low low-pressure operating parameter (250 psig), which increases the usable range of CNG vehicles by 3 to 5%

Many of the OEMs and integrators have entrusted their 2016 and onward model year CNG offerings to Parker. Learn more, then let us help you develop a CNG system to meet your toughest EPA, CARB emissions and that offers a user experience that far surpasses any of the conventional fuels.

 

Article contributed by Parker Hannifin Veriflo Division 

Related content:

New O-ring Face Seal Fitting Promotes Environmental Sustainability with Alternative Fuel Compatibility

Parker Veriflo CNG Dispensers Support Cleveland's Transition to CNG Buses

How New LNG and Natural Gas Fuel System Architecture is Advancing the ‘Golden Age of Gas’

Hydraulic Hybrid Technology Demonstrated on CNG Fueled Refuse Truck

The Choice Between LNG and CNG as Transportation Fuel

 

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for CNG Fuel Systems for Heavy Duty Vehicles


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha