Climate Control

Compressor Overheating is the Number One Refrigeration Problem

Compressor overheating is the number-one refrigeration problemMany refrigeration compressors break down simply because they overheat. There are two main reasons why overheating can have such a devastating effect on compressors:

  • Loss of the lubricating properties of the refrigeration oils

  • Chemical decomposition of the refrigerants and/or oils, which can occur suddenly

The oil breakdown in the refrigeration system has plenty of negative side effects. Sludge and solid particulate matter can plug the oil inlet screen in the compressor sump or the lubrication passages in the crankshaft—loss of lubrication can quickly result in failed bearings. Oil-breakdown deposits can also line the internal surfaces of the refrigeration system, especially the inner walls of the piping, compressor and control valves, plugging up thermostatic expansion valves (TEVs) and other control valves.

All these problems can be the result of a dirty condenser, which results in a higher condensing temperature. According to EPA research, a heat transfer coil with a meager 0.042-inch-thick film of dirt on its surface can result in nearly a 21-percent loss of heat-transfer capacity. A higher condensing temperature, combined with increased suction temperature (from underfeeding TEVs), can result in excessive discharge temperatures that accelerate oil decomposition.

 

Four causes of excessive discharge temperatures

Before they can fix the problem, technicians must know what caused the excessive discharge temperatures in the first place. The four most common root causes are listed below:

  • High suction superheatcommon system conditions that cause increased suction temperatures are high TEV superheat settings, ineffective or missing insulation and restricted TEVs.

  • Reduced condenser capacitytypically the result of poor maintenance, this occurs when the condenser fins become restricted with dirt and the airflow necessary to deliver the condenser’s rated capacity is reduced.

  • Lowering the suction pressurethis is important to operate the system with the highest possible suction pressure. When system suction pressure is reduced, instead of fixing the true issue, the compression ratio increases creating higher discharge temperatures.

  • Refrigerant characteristicsbecause R-22 is subject to higher compression ratios, which can stress bearings and reduce compression efficiency, R-22 can be problematic as a “refrigeration” refrigerant, particularly in low-temperature applications.

Compressor overheating is refrigeration’s most serious field problem.

In many cases, system problems and compressor failures are directly related to high discharge temperatures.

Condensers should be cleaned regularly to keep them operating at their rated capacity. The suction vapor temperature should be kept within acceptable limits by setting TEV to superheat appropriately and insulating the suction line properly. Compressors should not be allowed to operate below design suction pressures, because this will lead to higher discharge temperatures.

With some refrigerants and applications, other solutions (for example, a compressor body cooling fan motor) may be required to solve high discharge temperature issues. A temperature-responsive expansion valve, which responds to discharge temperature, may also be used. By injecting saturated liquid/vapor into the suction line temperature-responsive expansion valves will reduce the temperature of the superheated suction vapor, which in turn reduces the excessive discharge temperatures.

Article contributed by Sporlan Division, Supermarket Refrigeration, Parker Hannifin

 

Additional articles include:

Using P-T Analysis as a Service Tool for Refrigeration Systems

Use of Suction Line Filter-Driers for HVAC Clean-up After Burnout

Head Pressure Control for Supermarkets

Clean-up Procedure for Refrigeration and Air Conditioning Systems

Is the Compressed Air in Your Food Plant Safe?

 

Categories
Recent Posts by Author

How to Drive Business With HVACR Trends - Infographic

What’s changing in HVAC? It might be simpler to ask what isn’t changing. According to Steve Yurek, the president and CEO of the Air-Conditioning, Heating, and Refrigeration Institute (AHRI),...

HVACR Tech Tip: How to Correctly Size Solenoid Valves

To obtain reliable performance with solenoid valves on refrigeration or air conditioning systems, it demands careful consideration of application requirements during the selection process. Parker...

HVACR Tech Tip: Protect Your System During Maintenance With These Steps

Simple maintenance steps for system reliability There are simple steps that an HVACR technician can take during their routine spring and fall inspections or at any time when onsite to...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Compressor Overheating is the Number One Refrigeration Problem


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha