Hydraulic Filtration

In Oil and Gas, Condition Monitoring Curtails Costly Downtime to Drive Profitability

In Oil and Gas, Condition Monitoring Curtails Costly Downtime to Drive ProfitabilityThe global oil and gas industry is a highly competitive market in which companies must be willing to adopt cutting-edge technologies to get the most out of oil reserves, keep their operations running smoothly and maintain an advantage over the competition.

Depending on the segment of the market in which they operate, oil and gas companies control assets ranging from drilling rigs, offshore platforms, and wells in the upstream segment, to pipelines, LNG terminals and refineries in the midstream and downstream segments.

The process of designing, building, operating and maintaining these assets comes with a large capital expenditure, and realizing a valuable return on that investment is more critical than ever in the current downturn impacting the oil and gas industry. One key to doing so is to minimize non-productive time (NPT).

Any time during which a site such as a drilling rig, production plant or refinery is not operating at full capacity is classified as NPT. It is often measured by the percentage of days throughout the year during which operations cannot proceed as planned, and accounts for a large percentage of operating costs for many oil and gas projects.

While in the past technicians have largely maintained a “fix it when it breaks” mentality, that approach has been replaced as the cost of NPT has become better understood and monitored. Today the components and systems found on equipment at drill sites are not only tracked electronically, but every effort is made to analyze their status to better predict and avoid NPT.

In Oil and Gas, Condition Monitoring Curtails Costly Downtime to Drive ProfitabilityWith decades of experience in working to address the NPT challenge, Parker has developed the ATEX Metallic Wear Debris Sensor, ATEX Moisture Sensor, Icount Bottle Sampler and many other products designed to closely monitor the condition of components and systems on oil and gas equipment. By doing so, these solutions facilitate rapid and informed decision making which helps to keep equipment running efficiently and for longer.

Parker experts are also available to support customers in creating and implementing their condition monitoring program, offering a unique blend of technical expertise and market knowledge that makes Parker a valuable partner to oil and gas customers aiming to maximize productivity and profitability. 

Implementing a condition monitoring program improves asset uptime, extends asset life and, perhaps most importantly, improves safety by preventing potentially dangerous conditions when equipment fails. No matter how remote the location or demanding the environment, we can provide a condition monitoring system to effectively minimize risk and increase uptime.  

 

In oil and gas Condition Monitoring curtails costly downtime to drive profitability - Cristiano GarauArticle contributed by Cristiano Garau, lead application engineer, Parker Kittiwake, Hydraulic Filtration Division Parker Hannifin.

 

 

 

 

 

Additional resources related to condition monitoring:

Reliability Centered Maintenance Reduces Costly Downtime in Oil & Gas Applications

Streamline Your Condition Monitoring Process

New Wireless Sensor Monitors Compressed Air Systems with Ease

Condition Monitoring Solutions for Power Generation Plants

Wireless Transmission of Performance Data Extends Equipment Life

Oil and Gas: Monitor Chemical Mixing Wirelessly

Categories
Recent Posts by Author

How to Perform a Cold Corrosion Test for Cylinder Oil

The oil used to lubricate the cylinders of large 2-stroke marine diesel engines has to contend with high temperatures and acidic products formed during the combustion of sulphur-rich bunker...

Industrial Machine Vibration Analysis and Condition Monitoring

A condition monitoring system is concerned with the early detection of failure. Vibration monitoring systems, whether they use traditional techniques based on displacement or acoustic emission sensor...

Fuel Monitoring Matters

Whether you choose distillates, liquefied natural gas (LNG) or scrubbers to meet the new International Maritime Organization (IMO) fuel regulations in 2020, it will be even more critical to regularly...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for In Oil and Gas, Condition Monitoring Curtails Costly Downtime to Drive Profitability


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha