Fluid Gas Handling

Condition Monitoring Solutions for Power Generation Plants

Condition Monitoring Solutions for Power Generation Plants - SensoNODE closeup viewGas and steam turbines are staples in the electricity generation industry. As the market becomes more competitive, keeping assets running efficiently at power generation plants is more critical than ever. This means ensuring that turbines are operating reliably and efficiently is just as important.

Condition monitoring plays a significant role in that. By employing an effective solution that monitors the temperature, pressure, and humidity levels of a plant’s assets, operators can diagnose problems or damage to turbines and inconsistencies among processes. Addressing and repairing these issues before they become problems saves downtime and replacement costs.

 

Commissioning

Initial testing of the plant’s processes after construction can help ensure your assets and turbine are operating properly. Commissioning processes depend on the type of turbine, its application, and size, so there’s no cookie-cutter method for ensuring a new turbine is performing up to the task. Along with standard tests of the turbine’s electrical infrastructure and civil engineering quality checks, there are common tests at the plant level that must be a part of any commissioning process.

 

Condition Monitoring Solutions for Power Generation Plants - diagram of powerplant and locations for sensor - Parker Hannifin

 

Humidity monitoring

Turbines operate within harsh conditions that include inclement weather, high winds, and constant motion. Operating in these elements can adversely impact various components within a turbine’s gearbox, rotor, bearings, and the tower itself. Humidity and moisture in the gearbox can cause less than the optimal operation of rotary components, leading to corrosion, reduced product quality, and ultimately break down.

Monitoring a system’s performance can be a good indicator of any potential problems with a turbine. By keeping tabs on a system’s humidity, as well as the ambient humidity of the plant, operators can gauge any potential effects on a turbine’s performance.

 

Temperature and pressure monitoring

To keep a turbine operating consistently and with minimal chance of overheating, it is necessary to keep components within the gearbox well lubricated and cooled with clean oil. A good filtration package is also important. Monitoring changes in a system’s temperature and pressure levels can help operators identify when filters and/or oil in the turbine may need to be replaced.

Also, monitoring for increased fuel consumption and/or reduced output could indicate a more serious problem, such as compromised integrity of rotary components within the turbine. Such issues can lead to displacement or damage to toothed gears, blade damage or fatigue failures, and other structural damage that will ultimately impact a system’s performance.

 

The good news

Conditional Monitoring Solutions for Power Generation - SensoNODE Sensor closeup - Parker Hannifin Sensors need to handle the harsh environment in which turbines exist. They need to be able to consistently deliver accurate readings amid high-speed blade rotation, rapid airflows, high temperatures, and large-amplitude vibrations.

Parker’s SensoNODE™ Blue sensors and Voice of the Machine™ Software allow users to monitor conditions using multiple sensors simultaneously, each measuring the temperature, pressure, or humidity of specific points within a system. Using Bluetooth technology, the sensors transmit large volumes of data to mobile devices wirelessly, keeping operators out of dangerous situations.

Small and easy to install, SensoNODE Blue sensors eliminate the heavy, complex wiring setups that could limit the versatility of the sensors and stunt the monitoring process. Since no wires exist, they’re not at risk of being caught in moving parts, which means quicker and lower costs for the commissioning process.

Learn more about how SensoNODE™ Sensors and Voice of the Machine™ Software provide accurate diagnostics and condition monitoring for all aspects of Power Generation Plants.

 

Condition Monitoring Solutions for Power Generation Plants - Tad Orstad, Applications Engineer for SensoNODE Sensors and SCOUT SoftwareContributed by David Shannon, business team manager, Parker Hannifin, Quick Coupling Division.

 

 

 

 

Related articles on condition monitoring:

Dust is More Damaging Than You Think

Wireless Transmission of Performance Data Extends Equipment Life

Effective Predictive Maintenance of Rotary Machines

Scrap Happens – Save Money by Reducing Rework

Size Matters: Small, Wireless Sensors Make Diagnostic Efforts Easier for Mobile Equipment

Improve Solar Panel Maintenance and Condition Monitoring Efficiency

Streamline Your Condition Monitoring Process

Wireless Monitoring Improves Asset Management and Patient Safety

Have a question about Parker products or services? We can help: Contact Us!

Comments for Condition Monitoring Solutions for Power Generation Plants


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha