Fluid Gas Handling

Continuous Remote Monitoring vs. Route-Based Condition Monitoring Solutions

Continuous Remote Monitoring vs. Route-Based Condition Monitoring Solutions - Plant floor sensor image - Parker Hannifin Quick Coupling Division - SensoNODEWithout question, the Internet of Things (IoT) has changed the way we look at condition monitoring and diagnostics. Many now consider checking analog gauges and jotting down measurements on a clipboard obsolete.

Industries from manufacturing and automotive to health care and transportation are using advanced condition monitoring solutions to:

  • Identify issues before they escalate

  • Reduce downtime

  • Decrease maintenance costs

  • Avoid dangerous situations

  • Make better, more informed decisions

  • Improve labor efficiency

All of these benefits have opened the doors to Predictive Maintenance.

 

Which wireless solution is best for your business?

Continuous Remote Monitoring vs. Route-Based Condition Monitoring Solutions - Condition Monitoring Graphic - Parker Hannifin Quick Coupling Division - SensoNODENow, it isn’t a question of if you need an advanced condition monitoring solution, but which type? We break down the key differences between Continuous Remote Monitoring and Wireless Route-Based Monitoring to help you answer that question.

Wireless route-based monitoring for on-site diagnostics

If you need a solution for short-term monitoring or diagnostics, then a wireless route-based condition monitoring solution will likely give you the best return on your investment.

The “route” speaks to the asset manager’s maintenance routine, whether it’s walking a plant floor and inspecting each machine, or running diagnostics on a specific piece of equipment. Wireless sensors are installed at key points on your machines to monitor vital conditions (e.g. temperature, pressure, and humidity) and wirelessly transmit that information to a mobile device by using the required software or mobile app.

Wireless route-based condition monitoring 

Continuous Remote Monitoring vs. Route-Based Condition Monitoring Solutions - Route-based Monitoring Graphic - Parker Hannifin Quick Coupling division SensoNODEThis type of wireless route-based condition monitoring solution alleviates some of the common issues, including:

Time

Technicians within range can wirelessly retrieve information from sensors installed on the asset. Without the wires and cables required by a traditional monitoring solution, technicians can monitor and record each measurement simultaneously, then move on to the next piece of equipment. This helps cut down the time it takes to complete the route, thus potentially increasing the frequency of those routes.

More daily measurements mean a more robust archive. There is also a better chance of catching the sudden spikes or drops in condition levels that often go unnoticed, leading to decreased asset performance or outright failure.

Accuracy

With one mobile device, such as a smartphone, technicians can easily and quickly monitor the digital readout and automatically record a measurement with the click of a button. Now the grease, dirt, and grime that build upon an analog gauge, making it more difficult to read, are no longer an issue…and neither is the technician’s handwriting.

Record keeping

Maintaining a digital record that can be exported and uploaded to a computer ensures recorded measurements are no longer subject to being lost, misfiled, torn, or stained with the random coffee cup. It’s also easier to analyze digital files to identify trends than it is with hardcopy records.

Increased downtime

The biggest benefit is that wireless monitoring solutions don’t require shutting down the piece of equipment to take measurements. Leaving job-critical assets online while running diagnostics means companies can investigate issues without halting production.

These benefits allow workers to:

  • Easily take accurate measurements from individual machines

  • Wirelessly diagnose machine issues to reduce downtime and save money

  • Easily monitor your assets/machines on-site

  • Export recorded measurements

  • Avoid potentially unsafe working conditions

Route-based condition monitoring is perfect for companies that need an immediate, short-term diagnostic solution that is more accurate than traditional gauges.

Continuous monitoring for remote measurements

Continuous Remote Monitoring vs. Route-Based Condition Monitoring Solutions - Continuous Remote Monitoring Graphic - Parker Hannifin Quick Coupling division SensoNODEContinuous remote monitoring gives users a broader view of their assets by providing a steady stream of information, so they never miss a beat. Unlike wireless route-based monitoring, which requires a technician to be within the range of a sensor to get the measurement, users can take measurements with a continuous remote monitoring system anywhere they have an internet signal.

While conceptually similar, continuous remote monitoring solutions do have a few differences compared to route-based monitoring solutions:

Long-term vs. short-term monitoring

Route-Based Monitoring begins and ends when the end-user is actively using the system. Continuous Remote Monitoring solutions are designed for long-term monitoring to give users immediate access to the health of their machines. Continuous monitoring solutions are always ‘watching’ machines and systems for any issues that could lead to reduced performance or downtime. That means that at any time of the day, users can access critical information without interrupting production.

Big picture vs. snapshot

While Route-Based Monitoring helps users take measurements and run diagnostics on individual assets, a Continuous Monitoring solution gives users the bigger picture of how things are running. Users can gather trend data from all assets at all locations and analyze that information to find ways to optimize machine performance and keep production running smoothly.

Remote vs. on-site monitoring

By giving users access from anywhere with an internet connection, they can monitor and collect the data of multiple assets from multiple locations simultaneously. Cloud-based remote monitoring lets users access everything from their desktop, so plant managers can analyze trends for all assets right from their office whether they’re on-site or miles away.

Employing a continuous monitoring strategy allows companies to:

  • Access data anywhere, anytime

  • Receive alert notifications of potential issues

  • Visualize data in a way that makes the most sense

  • Customize alerts, trend charts, and dashboards

  • View measurement anomalies easily

  • Support continuous improvement efforts with trend data

  • Export data for analyzing later

Continuous remote monitoring is perfect for large-scale operations with multiple assets or production/assembly lines.

 

Final thought

If you’re considering either wireless route-based or continuous remote monitoring for your business, but you still have questions, our engineers can help you choose the best option for your needs. As a global leader in connected motion and control technologies, Parker has spent years developing solutions and strategies for both types of advanced condition monitoring.

Contact us today for more information on remote condition monitoring solutions

 

 

Marc Williams | Product Sales Manager | Parker HannifinContributed by Marc Wililams, IoT project lead, Parker Hannifin Corporation.

 

 

 

 

 

Related, helpful content for you:

Wireless Transmission of Performance Data Extends Equipment Life

How to Easily Connect Users to the Digital Plant

Reduce Diagnostic Risks with Heavy Machinery

IIoT Drives New Opportunities in Condition Monitoring

Turn any Wired Sensor into a Wireless Device with a 4-20mA Transmitter

Have a question about Parker products or services? We can help: Contact Us!

Comments for Continuous Remote Monitoring vs. Route-Based Condition Monitoring Solutions


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha