Sealing Shielding

Custom Environmental Seal Solutions: When Unique Requirements Throw A Curveball

Custom Environmental Seal Solutions: When Unique Requirements Throw A Curveball - hollow profiles - Parker Hannifin O-Ring & Engineered SealsWhen it comes to the topic of utilizing elastomeric seals, it’s stereotypical to consider environmental sealing as one of the simpler categories of applications. Near-ambient pressure and temperature conditions and a lack of exotic or aggressive chemistries are the kinds of details that typically come to mind. However, throw in a curveball or two and suddenly the challenges posed can make finding a solution seem reasonably more intricate.

 

Unique conditions call for custom design expertise

For instance, consider the potential challenges of sealing off a battery enclosure or other kind of electrical component. While this may seem like a simple issue of finding a material that seals against moisture or fluids found in open-air conditions, manufacturability also needs to be taken into consideration. Many electrical enclosures have Custom Environmental Seal Solutions: When Unique Requirements Throw A Curveball - electric vechicle enclosure seals - Parker Hannifin O-Ring & Engineered Seals Divisionparticular spatial requirements, including those which involve seal housings that require low closure force or those with sharp corners that could damage more conventional seal designs like solid-profile O-rings. These kinds of conditions are becoming more and more frequent, especially considering the automotive market and its increasing share of electric vehicles, which involve a larger proportion of electrical components in a more compact arrangement for reduced weight. Add to this the fact that these batteries and other electrical components are becoming more elaborate and more expensive as a result, and the need for highly-effective protective sealing design becomes imperative. This is where Parker engineers can design products like picture frames gaskets and hollow profiles that are customized to unique requirements.

 

Industry standards can get complicated

There are also industry standards for electrical enclosures that help ensure a seal material meets relevant requirements that might not be taken into consideration or well-understood by those outside the elastomer industry. For instance, the UL 50E standard evaluates the physical properties and volume swell requirements deemed necessary for a seal material to withstand the conditions in these applications. Parker has materials from the EPDM, nitrile, and silicone compound families that are certified under this standard.

Another set of industry standards that reveal the specialization of environmental sealing requirements are Ingress Protection (IP) Ratings, which rate sealing performance against both solid contaminates and various forms of water (the most strenuous ratings for sealing against solid contaminates - those most relevant for elastomeric seals - indicate prevention of dust contamination).  These ratings apply to the effectiveness of an entire assembly and not the material of a component specifically – this means each assembly must be assigned a rating on a case-by-case basis.

One example of an IP rating is IP65, which uses a special set of test requirements to evaluate designs for resistance to blasts from standard-pressure water jets. Another example is IP67, which rates sealing performance under water submersion conditions. Parker engineers can provide the design support necessary to ensure a system earns either of these two ratings in particular, as well as those that verify an assembly’s ability to prevent dust contamination from inhibiting performance.

To see how Parker engineers can provide environmental sealing solutions involving standards like these and many others, consult our Application Engineers or chat with us online. 

 

 

FFKM Offers Low Particle Generation and Extreme Etch Resisance - Nathanael Reis, Parker Hannifin

 

This article was contributed by Nathaniel Reis, applications engineer, Parker O-Ring & Engineered Seals Division

 

 

 

 

 

 

Related content:

Environmental Seal Enclosure 101

Environmental Seal Enclosures: UL94 V-0

Sealing for Harsh Environmental Conditions in Telecommunications Applications 

 

Categories
Recent Posts by Author

Is an ASTM Callout the Best Way to Specify Your Elastomer Needs?

I have had many discussions with customers as to the value of using an ASTM elastomer compound description on their prints to define a specific application or elastomer requirement versus listing...

Large-Size PTFE Seals Withstand Aggressive Media and High Temperatures

Seals made of the fluoropolymer PTFE are used where many other sealing materials (such as rubber elastomers, polyurethanes, fabric-reinforced elastomer seals, etc.) reach their limits in terms of...

5 Design Considerations for EMI and Weather Sealing Combination Gaskets

Combination electromagnetic interference (EMI) shielding and weather gaskets, more commonly known as EMI shielded combo strip gaskets, are an excellent choice for a variety of applications that...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Custom Environmental Seal Solutions: When Unique Requirements Throw A Curveball


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha