Sealing Shielding

Degradable Materials Simplify Well Completions in Oil & Gas Extraction

Degradable Materials Simplify Well Completions in Oil & Gas Extraction-GettyImage-901140746-HDR of Offshore drilling rig at day - Parker Degradable Materials Simplify Well Completions and Cut Costs in Oil & Gas Extraction_Parker O-Ring & Engineered Seals DivisionThe emergence of degradable and dissolvable materials is providing oilfield service companies an opportunity to increase efficiencies and cut costs in the oilfield by simplifying well completions. These materials replace their conventional metallic and polymeric counterparts in completion tools, but eventually, break down and disperse when exposed to common completion fluids. This eliminates the need for well interventions to mill out or retrieve used tools. This can result in a reduction of drill time, a safer work environment, and monetary savings for the operator. Parker Hannifin produces dissolvable and degradable metal alloys, thermoplastics, and elastomeric materials that can enhance your well completions.

 

Degradable elastomers

Parker O-Ring and Engineered Seals (OES) Division produces degradable elastomer formulations that can be used in frac plugs, liner wipers, and other sealing applications common in the completions segment. These elastomer formulas have tough physical properties and low compression set and are designed to replace materials such as Nitrile or HNBR in conventional tool designs. With proper design, tools using Parker degradable elastomer can withstand the high pressures (>8,000 psi) generated during hydraulic fracturing while still eventually deteriorating away, allowing well production without having to be drilled out. These degradable elastomers can be produced in a variety of desired forms such as O-rings, custom molded shapes, and packing elements. They can also be bonded to dissolvable metal alloys to produce completely degradable solutions. If needed, Parker offers a product engineering team to assist with the design of components and rapid prototyping services to help cut down on development timelines.

 

 

Degradable thermoplastics

Parker Engineered Polymer Systems (EPS) Division manufactures engineered degradable Thermoplastic materials which can be used in many types of completion tools that traditionally use non-degradable elastomers. Parker EPS’s high-grade thermoplastic materials have increased physical properties over conventional elastomers making it ideal for both high pressure/high temperature and wear-resistant applications. The increased physical properties of EPS thermoplastics provide enhanced resistance to extrusion, temperature and wear over most degradable non-metallics in the market. These unique thermoplastic materials may be manufactured in both homogenous as well as bonded components such as packers, Parker back-up rings, frac plugs, and liner wipers and are ideal for hot trouble well applications.

 

 

With a wide range of wellbore temperatures and completion fluids seen across the industry, selecting the right degradable compound can be complicated. Whether full degradation is needed in hours, days or weeks, Parker’s in-house testing capabilities and material development chemists can assist in recommending the proper parameters for the use of degradable elastomers in your application. For more information, or to discuss your project needs with a Parker engineer, contact us or visit us at our Oil and Gas webpage.

 

This article was written in collaboration and contributed by:

 

Degradable Materials Simplify Well Completions in Oil & Gas Extraction-Jacob Ballard, research and development engineer, Parker O-Ring & Engineered Seals DivisionJacob Ballard, research and development engineer, Parker Hannifin O-Ring & Engineered Seals Division

 

 

 

 

Degradable Materials Simplify Well Completions in Oil & Gas Extraction-Jason Fairbanks, business development engineer, Parker Engineered Polymer SystemsJason Fairbanks, market manager, Parker Hannifin Engineered Polymer Systems Division

 

 

 

 

Nathaniel Sowder, business development manager, Parker O-Ring & Engineered Seals DivisionNathaniel Sowder, business development engineer, Parker Hannifin O-Ring & Engineered Seals Division

 

 

 

 

 

Innovative Dissolvable and Degradable Materials Optimize Oil and Gas Extraction

Custom Designed Packing Elements for the Most Challenging Applications

Advanced Material Development for High-Pressure/High-Temperature Oil & Gas Extraction

 

 

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Degradable Materials Simplify Well Completions in Oil & Gas Extraction


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha