Sealing Shielding

Design Decisions Relating to EMC Shielding

Design Decisions Relating to EMC Shielding, Extruded EMI Gaskets, Parker Chomerics DivisionWhen approaching the problem of electromagnetic compatibility (EMC) the electronic design engineer quite often considers it to be a secondary issue that can be dealt with once the device is working and, after all, it can be dealt with by putting a metal box around it!

Mechanical engineers who have to address the issue, however, are faced with constraints such as weight, cost, environmental performance, and corrosion. So, unless both the electronics and mechanical engineers have up front visibility of each other's requirements, cost and time delays will be inevitable.

 

EMC sealing arrangement 

Let's consider the problem of an EMC sealing arrangement required to provide an IP67 seal on a box that is likely to be in a marine environment. The cabinet is to be made of aluminium alloy; the treatment is to be defined and the seal is made using O-rings in a groove and a cover which is to be bolted in position. Whilst the enclosure will not be on deck — and therefore not exposed directly to the sea - it will have to contend with difficult conditions. The cabinet is not to be opened often but should be easy to operate.

Traditionally, the solution would have been a gasket in a groove or even two, with the outer seal being a non-conductive rubber environmental gasket and the inner a conductive metal or metal filled rubber conductive gasket such as the CHO-SEAL type.Design Decisions Relating to EMC Shielding - Environmental gasket and conductive gasket - Parker Chomerics

 

The arrangement, shown in Figure 1 which provides flexibility and robustness, has been the starting point for most environmental and EMC designs. The downside is the cost of the machining and the fact that it takes up a relatively large amount of space. If space is in short supply, the EMC seal is often required to handle the environmental issues.

This sort of solution has the advantage of requiring less machining, fewer parts and the gasket can be conductive on the inside and non-conductive on the outside. The disadvantage is that a dual material gasket such as the Parker Chomerics co-extruded elastomers as shown in Figure 2, or dual moulded materials can be expensive.

Design Decisions Relating to EMC Shielding - non conductive and conductive gaskets

                                                                                                                                      

Even this solution may be required to reduce weight size and cost further, so we progress to small dispensed gaskets such as CHOFORM® located on a shoulder, which take up less than a quarter of the space required by the double O-ring solution while being asked to perform practically the same job. At this point, there is no non-conductive barrier between the EMC gasket and the environment. This immediately puts the gasket at risk of galvanic corrosion unless precautions are taken.

It can be seen from Figure 3 that the progression from what may have been a solution involving a wall thickness of around 12mm has been reduced to something that approaches 3mm or less with the resultant weight and cost savings. However, this comes at the expense of having to ensure better tolerances and flatness on the metalwork along with the possible risk of corrosion to both the cover and housing.

Design Decisions Relating to EMC Shielding - dispensed conductive gasket - Parker Chomerics

These problems can be mitigated by using a protective conversion coating on the metalwork and careful choice of the conductive fillers within the seal matrix to match the galvanic potentials of the interfaces as closely as possible. There is also the possibility of placing a similarly dispensed nonconductive bead outside of the EMI seal.

All of the solutions for the enclosure outlined above use a groove or a recess into or onto which the gasket is placed - primarily to ensure metal-metal contact and to provide a positive compression stop for the gasket. Even a groove is not always possible, some form of compression limiter is necessary in most cases. Using the gasket as the only electrical contact between the surfaces is not desirable.

While the arrangement can give satisfactory results and is sometimes the only option, it does mean that limited use is being made of the shielding that is inherent in the metal of the enclosure. This can provide 20dB or more of attenuation without an EMC gasket, depending on the design of the metalwork and the frequencies involved.

Remember that EMC gasketing is designed primarily for maintaining the continuity of the shield or Faraday cage around the device to be shielded. All other functions are secondary and may require the use of a specific seal.

 

Material, finishes, and corrosion

In the example of the aluminium box, the first problem is which aluminium alloy or other material you should use. This often is constrained by how you intend to make your box and cover.

In the case of a fairly small box, it's possible to machine the cover and the enclosure from a solid block. In this case, a broad grade of aluminium alloy can be used. But not all types of aluminium are suitable for surface finishing treatments and they have significantly different physical properties and corrosion resistance. Typically for marine environments, a 5000 series or 6000 series (Aluminium Association designations) alloy would normally be considered along with a trivalent chromate conversion coating (hexavalent versions whilst still available, are non-preferred due to health and environmental concerns). The type and class of the conversion coating then need to be specified: Mil-DTL-5541 and BS2437:2002 relate here.

Alternatively, the aluminium can be plated. This brings the possibility of galvanically matching the conductive material in the gasket. This is not always necessary but is desirable in cases where electrolytic contamination (salt fog) is likely.

This is because the electrolyte and the different metals form a galvanic cell, with the less noble metal - normally the aluminium structure — corroding or being damaged.

Design Decisions Relating to EMC Shielding, Corroded Aluminum Housing

If the galvanic potentials of the metals are matched as closely as possible - a difference of 0.5V or less is recommended, preferably approaching 0.25V - corrosion in the target environment can be eliminated or minimised.

Unfortunately, when it comes to aluminium, matching the galvanic potential with conductive gasketing materials is difficult and requires an additional coating/plating to resolve the issue.

Nickel plate or a silver or copper based paint are typical finishes but these finishes also have their own issues; if damaged or applied improperly, they can accelerate the rate of corrosion.

Design Decisions Relating to EMC Shielding, CHO-SHIELD 2001

 

Mechanical designers can ensure the reliability and performance of EMI seal

Therefore, if mechanical designers are to ensure the reliability and performance of the EMI seal, they need to take into account the nature of the enclosure material, the types of protective finishes and the nature of the gasket material, as well as the environment, operating conditions, expected life and the level of shielding required.

If the correct choices are made at the outset of the project, they can reduce the time taken for approval of the final product and reduce overall costs, while ensuring the product meets the design criteria.

The wide range of gasket materials available from shielding companies such as Parker Chomerics, along with recent developments such as the sheet and fabricated parts using  CHO-SEAL 6502 and 6503  elastomers, has improved the options for the designer. However, with ever-increasing frequencies and the tendency for lighter, thinner and lower power devices mean that EMI shielding for electronic devices will continue to be a challenge for the foreseeable future.

 

Design Decisions Relating to EMC Shielding

 

Article contributed by Gerard Young, AMIMechE MIEEE, applications engineering team leader, Parker Hannifin, Chomerics Division Europe. This was originally published in Markt&Tecnik

 

 

 

Related content: 

New Essential Handbook for EMI Shielding Applications

Top Three Design Tips for Corrosion Resistant EMI Protection

EMI Shielding Caulk Delivers Superior Performance in Military Radar Systems

Have a question about Parker products or services? We can help: Contact Us!

Comments for Design Decisions Relating to EMC Shielding


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha