Fluid Gas Handling

Dust is More Damaging Than You Think

Equipment in the field, including mining and construction, is subject to any number of conditions, from pouring rain to damaging winds, but dust is one factor that could be more damaging than you think.

 

Restricting airflow

Surprisingly, airflow is one of the chief concerns when it comes to dust accumulation. As filters and ventilation systems collect dust, airflow is reduced, which can cause equipment to overheat and malfunction or prematurely break down. When you think about how many electrical systems and mechanical components that require consistent air movement, you can imagine the numerous opportunities for breakdown within a single machine.

Preventing unplanned downtime and avoiding unnecessary replacement costs can be possible with predictive maintenance, for example changing air filters and cleaning cooling air intake and exhaust ducting. Inspections and regularly scheduled maintenance are also good practices, but employing a more strategic maintenance schedule is even better.

Monitoring the temperature of your asset alerts you to damaging temperature changes. It also provides analytics to help you identify temperature trends and address them as needed, reducing unnecessary maintenance routines.

 

Dust and moisture – the dynamic downtime duo

Even when an asset isn’t directly affected by water, moisture is still present in the air and will be absorbed by dust, making it more likely to adhere to surfaces.

As dust finds its way into an asset’s overlooked nooks and crannies, as well as cooling fans, the moisture it absorbs corrodes internal components and circuitry, leading to more problems that are difficult to diagnose. Dust and moisture can also lead to:

  • Inefficient operation and breakdowns

  • False/inaccurate readings from monitoring processes

  • Loss of structural integrity due to corrosion

As with temperature, an advanced condition monitoring solution provides maintenance managers with analytics to identify steady or sudden increases in humidity that promote dust/moisture buildup within components.

 

The good news

Dust is More Damaging Than You Think - SensoNODE and SCOUT Software image - Parker Hannifin Predictive maintenance does not require a specialist. With the right solution in place, managers and maintenance staff can easily employ a condition monitoring strategy that reduces downtime and minimizes unnecessary maintenance costs. The Internet of Things (IoT) has made this even simpler by creating a foundation for Internet-based solutions that track large amounts of data with ease.

Parker has successfully launched such a solution: SensoNODE™ Blue Sensors and Voice of the Machine™ Mobile software. When used in tandem, SensoNODE Sensors track an asset’s temperature, pressure, vibration and humidity, and transmit the data wirelessly to the Voice of the Machine Mobile App. This gives users real-time and historic trends and easy-to-understand analyses of their asset conditions to help address dust-related issues before they escalate.

To learn more about condition monitoring click here

 

 

 

 

Dust is More Damaging Than You Think - Westin Siemsglusz - Product Sales Manager for SensoNODE Parker Hannifin Article contributed by Westin Siemsglusz, IoT market sales manager, Parker Hannifin.

 

 

 

 

 

Additional info on condition monitoring:

Effective Predictive Maintenance of Rotary Machines

Effective Predictive Maintenance of Rotary Machines

Wireless Transmission of Performance Data Extends Equipment Life

Improve Solar Panel Maintenance and Condition Monitoring Efficiency

Streamline Your Condition Monitoring Process

IIoT Drives New Opportunities in Condition Monitoring

 

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Dust is More Damaging Than You Think

Dale Constantine
"Predictive maintenance does not require a specialist" Really hmmmmmm. Mobile has been without them forever and look where it has gotten us. Oil changes at 250 hrs, overhauling engines at 10,000 hrs, chasing failure after failure!

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha