Bioprocess Pharmaceutical Filtration

Effective Filtration of Biopharmaceutical Buffers

Effective Filtration of Biopharmaceutical Buffers - Buffer Filtration Schematic - Parker domnick hunter - Bioprocessing and Pharmaceutical FiltrationBuffers are used throughout the production of pharmaceuticals and buffer filtration is essential in protecting downstream chromatography and ultrafiltration equipment, controlling bioburden throughout the process and maintaining an endotoxin-free final product.

 

Growing pressure to decrease production time and increase throughput means the optimization of buffer filtration stages has never been more important.

 

PES membrane is recognized as having exceptional flux rates compared to alternative membranes such as PVDF, as well as being more chemical-resistant.

 

 

Parker domnick hunter supplies a choice of PES-based filters – the PROPOR range - for bioburden reduction or assurance of sterility, which can be used for a wide range of buffers, including difficult to filter buffers such as 6M urea.

The PROPOR range of filters provide a more efficient, cost-effective system.

 

Benefits of the PROPOR range

  • Using a filter from the PROPOR range speeds up filtration time by up to 40%, meaning more batches can be processed per day, relieving the bottleneck that often occurs in the buffer preparation area.
  • The range can provide a smaller system size, reducing the cost per batch.
  • The PROPOR range has been shown to outperform its competitors in filtering a wide range of common buffers, including those which are more difficult to filter, such as 6M urea.

 

Standard sterilizing grade filtration

  • PROPOR SG single layer 0.2 micron filters are configured for maximum flow rates and assured sterility 
  • For standard buffers requiring sterility such as those used as fermenter additions or in final product formulations, PROPOR SG offers reduced batch processing time.

 

Bioburden reduction filtration

  • PROPOR BR 0.2 micron filters deliver bioburden reductions of >log5 and incorporate an integral depth prefilter layer to extend filter life under high precipitate loading.
  • PROPOR BR filters are ideal for buffers used in applications that only require bioburden reduction such as chromatography and diafiltration.

 

Sterilization of difficult to filter buffers

  • PROPOR HC dual layer 0.2 micron filters maximize throughput to ensure sterility of more difficult to filter buffers
  • The highly asymmetric PES prefilter layer provides up to 10 times improvement in capacity compared to single layer membrane filters.

 

Reducing filtration system size

Tests have been completed on competing sterilizing-grade PES membrane products using a standard range of buffers. Results show that significant benefits can be achieved using the PROPOR range.

 

Buffers chosen for test were:

  • 1M hydrochloric acid (pH=1)
  • 1M sodium hydroxide (pH=13)
  • 50mM tris-buffered saline (pH=8)
  • 10mM phosphate-buffered saline (pH=7)
  • 50mM phosphate-citrate buffer (pH=5)
  • 0.1M acetic acid
  • 10% ethanol
  • 6M Urea

 

Effective Filtration of Biopharmaceutical Buffers - Parker domnick hunter - Bioprocessing and Pharmaceutical Filtration - Comparative Performance Graph

 

Effective Filtration of Biopharmaceutical Buffers - Parker domnick hunter - Bioprocessing and Pharmaceutical Filtration - Key Specification Requirements Diagram

 

Effective Filtration of Biopharmaceutical Buffers - Buffer Filtration Schematic - Andrew Kelly, Filtration Product Manager - Parker domnick hunter - Bioprocessing and Pharmaceutical Filtration

This post was contributed by Andrew Kelly, Filtration Product Manager (Life Sciences), Parker domnick hunter Process Filtration, UK.

Email: dhprocessinfo@parker.com

 

 

 

 

Find out more about Parker domnick hunter's solutions for buffer preparation and storage.

 

 

Related Blog Posts

What is Sterilizing Filtration and Why is it Important?

How to Select the Right Filter for Your Bioprocess

A Case Study for Collaborative Filter Product Development

The Role of Prefiltration in the Optimization of Bioprocess Filtration Systems

Why You Should Consider Hollow Fibres for Ultrafiltration

Best Practices for Developing Single-Use TFF Steps

 

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Effective Filtration of Biopharmaceutical Buffers


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha