Over the last few years there has been a significant increase in
the popularity of electric cars. These vehicles are efficient,
silent and do not pollute the air (at least where they are driven).
In...
Posted On 03/29/2021
Read More ►
With the increased emphasis to reduce emissions, air pollution,
resource waste, and traffic noise, government legislation is
pushing towards the use of electric power to drive ancillaries in
work...
Posted On 03/09/2021
Read More ►
As the wheel loader is the stalwart of the construction site,
equipment manufacturers know that technological advances are
important in their customers' buying decisions. Add in the
stringent...
Posted On 01/30/2021
Read More ►
The evolution and refinement of the hydraulic excavator’s design
have been constant, with today’s
models incorporating electrification, hydraulic
technology, and machine analytics; which all...
Posted On 01/30/2021
Read More ►
Looking for efficiency and reliability as well as peak power for
on-highway and off-highway vehicles, both electric and hybrid?
Comparison analysis and 135 million road miles logged have shown
that...
Posted On 01/26/2021
Read More ►
Sewing may not be widely regarded as glamorous, but it is literally
what holds the very fabric of society together. All of the clothing
we wear can be found to contain neat stitching, but have you...
Posted On 01/05/2021
Read More ►
Electrification remains one of the primary trends in the automotive
sector, as vehicle makers push hard to introduce cleaner
technologies that result in lower emissions. According to a recent
report...
Posted On 11/23/2020
Read More ►
Many industries are now being required to drastically reduce carbon
emissions as a consequence of rising global temperatures, and
the automotive industry in particular is a focus of much
regulatory...
Posted On 09/23/2020
Read More ►
Motors and sensors go hand in hand. The EX range of motors already
feature a wide range of sensors that deliver feedback on various
parameters and, now, Parker has added a HIPERFACE DSL® encoder...
Posted On 07/30/2020
Read More ►
Thanks to our loyal followers for all of the interest in the topics
covered in this blog over the past year. In examining the most-read
blog posts over the course of 2019, it becomes obvious that...
Posted On 01/14/2020
Read More ►
This is the final of a three-part series that spoke to the various
feedback devices that are provided as options on Parker Servo
Motors. Part 1 & Part 2 provided the basic theory of operation
for the...
Posted On 07/31/2019
Read More ►
Although the basic recipe for the solid soap bar has not varied
much for decades, the process of making this basic commodity has
changed significantly since the advent of industrialisation....
Posted On 02/01/2019
Read More ►
Throughout the world, various types of metrology applications share
a common need for increased precision. Metrology is the scientific
study of measurement. Metrology applications take some type...
Posted On 10/11/2018
Read More ►
When it comes to gearbox test rigs deployed in the automotive and
aerospace industries, one thing is certain - there is no margin for
failure. A test rig or system that is unreliable or...
Posted On 09/24/2018
Read More ►
Modern Swiss-type lathes have evolved from simple screw machines to
high-precision, high-production machines and are now widely used
across many industries to completely machine small parts, even...
Posted On 07/24/2018
Read More ►
Hazardous locations are operating environments in which explosive
or ignitable vapors or dust are present, or are likely to become
present. It is normal for various processing applications where
gas,...
Posted On 05/02/2018
Read More ►
The automotive vehicle industry has experienced introductions of
several new technologies and upgrades. One significant example is
the rising amount of electrical content per vehicle. Testing...
Posted On 04/19/2018
Read More ►
With its high power density and flexible mounting capabilities,
permanent magnet direct drive servo motors like the Parker PM-DD
series have a proven track record in many manufacturing
applications....
Posted On 01/10/2018
Read More ►
The basic theory of operation for brushless servo motors revolves
around the principles of magnetism where like poles repel and
opposite poles attract. There are two magnetic sources found within
a...
Posted On 10/05/2017
Read More ►
Most engineers recognize that gearheads can be used to create a
better inertia match between the object that is being moved and the
motor being driven. Put simply, it is dictated by the gearhead
ratio...
Posted On 06/08/2017
Read More ►