Sealing Shielding

Electromagnetic Compatibility in Next Gen Autonomous Vehicles

Electromagnetic Compatibility in Next Gen Autonomous Vehicles, Parker Chomerics, POWERING THE FUTURE OF EVs For more than 100 years, the car has simply been used as a device for transporting a driver and passengers from point A to point B at speed with minimum effort.  

With the introduction of Advanced Driver Assistance Systems (ADAS) and other semi-autonomous driving technologies, a different concept of the vehicle is emerging. In the future, the car will be a media playback center, telephone, office and extension of the home’s living room which also happens to be able to convey passengers from A to B.

This is having a profound effect on the characteristics and on the sheer number of electronics systems in new vehicles and this, in turn, will dramatically extend the demands on the EMI shielding devices used to attenuate the radiated emissions that could affect circuits in the car. EMI shielding materials will need to perform over a wide range of frequencies, in more applications as electronic systems take over more and more aspects of the car’s driving operations while adding as little as possible to the weight of the vehicle.   

The time for OEMs to consider the options for achieving EMC in new car designs is at the start of a new design project before the electrical and mechanical features of the vehicle’s systems have been decided. This gives design engineers the opportunity to bring considerations of EMI and shielding devices into the design process and enable optimization of the size, cost and performance of EMI shielding in the final system. 

Top challenges of next-generation 5G networks

  • The first challenge for automotive design engineers is the range of frequencies that need to be attenuated will be far greater in new cars than it was in the past. Until recently, the main frequencies of interest were the AM and FM bands used by radio and frequencies below 3GHz used by Bluetooth radio and mobile phone networks.
     

    With the future introduction of 5G mobile phone network coverage, frequency coverage of EMI shielding materials will need to be extended. A higher frequency range is not the only issue. Cars are also going to support a much greater number of wireless communications systems within the vehicle.

New strict measures to attenuate RF emissions in compliance with safety standards

  • The second challenge is that the effectiveness of EMI shielding is likely to be more tightly specified in the future as automotive manufacturers move towards a strict view of the functional safety of the electronics systems in cars, codified in the ISO 26262 functional safety standard.

    So, what does this mean for the specification of EMI shielding materials?

Continuous development of new elastomer fillers

Parker Chomerics maintains an intensive research and development program aimed at producing new filler materials for electrically conductive elastomer products. An important goal for this research program is to produce EMI gaskets that can cover the broader frequency range of interest in autonomous vehicles while maintaining the desired mechanical characteristics. Parker Chomerics CHO-SEAL conductive elastomers are widely used in automotive systems and offer useful properties, including resistance to high temperatures and contaminants, and the ability to provide environmental sealing to protect circuits from the ingress of liquids.

These elastomer gaskets resist compression set, accommodate low closure force, and help control air flow. They are available in standard sheet form, extruded or custom shapes. 

In addition, Parker Chomerics CHOFORM Form-In-Place automated EMI gasket material can be dispensed directly onto castings, machined metal and conductive plastic and is widely used in tightly packed electronic housings. This advanced technology allows dispensing of precise positioned gaskets in very small cross sections and can free up valuable packing space of up to 60%. CHOFORM offers excellent shielding effectiveness which exceeds 100dB between 200 MHz and 12GHz.

New opportunities for weight saving

The development of autonomous and semi-autonomous vehicles is leading to a huge increase in the number of electronics modules per vehicle. This increases the scope for car makers to reduce weight by replacing conventional metal housings with lighter conductive plastic housings. While the weight saving on each module might appear small, when multiplied across the 100 or more electronics modules, the total weight saving becomes invaluable.

Parker Chomerics PREMIER™ PBT-225 is a single-pellet conductive plastic for use in automotive housings. PREMIER PBT-225 offers excellent resistance to hydrolysis when exposed to extreme temperatures and provides for easy processing and uniform filler dispersion. As a result, EMI housings made from PBT-225 offer tightly controlled electrical and mechanical performance throughout complex geometries. A weight saving of 30% is also possible when replacing an equivalent metal or aluminum housing with PBT-225.

By collaborating early in development projects with Parker Chomerics, automotive system designers can ensure that their electronic and mechanical design is optimized for shielding purposes.

Learn more about Parker Chomerics EMI shielding and thermal solutions for the automotive Industry.

POWERING THE FUTURE OF EVs

 

 

 

 

 

 

 

Attending Electric & Hybrid Vehicle Technology Expo 2019?

The Electric & Hybrid Vehicle Technology Expo connects you with more than 8,000 automotive engineers and executives, and more than 600 leading suppliers, from across the H/EV manufacturing industry. A powerful end-to-end showcase, this mega event delivers up-to-the-minute insights on electric, hybrid, and plugin hybrid vehicle technology, along with the latest manufacturing solutions along the supply chain including electrical powertrains and components, battery management systems, materials and equipment. Discover everything you need to make faster, smarter, and more cost-effective products at the most comprehensive event in North America.

Visit Parker in Novi, MI, at booth 745 September 10 - 12th and learn how our engineering and materials expertise helps EV manufacturers produce the vehicles that consumers want at the scale needed.

 

Mel French 

 

This blog post was contributed by Mel French, marketing communications manager, Chomerics Division Europe. 

 

 

 

 

Related content:

Five Ways to Maximize Performance of Electric Vehicle Batteries

Design Decisions Relating to EMC Shielding

Improved EMI Shielding Consistency of Single Pellet Conductive Plastics

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Electromagnetic Compatibility in Next Gen Autonomous Vehicles


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha