EMI Shielding
Need Better Flow Rate Control? Look to THERM-A-GAP GEL 37
The demand for dispensing thermal interface material (TIM) has increased exponentially because dispensables offer engineers flexibility in the designs and patterns that can be applied to electronics...
Read More ►
Meeting NASA Low Outgassing Requirements in EMI Shielding Applications
Design factors for satellite, high altitude, and space-based applications vary dramatically from those of land or ship-based programs. These factors include: low payload capacity, low operating...
Read More ►
Critical Systems and Components for Ventilator Manufacturing
Today, the demand for life-saving ventilators is challenging medical equipment manufacturers’ production capacity and supply chains around the world to perform at levels well beyond...
Read More ►
Supporting Medical Device Manufacturing With Business Critical Parts
For medical device manufacturers, it is now more important than ever to operate at the highest capacity in order to increase the supply of essential equipment used for patient care.   COVID-19 is...
Read More ►
Chomerics Earns GM Supplier Quality Excellence Award for 3rd Year
We’re thrilled to announce the Chomerics Division of Parker Hannifin Corporation, the global leader in motion and control technologies, has been awarded the prestigious 2019 GM Global Supplier Quality...
Read More ►
What You Should Know About Electrically Conductive Elastomers
Electrically conductive elastomers are elastomeric polymers filled with metal particles. They can be grouped by filler type and elastomer type. Then within each of these classes, there are standard...
Read More ►
6 Tips When Selecting an Electrically Conductive Adhesive
There are many ways to improve the electrical continuity of electronic enclosures and the resultant EMC performance using a variety of electrically conductive gaskets and mechanical fasteners.  Such...
Read More ►
Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel
Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Read More ►
Managing EMI and Lightning Strike Protection in Today’s Aircraft
Composite materials have been replacing metal structures throughout the aircraft industry primarily to save weight, improve fuel economy and reduce costs.  But the lack of electrical conductivity in...
Read More ►
Form-In-Place Gaskets: What They Are and What They Are Not
Form-in-place EMI gaskets, also known as FIP EMI gaskets, is a robotically dispensed electromagnetic interference (EMI) shielding solution that is ideal for modern densely populated...
Read More ►
EMI and Environmental Sealing for Munitions Applications
Material selection for military applications requires careful consideration, as there are strict requirements to ensure maximum durability, security and of course performance. In munitions, or...
Read More ►
5 Design Considerations for EMI and Weather Sealing Combination Gaskets
Combination electromagnetic interference (EMI) shielding and weather gaskets, more commonly known as EMI shielded combo strip gaskets, are an excellent choice for a variety of applications that...
Read More ►
Discover a New Electrically Conductive Flame Retardant Plastic
Electrically conductive plastics continue to provide reliable EMI shielding in a wide variety of applications. Specifically, thermoplastics can overtake bulky metal enclosures due to their superior...
Read More ►
6 Benefits of Overmolded Covers for Aerospace and Defense Applications
It's no surprise that electronic enclosures and housings in aerospace and defense applications are built to meet the most stringent of military standards. These include but are not limited to...
Read More ►
Observations From the Electric & Hybrid Vehicle Technology Expo NA
Another Electric & Hybrid Vehicle Tech Expo North America has concluded and it is evident that this show has grown by leaps and bounds. In just a few years since Parker Hannifin has started...
Read More ►
Parker Chomerics Earns 2018 Outstanding Quality Supplier Award from FCA
We're thrilled to announce that the Chomerics Division of Parker Hannifin Corporation, the global leader in motion and control technologies, has been recognized for its outstanding quality by global...
Read More ►
Why You Should Single-Source EMI Shielding Materials
  EMI shielding of electronics using thermoplastic housings traditionally has been a complex and costly process. Today, OEMs not only have to meet form, fit and function requirements, but also must...
Read More ►
Can Electrical Resistance Be Used to Predict Shielding Effectiveness?
Conductive elastomer EMI shielding gaskets use metallic particles to create a conductive path and shield enclosures from electromagnetic radiation. A key measurement of these gaskets is Electrical...
Read More ►
How to Reduce Galvanic Corrosion Using Conductive Filler Systems
Galvanic corrosion (also known as bimetallic corrosion or dissimilar metal corrosion) is the breakdown of metallic surfaces as a result of the difference in electrical potential of adjacent metals and...
Read More ►
EMI Shielding Gaskets: Spliced Gaskets vs. Molded Gaskets
EMI shielding gaskets such as conductive elastomer gaskets come in many different materials and almost a limitless number of shapes and sizes. They are most commonly made of a base material...
Read More ►