Sealing Shielding

Engineered Materials and Sealing Solutions for Flow Batteries

Engineered Materials and Sealing Solutions for Flow Batteries, solar panels and windmills, O-Ring & Engineered Seals Division, Parker HannifinSealing can often be a frustrating challenge when dealing with flow batteries. Determining what materials are compatible with certain chemistries or developing a profile that provides optimal sealing under available compression can be a time-consuming task for those outside the sealing industry. A trial and error approach can have a significant overall cost impact through multiple prototype iterations, prolonged testing, and ultimately, delaying product commercialization. 

 

Specialized support

Parker’s design and material engineers can provide support to your team in the critical, early stages of product development. With hundreds of engineered elastomeric materials to choose from, our team can identify and recommend a compound that works with your specific electrolytes or other fluids. With the exceptionally long lifetime requirements of flow batteries, our homogeneous rubber provides the elasticity needed to handle the many charge-discharge cycles the battery will see in its life.

 

Engineered Materials and Sealing Solutions for Flow Batteries, Hollow O FEA on tablet, O-Ring & Engineered Seals Division, Parker HannifinFinite Element Analysis (FEA)

Our engineers can significantly reduce design time by utilizing finite element analysis early in the process. FEA is a sophisticated computer modeling program that demonstrates a visual simulation of how materials for a proposed seal design might perform in the application. Material performance over a range of conditions is tested to see if the product will perform as expected. FEA can be repeated as many times as needed to fine-tune the design and make the final product as robust, functional, and reliable as possible. This process can be performed before prototyping, mold design or production is undertaken, greatly reducing the possibility of errors or redesign issues occurring later.

 

Launch speed is critical

With continuous advancements materializing in the energy storage market, we fully understand the urgency of moving a product from development to commercialization. Parker can provide your team with resources to improve both the quality and speed of seal design in the critical prototyping stage, reducing overall cost.

After commercialization, Parker’s O-Ring & Engineered Seals Division can support your high volume production utilizing one of our 14 manufacturing locations dedicated to molding and extruding elastomeric products. To ensure the highest levels of material quality, state-of-the-art laboratories and testing equipment are housed in our two North American technology centers.

For more information, visit Parker O-Ring & Engineered Seals Division online and chat with our experienced applications engineers.

 

Wesley Burcham, Engineered Materials and Sealing Solutions for Flow Batteries

 

 

This article was contributed by Wesley Burcham, market managerParker O-Ring & Engineered Seals Division.

 

 

 

Related content:

Sealing Groove-less Applications with Flat Panel Gaskets

Sealing Fundamentals | How to Properly Install a Parker Hollow O-ring

Sealing for Harsh Environmental Conditions in Telecommunications Applications 

Environmental Seal Enclosure 101

Categories
Recent Posts by Author

Discover a New Electrically Conductive Flame Retardant Plastic

Electrically conductive plastics continue to provide reliable EMI shielding in a wide variety of applications. Specifically, thermoplastics can overtake bulky metal enclosures due to their superior...

Semiconductor Fabs Lower Cost of Ownership with HiFluor Materials

  In our July Semiconductor entry, we noted that lowering the cost of ownership is a multi-faceted goal. We discussed how one of the areas for potential improvement is mechanical design and how the...

6 Benefits of Overmolded Covers for Aerospace and Defense Applications

It's no surprise that electronic enclosures and housings in aerospace and defense applications are built to meet the most stringent of military standards. These include but are not limited to...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Engineered Materials and Sealing Solutions for Flow Batteries


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha