Fluid Gas Handling

Expanding Your Diagnostic Capabilities with Wireless Sensors

Expanding Your Diagnostic Capabilities - Asset Condition Monitoring Image - Parker SensoNODEWhen it comes to a successful predictive maintenance strategy, diagnostics is king. Being able to pull meaningful information from your assets allows you to detect patterns in their performance, so you can see where issues might be forming.

By monitoring and tracking an asset’s pressure, temperature, and humidity levels, users cover the three most important aspects of an effective predictive maintenance strategy:

  • Acquiring real-time and historical data trends of assets and processes
  • Detecting and diagnosing any issues that could snowball into problems
  • Delivering analytics and alerts to operators when needed

Ultimately, the goal is to minimize unplanned downtime and reduce repair costs by basing maintenance routines on what’s actually happening rather than reacting to unexpected events, or fixing problems that don’t exist. However, some assets can be more difficult to monitor than others.

Traditional diagnostic devices require additional wires and cables attached to power supplies and sensors. This sometimes prevents operators from running their assets while performing diagnostics, making for less-than-precise measurements. Also, because it takes time to set up the sensor and perform the diagnostics, measurements aren’t taken very often, offering just a snapshot of an asset’s conditions. 

Fortunately, the Internet of Things has opened the door to innovation, and Parker Hannifin has developed state-of-the-art solutions to help push the limits of your diagnostic capabilities into exciting new territory.

 

Making wireless diagnostics easier

Expanding Your Diagnostic Capabilities - Wireless Diagnostics Product Line - Parker Quick Coupling DivisionThe 4-20mA transmitter turns any 4-20mA sensor wireless, making it easier to monitor an asset without shutting it down. The transmitter can be mounted with either the magnetized base or the threaded stud port.

Soft, thin, and conformable, the SensoNODE flexible displacement sensor takes accurate measurements and readings while being strained over 100% for millions of cycles. Made with the durable electroactive polymer technology (EAP), the sensors can withstand the harshest environments.

The new wireless ServiceJunior™ CONNECT digital pressure sensor features min/max memory capability and graphic display. Its 10ms scan rate provides increased accuracy and faster frequencies to diagnostics.

Tired of replacing batteries? The new wired power supply lets you power wireless sensors from a standard wall outlet for a continuous power source.

A new vacuum sensor monitors expanding pressure ranges and is ideal for vacuum pump monitoring and detecting system leaks. We’ve also introduced two new temperature sensors to better accommodate specific applications: The foot sensor makes it easier to monitor the temperature of your pipes and hoses, while the probe sensor is perfect for injection molding applications.

 

Learn More

To learn more about Parker's condition monitoring product solutions and to see which is best for your application, visit our website

Find a distributor 

 

Expanding Your Diagnostic Capabilities - Dan Davis Product Manager - Parker Hannifin SensoNODEThis post was contributed by Dan Davis, product sales manager, SensoNODE Sensors and SCOUT Software, Parker Hannifin.

 

 

 

 

 

Related posts: 

Turn any Wired Sensor into a Wireless Device with a 4-20mA Transmitter

Parker’s Most Powerful Diagnostic Tool is Now Wireless 

Wireless Transmission of Performance Data Extends Equipment Life

How to Easily Connect Users to the Digital Plant 

Size Matters: Small, Wireless Sensors Make Diagnostic Efforts Easier for Mobile Equipment 

Condition Monitoring Solutions for Power Generation Plants

Expanded SensoNODE™ Line Launched at Sensors Midwest Conference

Categories
Recent Posts by Author

Install Transair Push to Connect Fittings In 7 Easy Steps

Push to connect fittings have grown in popularity due to their ability to efficiently couple fittings to thermoplastic tubing while maintaining performance. Invented in 1969, push-to-connect fittings...

Choosing a Solenoid Valve for Applications Requiring Extreme Performance

Today's state-of-the-art laboratory and medical instruments are smaller, more accurate and higher performing. Many applications, such as those in analytical chemistry (mass spectrometry and...

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Expanding Your Diagnostic Capabilities with Wireless Sensors


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha