Advanced compounds extend downhole drilling time. Hydrogenated acrylonitrile butadiene (HNBR) compounds have been developed specifically for downhole mud motor boots. These compounds offer improved mechanical properties, toughness, and fluid resistance leading to extended drill time. See the physical properties listed in the graph below for the HNBR compounds KA261-60, KA271-70, KA281-80, and KB282-80 that Parker has to offer.

Mud motor boots must perform in harsh environments of drilling fluids and high temperatures without failure, in order to protect the drill string. Boots must operate in a vast array of water and oil-based muds specifically formulated to enhance drilling productivity, often at the expense of rubber articles. Specific compounding is required to overcome these obstacles. Downhole temperatures during mud circulation can exceed 300˚F, placing additional stress on the boot. Debris contained in the mud is circulated at high flow rates which can abrade the boot surface, leading to premature failure of the rubber. Operation of the drill string places the boots under severe mechanical loads causing flex and torsional fatigue. Customer feedback has shown that competitive mud motor boots experience field issues, which has driven Parker to the development of new compounds for the market.

Parker benchmarked industry standard boots using downhole muds and high-temperature mechanical properties to validate its newly developed HNBR compounds. The compounds have been evaluated at 350˚F and show performance enhancements over competitive boot compounds. While testing in drilling mud procured from the drilling site, it was determined that the current rubber boots were undergoing chemical degradation leading to premature failure. Parker’s expertise in material compounding overcame the fluid resistance barrier to produce a material that extends the drilling time available. Field testing of the new boots reduced the failure rate to zero.
Take a look at the latest Mud Motor Boot bulletin to learn how Parker partners with its customers in the oil and gas industry to maximize safety, efficiency and profitability.
Additional information
Parker is leveraging a century of engineering expertise to help its partners in the onshore and offshore oil and gas industry increase performance, improve safety and eliminate unplanned downtime. Learn more by visiting our Oil and Gas solutions page.

This article was contributed by Ericka Norris, market manager, Parker O-Ring & Engineered Seals Division.
Related content:
Advanced Material Development for High-Pressure/High-Temperature Oil & Gas Extraction
Do Your Seals Meet the Demands of the Oil and Gas Industry?
Mud Logging Gas Analysis: Using Hydrogen to Determine Total Organic Content of Samples
Have a question about Parker products or services? We can help: Contact Us!
Comments for Extend Downhole Drilling Time with Mud Motor Boot Sealing Technology
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.