Filtration

Extending Dust Collector Cartridge Filter Life in Metalworking Applications

Extending Dust Collector Filter Life in Metalworking Applications - Metalworking application - Parker HannifinThe amount of dust created in metalworking applications calls for plant engineers and maintenance managers to make careful selections in their mitigation measures and equipment. While dust collectors are carefully engineered to handle the load, they are often overcome as production expands. In bronze manufacturing, for example, there is a strong need to find ways to extend filter life due to the high quantities of the dust generated in zinc processing operations. Here, we will examine how one company resolved an issue with premature binding of paper filter media.

 

The challenge

In the processing of zinc, a sticky, highly binding dust is created. A dust collector in operation at a bronze manufacturing facility offered a reasonable 2” differential pressure when it was first installed. Soon after installation, however, the pressure drop increased to over 5” and in a three month period, surpassed the 8” mark. The plant maintenance team investigated and determined that the increase in pressure drop was caused by an acute binding effect. The paper filter media used in the dust collector was clogged with a heavy conglomeration of dust created during processing resulting in:

  • Slow production.
  • Replacement of over 100 costly filter cartridges every 3 months.
  • An inability to keep up with customer demand. 

 

Extending Dust Collector Cartridge Filter Life in Metalworking Applications - download the case study - Parker Hannifin

 

To learn more, download the full case study "BHA® Spunbond Cartridges & BHA Neutralite® SR Conditioning Agent extends filter life at Bronze Manufacturer"

 

 

 

 

The solution

The manufacturer turned to Parker for a solution. Parker’s experienced filtration engineers reviewed the situation carefully and made the recommendation of replacing the paper media with BHA®  Spunbond Polyester Cartridges. In addition, Parker recommended the initial, then daily application of BHA® Neutralite SR Spark Resistant Conditioning Agent. 

 

BHA® Neutralite SR

Extending Dust Collector Filter Life in Metalworking Applications - Neutralite SR - Parker HannifinNeutralite SR is a light-density, neutral aluminum silicate powder that extinguishes hot sparks on contact before they can damage filters. The powder consists of microscopic particles of varying shapes. When injected into a baghouse, it creates a porous dustcake layer on the outer surface of the filter bags that increases filtering efficiency, improves airflow, and absorbs moisture and hydrocarbons.

 

BHA®  Spunbond Polyester Cartridges

Extending Dust Collector Filter Life in Metalworking Applications - spunbound polyester cartrdges - Parker HannifinIdeal for industrial applications like metalworking, spunbond polyester is a synthetic media that has similar filtration efficiencies to cellulose. It’s strong, more resistant to abrasion and moisture, and it has a better life cycle. It carries an average MERV rating of 10 and a MERV rating of 15 with nanofibers applied to the surface. With an ePTFE membrane applied to the surface of the base media, it has a MERV rating of 16+. The temperature rating is 265F, continuous.

To test the effectiveness of the recommendation, the Parker BHA® Spunbond Cartridges and Neutralite SR treatment were installed to run a side by side comparison with the paper cartridges.

 

 

Results

  • Filter life was extended by more than two times, decreasing the need for costly baghouse change-outs.
  • Differential pressure remained consistent.
  • Production increased and maintenance was reduced by 50%.
  • After four months of testing, the paper filters were plugged and needed to be replaced, whereas the BHA® Spunbond Polyester Cartridges looked brand new.

 

Conclusion

The dust created in metalworking applications can be extensive and cause delayed or lost production and costly maintenance. Choosing high-quality filtration equipment, like BHA® Spunbond Cartridges, can prevent premature filter binding, extend the life of baghouse filters and reduce downtime and expensive maintenance. 

 

Extending Dust Collector Cartridge Filter Life in Metalworking Applications - download the case study - Parker HannifinThis article was based on the case study "BHA® Spunbond Cartridges & BHA Neutralite® SR Conditioning Agent extends filter life at Bronze Manufacturer", download a copy for your reference

 

This blog was contributed by the Industrial Gas Filtration and Generation Division Team.

 

Related content

Defining Our Unique Contribution to the World

Choosing the Best Dust Collector for Air Quality Control in Manufacturing

How to Solve Baghouse Airflow Restriction in Foundry Applications

Filter Upgrade Improves Baghouse Performance in Industrial Manufacturing

Foundry Eliminates Shutdowns and Extends Baghouse Filter Life

BHA® Pleated Filter Elements Improve Dust Collection for the Foundry Industry

Have a question about Parker products or services? We can help: Contact Us!

Comments for Extending Dust Collector Cartridge Filter Life in Metalworking Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha