With its high power density and flexible mounting capabilities, permanent magnet direct drive servo motors like the Parker PM-DD series have a proven track record in many manufacturing applications. Let's take a look at five successes spanning various industries.
As the world's communications infrastructure continues to grow and evolve, the demand for fiber optic cable has been increasing. With Parker distributor Cross Automation in Charlotte NC, we were able to provide PM-DD motors for a vertical lathe, used to dispense glass for fiber optic wiring. The combination of smooth low-speed operation, compactness, and the ability to mount directly to the rotating shaft made the PM-DD a winner over standard servo motors.
Machine tools demand accuracy, and in the second case study, the task at hand was to repeatedly index a table that was three feet in diameter. With displacement occurring 1.5 feet (457 mm) away from the motor centerline, its high resolution (20 bit) absolute encoder was critical to the application. Thanks to the PM-DD's high load carry bearings, (1500 N in this case) where previously a conventional servo motor and worm gear solution was used, the PM-DD proved to do the job while eliminating the worm gear. The drive train was simplified and ongoing maintenance associated with the mechanical gearing was eliminated. This solution was sold by Faber Associates, a Parker distributor based in Clifton NJ.
Automotive assembly is a rigorous application with hundreds of interdependent operations, all of which must function reliably, at the risk of costly downtime. A rotary table was used in the operation of adjusting vehicle headlights. Simplicity and high positioning resolution were the main factors leading to the adoption of the PM-DD in an application solved by Parker distributor Reco-Wesco from Indianapolis. Being able to mount the motor directly to the table eliminated the need for multiple mechanical components that would have required maintenance and been a potential failure mode.
Automotive industry testing applications often duplicate real-life scenarios that the finished vehicles will be exposed to, but must take into account the worst-case situations. In this case, the PM-DD motor was used for an electronics test bench. As part of a multi-axis assembly, the test bench would simulate the rough vehicle road conditions, including a rollover, that the electronics might be subjected to. PM-DD was preferred over a standard servo motor due to its smooth, slow speed, operation, good bearing support, and high torque. This solution was sold by Parker distributor RSA of Fond du Lac WI.
The fifth and final application was in the life sciences field. A PM-DD motor was used for an indexing table that carried five stations to support the assembly of medical devices. The first station was to load the part, the second applied adhesive, the third was for UV curing of the adhesive, the fourth was inspection and the fifth was where the part was unloaded. In this case, the PM-DD replaced a pneumatic indexing table. Key to its success was a smooth start and stop operation versus the previous pneumatic solution. Also, the PM-DD with Parker P-Series Drive allowed for a variety of indexing locations to be programmed providing more flexibility than a more traditional rotary indexing table. This solution was provided by Automation Incorporated, a Parker distributor out of Minneapolis MN.
Learn more about the PM-DD by visiting our Precision Direct Drive Rotary Servo Motor Series Product webpage to buy or download a Parker P series
Direct Drive Rotary Motors catalog.
Article contributed by Jeff Nazzaro, gearhead and motor product manager, Electromechanical & Drives Division, Parker Hannifin Corporation.
Related posts:
A Quick Guide: How Servo Motors Work
Tube Bending OEMs Embracing All-Electric Automation
Linear Motors | Servo Drives | PAC and More: SLAS 2016 Featured Products
Have a question about Parker products or services? We can help: Contact Us!
Comments for Five Great Applications for Permanent Magnet Direct Drive Servo Motors
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.