Hydraulics

Flow Force is Essential for Proper Cartridge Valve Function

Flow Force is Essential for Proper Cartridge Valve Function Mini Excavator Hydraulic Cartridge SystemsOften times hydraulic components can begin to act differently or unpredictably when the conditions of the hydraulic system change from the expected. In some cases, when the hydraulic flow is either lower or higher than anticipated, the valves will not perform as they were designed. Cartridge valves are no exception and can sometimes be even more sensitive to altered flow rates when compared to many other hydraulic components, specifically when it comes to high flow rates due to the nature of their compact design.

 

Applying the science

The reason why high flows can affect valves can be attributed to simple physics. The higher the flow rate, the greater the forces the hydraulic oil has on the internal components of the valve. This phenomenon is simply known as flow forces. When you think of a firefighter's hose or garden hose without water flowing through it, it is very flexible and easy to move, however, when water is flowing through at the full rate, the hose naturally begins to straighten out and becomes more difficult to maneuver. This is due to the flow forces from the water acting upon the internal sidewalls of the hose. Similarly, the hydraulic oil inside the valve will act upon all the different surfaces of the spool, sleeves, poppets, and other components with forces that are proportional to the surface area of those components that encounter the hydraulic oil flow.

 

Explanation

What begins to happen in these circumstances is because of the high flow rates, or flow rates that the valve is not designed or tested for, the valve can either become stuck in its current position unable to be shifted, or the opposite will occur where the valve unexpectedly shifts without the intention to. For this reason, it is imperative that hydraulic system designers and operators follow the manufacturer's recommendation for valve flow ratings. The combination of hydraulic oil flow and pressure strikes a critical balance for valve performance and must be adhered to achieve proper functionality.

 

Flow Force is Essential for Proper Cartridge Valve Function Flow Force Hydraulic Cartridge Systems

Image 1: Casoli, P., Vacca, A., Franzoni, G., 2003, A numerical model for simulation of “load-sensing” spool valves, The 18th International Conference on Hydraulics and Pneumatics, Prague, Czech Republic, September 30 – October 1, 2003

 

Solution

Parker Hydraulic Cartridge System Division’s valve collection is ideal for consumers due to the wide selection of cartridge style valves with a wide range of flow and pressure capabilities. Additionally, HCS’s cartridge technology features low-pressure drops, which correlates with lower internal flow forces, making Parker’s cartridge technology easier to work with, perform more predictably and reliably, and able to use in a wider variety of hydraulic system applications.

For more information on Parker's cartridge valves, contact us.
 

Flow Force is Essential for Proper Cartridge Valve Function - IFPE - ParkerTo learn more about Parker’s off-road machinery solutions stop by Booth #S80245 at IFPE/CONEXPO-Con/AGG in Las Vegas March 10 – 14.

 

Flow Force is Essential for Proper Cartridge Valve Function Stephen BruntonArticle contributed by Stephen Brunton, product manager, Hydraulic Cartridge Systems Division. 

 

 

 

 

 

Related articles:

Unique Valves Manage Flow Better in Construction Equipment

Three Ways to Improve the Operation of Your Proportional Valve

 

Categories
Recent Posts by Author

Hydraulic Pump and Motor Combination Packs Power on Rayco Stump Cutter

Following new, more stringent Tier IV diesel engine emissions regulations, Rayco, an environmental equipment designer for the tree care and landscape industries, took the opportunity to develop a more...

Sprayer Steers Clear of the Ordinary

Traditionally, agricultural sprayer machines were custom-built on a four-wheel chassis. These custom-built units were heavy, expensive and not easily adapted to other farm applications. Sprayers...

Power Shift Power Take-Off (PTO) Troubleshooting

Parker Chelsea’s Power Take-Off (PTO) is designed and built to meet the demands of the mobile equipment industry. The Chelsea PTO is intended to provide a long service life, both on-highway...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Flow Force is Essential for Proper Cartridge Valve Function


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha