Fluid Gas Handling

Fluidic Components Take the Pain Out of Designing Capnography Monitors

Fluidic Components Take the Pain Out of Designing Capnography Monitors - Sidestream Capnography Application - Parker Precision Fluidics DivisionTo meet the needs of today's ever-changing hospital environments, medical equipment manufacturers are under pressure to design smaller, lighter and more portable devices without compromising functionality. Medical device engineers are challenged with integrating components that meet design specifications, yet also deliver the high performance expected for critical applications.

A capnography monitor, for example, is a medical device used by anesthesiologists in the operating room or in intensive care units to capture, measure and display readings on the exhaled carbon dioxide (CO2) of a patient.

There are two methods used by capnography monitors to measure exhaled CO2:

  • Mainstream capnography uses an in-line infrared CO2 sensor connected directly to the airway, between the endotracheal tube and the breathing circuit.
  • Sidestream capnography pulls a sample of the patient’s exhaled gas from the breathing circuit through tubing to the infrared sensor located in a remote monitor.

This blog examines the challenges medical device engineers face when designing next generation sidestream capnography monitors and presents fluidic component solutions to these problems.

 

Fluidic Components Take the Pain Out of Designing Capnography Monitors-White Paper - Parker Precision FluidicsTo learn more about sidestream capnography and how to overcome the challenges faced by design engineers, download the white paper.

 

 

 

 

 

 

Since its introduction in the 1950s, capnography has continued to advance and has rapidly become the standard of care in anesthesia and respiratory therapy. Capnography is non-invasive, easy to use, and offers great promise in the assessment of acute and critically ill patients. The success of capnography depends largely on how well manufacturers underscore its functionality by improving fluidic controls.

 

Fluidic components used in sidestream capnography

Sidestream capnography requires a vacuum source, usually a diaphragm or sampling pump to pull a sample of exhaled air from the patient’s breathing circuit, through a length of tubing, into the remote monitor and across the CO2 sensor. The CO2 sensor requires regular calibration to ensure accuracy and system integrity. This is done through “auto-zeroing” the sensor by switching a solenoid valve in line with the sensors to expose it to ambient air (atmosphere). The sensor auto-zero valve acts to shut off flow from the system to the differential pressure and CO2 sensors in order for the sensors to self-calibrate.

Depending on the complexity of the capnograph, the equipment can also include other solenoid valves that divert the airflow of the pump away from the sensor and perform a purge of the tubing to prevent occlusion.

 

Design challenges

The increased use of capnography monitors combined with the life science industry’s evolving design requirements has resulted in the need for enhanced devices with complex technology and more advanced fluidic controls. Some of the design challenges engineers face include:

Size

Next generation of capnography monitors are smaller and designed for portability. To support this trend, fluidic components should meet these requirements without compromising key performance characteristics such as flow rate, pressure capability, and leak integrity.

Longer life

To address the continued rise in healthcare costs, manufacturers are designing capnographs with longer life expectancy. Consequently, component life is becoming a concern. Engineers must source components capable of operation in excess of 5,000 hours.

Component integration

When developing a system, engineers must coordinate the integration of several sub-components into a functional layout to fit within a reduced device footprint.

Calibration

The need for sidestream CO2 OEM modules drives requirements for remote purging and more advanced sensor technologies which require valves for calibration

Battery power

Portable devices that run on battery power requires lower power consuming components that maintain a high level of performance without loss of functionality.

 

Combining miniaturization, low power, and high performance

Parker Precision Fluids addresses the sidestream capnography monitor design challenges with lightweight valves and pumps that offer reduced power requirements, high performance, and are small enough to fit in the palm of your hand.

Parker’s T2-05 pump combined with miniature X-valves are ideal for sidestream capnography devices and offer:

  • Small size
  • Low power consumption
  • Long life
  • Easy integration

Fluidic Components Take the Pain Out of Designing Capnography Monitors - T2-05 Micro Diaphragm Pump - Parker Precision Fluidics DivisionThe compact T2-05 Micro Diaphragm Pump is uniquely designed to fit in tight spaces where other pumps cannot, minimizing overall device weight. Also, the valve design has been optimized to provide the highest flow rates available with the lowest current draw — only 0.36 Watts is consumed if operated at full voltage. This results in longer battery life and extends the portable range of the system. Other features include:

  • Prolonged life expectancy ranges up to 10,000 rated hours, depending on motor type options.
  • Ideal for portable applications
  • RoHS compliant

Fluidic Components Take the Pain Out of Designing Capnography Monitors - X-Valve Miniature Pneumatic Solenoid Valve - Parker Precision Fluidics DivisionThe X-Valve Miniature Pneumatic Solenoid Valve is a compact, lightweight 8 mm PBT plastic valve commonly used for calibration of the CO2 sensor. The valve is rated for 25 million cycles of operation. Given the infrequency of sensor calibration over its life, the X-Valve exceeds the life requirements of the capnography module. Other features include:

  • Direct PC and side-to-side mounting enables compact and efficient system design
  • Large range of pressure options (6, 30 and 100 psi) to meet various application requirements
  • Light weight valve construction is ideal for portable applications
  • Available low power model (0.5 Watt) for continuous duty applications
  • RoHS compliant

 

Fluidic Components Take the Pain Out of Designing Capnography Monitors - Download White Paper - Parker Precision Fluidics DivisionFor more information on capnography design solutions, read the full white paper. 

 

Fluidic Components Take the Pain Out of Designing Capnography Monitors - Richard Whipple - Parker Precision Fluidics DivisionThis blog was contributed by Richard Whipple, marketing communications manager, Parker Precision Fluidics Division.

 

 
 
 
 
 
Related posts
 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Fluidic Components Take the Pain Out of Designing Capnography Monitors


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha