Hydrogen is commonly used as a fuel gas, reaction gas, and carrier gas in gas chromatography applications. Hydrogen gas generators are a safe, cost-effective alternative to using high pressure hydrogen cylinders in the laboratory. Below we explore the top frequently asked questions about using a hydrogen gas generator.
Yes. The hydrogen generator stores less than 300ml at a low pressure, compared to cylinders that store up to 6500 liters at high pressure. Parker Hydrogen Gas Generators produce only the amount needed by the gas chromatograph (GC) and shut down automatically if a loss in pressure is detected. The generator will also sound an audible alarm and shut down if demand exceeds the generator’s capacity, pressure builds inside the generator, or there is a leak inside the generator.
No. Any hydrogen exhausted from the GC will quickly diffuse in the air. The lower explosive limit (LEL) of hydrogen is 4%, and it is nearly impossible to reach this level in a normal laboratory environment.
No. The amount of hydrogen exhausted in the laboratory is not enough to accumulate and reach the LEL of hydrogen. As mentioned above, the LEL of hydrogen is 4% and it is nearly impossible to reach this level in a normal laboratory environment.
No. Many new GCs come with sensors inside the oven. GC ovens, by design, are not sealed, so buildup does not easily occur. Please check with the manufacturer of your GC.
No. Maintenance is easy and cost-effective. Simply fill the deionized water reservoir weekly/biweekly, or use the auto fill feature. Preventive maintenance (PM) services are available whereby a trained technician can conduct the maintenance.
There is no "one size fits all" solution for sizing a hydrogen generator for carrier use. Please contact your local sales representative for assistance.
Although it is possible, Parker Hannifin does not recommend storing the hydrogen in a reservoir.
Hydrogen gas generators completely eliminate the safety hazards involved with handling high pressure cylinders. Enjoy hassle-free automation with no tanks to change and no downtime.
• Lower pressure is safer.
• Controlled flow maintains safe hydrogen levels.
• Built-in leak sensors and automatic shut down feature.
• On-demand production means smaller storage quantities.
Not at all. Simply fill with deionized water and connect to an electrical supply. Then plumb to your instrument using 1/8” pre-cleaned, refrigerant grade copper or stainless steel piping for carrier gas applications.
Parker Hannifin Hydrogen Generators require deionized water (DI) of 1 megohm purity or better. If DI water is not available, please source a system with adequate capacity and purity for your hydrogen generator.
For more information about the benefits of using Parker Hydrogen Gas Generators, read this case study. You can also visit our website or call (800) 343-4048.
This post was contributed by Gas Generation Technology team.
Is Hydrogen a Safe Gas Chromatography (GC) Carrier Gas? Part 2 of 3
A Simple Guide to How To Use Hydrogen in Flame-based Gas Chromatography Systems Part 3 of 3
Using Hydrogen as a Carrier Gas for GC
The Hidden Costs of Gas Cylinders
Facts You Should Know About Storing Compressed Gas Cylinders
Have a question about Parker products or services? We can help: Contact Us!
Comments for Frequently Asked Questions About Using a Hydrogen Generator
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.