Sealing Shielding

Get Rid of Stick-slip Trouble With These Tips

Stick-slip failure image supplied by Parker Hannifin TechSeal DivisionThe stick-slip phenomenon, also known as the slip-stick phenomenon or simply stick-slip, is "the spontaneous jerking motion that can occur while two objects are sliding over each other." 

In the area of seals and cylinders, Stick-slip is characterized by a distinct stop-start movement of the cylinder, and may be so rapid that it resembles severe vibration, high pitched noise or chatter. Seals are often thought to be the source of the stick-slip, but other components or hardware can create this issue.

Causes for stick-slip

The causes for stick-slip may include
 

  •     Swelling of wear rings or back-up rings
  •     Extreme side-loading
  •     Valve pulsation
  •     Poor fluid lubricity
  •     External sliding surfaces
  •     Seal pressure trapping

 
Tips for stick-slip trouble-shooting

The following are tips for trouble-shooting and solving stick-slip.

 

 
Possible Cause Trouble-shooting Tip
Surface finish out of specification Verify surface is neither too smooth or too rough
Poor fluid lubricity Change fluid or use oil treatments or friction reducers
Binding wear rings Check gland dimensions, check for thermal or chemical swell
Side loading Review cylinder alignment, incorporate adequate bearing area
Seal friction Use material with lower coefficient of friction
Cycle speed Slow movement increases the likelihood of stick-slip
External hardware Review system for harmonic resonance
Valve pulsation Ensure valves are properly sized and adjusted
Temperature High temperature softens seals, expands wear rings, and can cause thermal expansion difference within hardware

Download more frequently asked questions supplied by Parker's Engineered Polymer Division for further help.


More Support Info

You can find more support info, FAQs and our CAD Library on our website at this Literature and Support Link. If you have immediate questions, we offer live chat with one of our application engineers for a number of our divisions - look for the "Chat with an Engineer Button."

Parker Hannifin Live Chat and Ask an Engineer Live Chat button locations

 

 

 

 

 

 

 

 

More articles about seals:

Selecting the Right O-Ring Seal Squeeze Ratio

O-Ring Squeeze - More is Not Always Better

Press-in-Place Seals Solve Problems for Automotive Applications

Have a question about Parker products or services? We can help: Contact Us!

Comments for Get Rid of Stick-slip Trouble With These Tips


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha