Heavy Duty Mobile

Using a Mobile Display as a Dynamic Numeric Keypad Input Device

Control of vehicle speed is important to equipment operators. The ability to accurately set the speed of a conveyor or roller in applications such as road paving or striping, crop sprayers and sugar...
On July 30, 2018

Brazil Terminal Operation Increases Predictive Maintenance Success With Asset Tracking

Located in the Rio Grande do Sul, the Port of Rio Grande is one of the main shipping ports for Brazilian products to the world. Geographically speaking, the Port of Rio Grande is ideally located and...
On June 23, 2018

New Testing Results Give Way to Changing Specifications for Engine OEMs

Diesel and biodiesel engine manufacturers are moving toward electroless nickel plated connectors as part of their fuel system specification. We’ll tell you why.   Meeting the needs of changing...
On June 19, 2018

Reduce Exhaust Leakage in Heavy Duty Engines by 80 Percent with an Air Duct Seal

Increased emission restrictions are requiring engine manufacturers to conform to Euro 6 and Tier IV regulations to reduce exhaust leakage 80% or more. In order to achieve these new standards, engines...
On May 30, 2018

Advances in Engine Air Filtration for Heavy-Duty Trucks

  Reducing routine service intervals is an important objective of any fleet manager. Preventing unscheduled maintenance is even more critical to keeping heavy-duty trucks and equipment operational....
On March 16, 2018

Hydraulic Fan Drives: Efficiency Driven

Looking to improve the efficiency of your construction equipment? Consider a hydraulic fan drive. Compared to mechanically driven fans, hydraulic fan drives provide several advantages. This is proven...
On November 8, 2017

Split Pump IFC on a Wheel Loader: Simply Smarter

For increased simplicity, reliability and energy savings from your wheel loader, consider the proven results of split pump Intelligent Flow Control (IFC) architecture.    Typical wheel...
On November 7, 2017

Variable Flow Open Center Delivers Constant Efficiency

As hydraulic systems on construction equipment continue to evolve, the goal of increasing simplicity, reliability and productivity remains the same. Parker Variable Flow Open-Center (VFO) takes a big...
On November 2, 2017

New Sealing Solution Extends Service Life of Swivel Joints for Mobile Cranes

Mobile cranes perform a wide variety of tasks, typically of the heavy-duty kind. The work they do and the locations at which they operate are frequently exposed to harsh climatic conditions in places...
On October 25, 2017

New Coating Extends Cylinder Life Up to Eight Times Longer

Hydroelectric turbine systems operate in extremely harsh conditions. The corrosive conditions in challenging industrial and outdoor environments, especially in hydro market applications, greatly...
On August 9, 2017

New CPI FFKM Extends Seal Life, Solving Long Time Industry Challenge

For several years, one of the biggest drawbacks of “chemically resistant” FFKMs, or perfluoroelasters, has been their relatively poor compression set resistance. Typically, compounding these materials...
On August 9, 2017

Seal T-Joints Without RTV Silicone

A common problem I hear in the heavy duty industry today is sealing T-Joint applications effectively without the use of RTV Silicone (Room Temperature Vulcanization). Although RTV may be effective...
On July 26, 2017

The Complicated World of SAE Standards

Hydraulic hose construction and performance is covered by various national and international standards including ISO, BSI, SAE, DIN, API and CETOP. Most proprietary hoses conform to one standard...
On July 13, 2017

Making Strides Towards Liner Seal Technology

Parker Engineered Materials Group has developed a wide range of materials for liner seals to meet the demands of the ever increasing temperature requirements in liner seal applications. The new...
On June 29, 2017

Use a Metal Seal for Those High Temperature or High Pressure Situations!

Parker Hannifin Engineered Materials Group has developed a wide variety of metal seals which can be formed or machined. A metal seal is a highly engineered sealing solution which provides...
On June 22, 2017

The Importance of Natural Gas Product Certifications

To stay at the forefront of the competitive transportation markets, fleet managers are turning to alternative fuels that meet the environmental and economic needs of today and in the future.  Natural...
On June 12, 2017

Growing Leaders and Profits

Like many companies, Parker is focused on attracting and developing talented individuals who contribute value to the company over time. What's different about Parker is the landscape of...
On May 8, 2017

Certified Natural Gas Vehicle and Fueling System Products

As we move into the future, the need for transportation is merging with society’s concerns about pollution, climate change, depletion of natural resources and the long-term sustainability of our...
On April 21, 2017

3 Easy Steps to Configure a Wetline Kit for Your Work Truck

When you think of dump trucks, moving floors, oil transfers, lowboys, live floors and roll-offs, your first thought might not be Wetline Kits. Instead, you probably think about the function of each of...
On March 6, 2017

Bringing Tomorrow's Filtration Technology to the Commercial Vehicle Aftermarket

  Parker Racor are original equipment (OE) filtration partners to some of the biggest names in the commercial vehicle business. Now we’re using our world-leading expertise to bring positive change to...
On March 1, 2017