techConnect

How Many Times Can I Reassemble a Hydraulic Fitting?

Wouldn’t it be nice if leak-free connections could last forever? Nice, yes, but not exactly realistic. The good news is that fitting designs have improved significantly over time, making it easier to assemble and reassemble most connections and conduct routine maintenance without increasing the risk of leak paths.
 
There are two common types of fittings, however, that generally rank poor for reusability. When dealing with tapered thread pipe and JIC (Joint Industry Council) or 37° flare fittings, in particular, anyone doing maintenance on a fluid system should always ask: can I reassemble this fitting or does it need to be replaced?  
 

Tapered Thread Pipe Fittings

These torque-sensitive fittings have been around for many years, and if you are working on old equipment, you’re likely to come across tapered thread pipe fittings. They use a thread interface to make a metal-to-metal seal that generally is supplemented with the use of a sealant such as tape or paste. Repeated assembly and disassembly can distort the threads, so it’s important to thoroughly inspect the threads for damage before reusing one of these fittings.

It would not be unwise to replace the male fitting any time you disassemble a tapered thread fitting. But, if you’re being frugal and want to try to reuse a fitting, here’s a quick way to determine if your re-connection will be leak-free:

  1. Are more than six threads engaging? In other words, has the sixth thread from the end has gone into the female port? (Figure 1)
  2. Does it take more than two turns of sealant tape to make a seal?

Proper NPT thread engagement for hydraulic fitting

                                Figure 1: Fitting at sixth thread - this is the maximum depth.

If you answered yes to either of these questions, you should definitely replace the fitting. Why? Because six or more threads indicate that the threads are already damaged, and more than two turns of sealant tape is likely to crack the female port. Also, be careful with the use of sealants on pipe threads. If some of the sealant gets into the hydraulic system, it can clog and cause other problems.


JIC 37° Flare Fittings

Tubing connections are made with cone, flare and O-ring connectors, and one of the most often used is the JIC 37° flare fitting, especially in high-pressure applications. Though industry generally accepts that JIC 37° flare fittings are reusable, they may not always be reliable when reused.  In fact, the JIC 37° flare fitting tops the Most Questionable list for reassembly.

JIC 37° flare fittings have a cone on the female adapter and a flare on the male adapter. The cone and flare seat against one another to create a complete mechanical seal between the male and female fitting. But, each time the metal-to-metal seal is made, the cone and flare collapse more and more, causing the material to be cold-worked.  The result is a harder metal, which makes each subsequent assembly more difficult and problematic on two fronts: a leaking seal and reduced flow due to excessive nose collapse.

How can you determine if a JIC 37° flare connection is reusable or not?  Measure the amount of nose collapse and make certain that the hole diameter reduction is no more than 10 percent (Figure 2). For example, if the original hole diameter on a cone female adapter was 0.5 inches and it has been reduced to 0.45 inches or smaller, the fitting should be replaced. For a quick check, a pin gauge works well.

Measure the nose collapse of a 37 degree flared fitting to see if it is reusable - fitting reusability tips from Parker Hannifin
Figure 2: To determine if a JIC connection is reusable, measure the amount of nose collapse and make certain that the hole diameter reduction is no more than 10 percent. 


Do you have any tips or stories about reassembling fittings that you would like to share? If so, please send them along!  As always, if you have questions or comments, please post them and I’ll respond if warranted. If you want to talk to me directly, I can be reached at Parker Tube Fittings Division, 614.279.7070 or via email.

Did you find this post helpful? Subscribe to TFD techConnect posts by email. TFD techConnect is a technically-focused monthly blog written for engineers specifically around motion and control engineering challenges.

Download a print-friendly version of How Many Times Can I Reassemble a Hydraulic Fitting.

Do you also want to receive new product announcements and technology updates from Parker Tube Fittings Division? Subscribe today and stay informed

 

Rob King Parker Tube Fittings Division Engineering Manager

 

Rob King, Engineering Supervisor, Parker Tube Fittings Division

 

 

 

​Additional helpful content:

Turn vs. Torque? How Making the Right Choice Keeps Your Hydraulic Fitting Connections Leak-Free 

10 Things Not to Do When Your Hydraulic Fitting Leaks 

Four Easy Steps to Identify Hydraulic Threads

Sizing Tube to Maximize Hydraulic System Efficiency

State-of-the-Art Metallurgical Lab Helps Drive Product Safety and Reliability for Industrial Tube Fittings and Adapters 

Categories
Recent Posts by Author

Proper Assembly Steps for 37° Flare Fittings Using the Flats Method

Properly assembling your fitting connections help to ensure that your systems install and stay leak-free. This is why we have started a series of assembly posts/videos featuring the proper assembly of...

Proper Assembly Steps for Parallel Thread Adjustable Style Port End Fittings

Properly assembling your fitting connections help to ensure that your systems install and stay leak-free. This is why we have started a series of assembly posts/videos featuring the proper assembly of...

Assembly Instructions for Ensuring Leak-Free O-ring Face Seal Fittings

No matter what type of port, tube or hose ends your fittings have, it's important to know and use the proper assembly and installation steps. Today we are talking about O-ring Face Seal (ORFS)...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for How Many Times Can I Reassemble a Hydraulic Fitting?

rajkumar yadav
That's why all electric machines demand is increasing.leakage is one of the critical issue.
good knowledgeable material.g
Kevin Zemko
Thank you for this insightful article.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha