Process Control

How Parker's THM Analyzer Helps to Improve Safety of Drinking Water

How Parker's THM analyser helps to improve safety of drinking water, Parker Hannifin, Instrumentation Products Division, Water Plant - Image courtesy of Anglian WaterMost public drinking water supplies in the developed world are treated with a disinfectant chemical such as chlorine, to eliminate any harmful organisms and to preserve the quality and safety of the water throughout the distribution network. However, reaction between the disinfectant and naturally occurring organic compounds in the water can form disinfection by-products (DBPs) which may, in themselves, pose a risk to human health. The use of chemical disinfectants is therefore a balance between protecting against microbial and the potential health risks of DBPs.

Fig. 1. Drinking water supply companies can now perform near real-time monitoring of THM levels. Image courtesy of Anglian Water.

The most common DBPs are chemical compounds known as trihalomethanes (THMs). The four main THM compounds are:

  • chloroform
  • bromoform
  • bromodichloromethane
  • dibromochloromethane

Learn more about this product, case studies and research at our THM Analyzer page 

Drinking water standards

To reduce the potential risk of DBPs to public health, the World Health Organisation (WHO) sets guidelines for maximum levels of THMs in drinking water:

  • 300 µg/l of chloroform
  • 100 µg/l of bromoform
  • 60 µg/l of bromodichloromethane
  • 100 µg/l of dibromochloromethane

Many governments set drinking water standards mandating even lower levels of THMs. In the USA, for example, the Environmental Protection Agency (EPA) stipulates that drinking water should contain less than 80 parts per billion (80 µg/l) of THMs. Within the EU, the standard is 100 µg/l, although in some countries this figure is lower – in Germany and the Netherlands, for example, it is 50 µg/l. In England and Wales, the Drinking Water Inspectorate (DWI) enforces the EU standard of 100 µg/l for total THM concentration; failure to comply with this standard is a criminal offence and renders the water company liable to prosecution.

Current THM analysis procedures

Most water supply companies currently rely on laboratories for THM analysis. This involves sending samples to the laboratory and waiting for the results – a procedure that can take from days to weeks, depending on the laboratories’ workload and location. As well as being expensive, this approach means that the analysis data cannot be used for real-time process control – which can lead to over-use of disinfectant or in the worst case could result in contaminated water being consumed before the laboratory results were available.

Parker’s THM analyzer – features and benefits

Parker’s new portable THM analyzer overcomes all these issues, providing water supply companies with a compact and easy-to-use means of performing accurate, near real-time THM analysis on-site. The analyzer comprises an integrated purge-and-trap system connected to a compact gas chromatograph column and a very sensitive surface acoustic wave (SAW) detector.

  • Real-time measurement and analysis

It provides a completely self-contained solution for real-time measurement and analysis of THM concentration levels, down to as low as 1 part per billion (1 µg/l) for each individual species of THMs. The analyzer can measure chloroform, bromoform, bromodichloromethane and dibromochloromethane to within 10% of certified laboratory results.

How Parker's THM analyser helps to improve safety of drinking water, Parker Hannifin, Instrumentation Products Division, Parker's THM Analyser

Fig. 2 Parker’s THM analyzer provides water companies with a compact and easy to use water quality monitoring system.

  • No sample preparation

A key advantage of Parker’s THM analyzer is that it does not require sample preparation – a tedious task traditionally associated with gas chromatography. The analyzer’s purge-and-trap function automates the measurement process to the extent that the user simply connects the collected water sample to the analyzer’s sparging system and pushes the ‘start’ button. All sample purging, TTHM component separation and data analysis operations are then performed entirely automatically. Individual species and total THM information is displayed on a front panel LCD touchscreen and on the associated laptop computer, as analysis progresses. The entire process takes less than 30 minutes.

After each analysis run, the analyzer’s PC-based software displays the processed chromatogram showing the compound peaks and corresponding chromatography data. Analytical results, including measured concentration and detailed chromatography data, as well as optional data such as carrier gas pressure, GC column and pre-concentrator temperature profiles, are automatically archived for more in-depth data analysis and review.

  • Long term cost benefits

The long term cost benefits of Parker’s THM analyzer are significant. By implementing near real-time control over treatment processes on-site, water companies can reduce laboratory analysis costs and achieve much more efficient use of disinfectants. The analyzer’s annual running costs are also very low – the only consumables are high purity helium and concentrated standard solutions for verification runs.

  • Complete turnkey package

Parker supplies the THM analyzer as a complete turnkey package. The high purity pressure regulators and precision control valves for its helium carrier gas system are manufactured by our Veriflo Division.

How Parker's THM analyser helps to improve safety of drinking water, Parker Hannifin, Instrumentation Products Division, Graham JohnsonGraham Johnson, product manager – downstream applications – EMEA, Instrumentation Products Division Europe

 

 

 

 

Related Content:

Case Study - Anglian Water
Product detail and where to buy
Catalog
Improving Performance of Stream Switching Systems Under Low Air Conditions
Using Hydrogen as a Carrier Gas for GC

In-House Gas Generation Is Ideal for LC-MS


 

Have a question about Parker products or services? We can help: Contact Us!

Comments for How Parker's THM Analyzer Helps to Improve Safety of Drinking Water

Jane
Parker's THM Analyzer is a huge help for people whose taking public water, good job for this new discovery. Most public drinking water are treated with chemicals, with this we can monitor quality and safety of the water we are drinking. Im looking forward for more news about this
Linda G. Dickinson
This is such a good read. And very useful information. Thanks for sharing this.

Water Filter

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha