Pneumatics

How to Achieve Safe Motion Control in ATEX Environments

How to achieve safe motion control in ATEX environments - Oil and Gas Plant - Parker Hannifin Pneumatic Division EuropeMachinery and moving equipment is a vital element in all modern automated industries, but what happens when the atmosphere in the working environment is potentially explosive? 

All motion control creates friction and, with sufficient magnitude, could provide a source of heat or ignition. A simple switch could be viewed as a potential ignition source. Therefore, machinery and equipment OEMs must use motion control components that are tested, rated, and certified for safe use. 

 

Explosive atmospheres in the workplace can be caused by flammable gases, mists or vapours, or by combustible dust. If there is enough of the substance, mixed with air, then all it needs is a source of ignition to cause an explosion.

 

The ATEX Directive
 

ATEX (derived from the French term ATmospheres EXplosive) is the name commonly given to the European directives for controlling equipment designated for operation in explosive atmospheres. 

The directives state that employers have a duty to eliminate or control the risks from explosive atmospheres in the workplace. Areas, where hazardous explosive atmospheres may occur, must be classified into zones. The classification is given to a particular zone, and its size and location, depends on the likelihood of an explosive atmosphere occurring and its persistence if it does. 

 
Zones and classifications
 
Three zones are classifying the presence of a potentially explosive atmosphere:
  • Present continuously or for long periods (Gas Zone 0)

  • Likely to occur in normal operation occasionally, typically between 10-1000 hours per annum (Gas Zone 1)

  • Not likely to occur in normal operation, but if it does occur it will persist for a period typically less than 10 hours a year (Gas Zone 2)

How to achieve safe motion control in ATEX environments - ATEX Zones - Parker Hannifin Pneumatic Division Europe

Equipment and protective systems earmarked for deployment in these zones should meet the Equipment and Protective Systems Intended for Use in Potentially Explosive Atmospheres Regulations 1996 (EPS). 

EPS implements the ATEX directive within the UK, regulating the supply of products intended for operation in these hazardous environments. However, EPS also requires the supplier to provide instructions for the safe operation of the products. 

To help with equipment classification, two classification groups have been established:

  • Group 1 equipment is intended for use in underground mines and surface installations of such mines likely to be endangered by flammable vapours and/or dust.

  • Group 2 equipment is intended for use in other places exposed to explosive atmospheres. 

The level of protection offered in each group can be classified into normal, high and very high categories.
 

Specifying Motion Control Solutions
 

How to achieve safe motion control in ATEX environments - Chemical Plant - Parker Hannifin Pneumatic Division Europe

There are many examples of potentially explosive atmospheres across the industry in sectors such as oil and gas, power generation, chemical, pharmaceutical, wood processing, and paint spraying.

 

Deploying motion control solutions in these industries means using a supplier with a thorough understanding of ATEX and products that can be operated safely and with confidence.

 

This means ensuring their products meet essential safety requirements and undergo appropriate conformity procedures. As a result, any component that contains or constitutes a potential ignition source requires preventative measures to be incorporated into its design or installation to prevent it from initiating an explosion.

How to achieve safe motion control in ATEX environments - ATEX logo - Parker Hannifin Pneumatic Division Europe

The components are tested and certified by a 'third-party' certification body (known as a Notified Body) although some components can be self-certified for use in less hazardous explosive atmospheres. 

Once certified, the equipment is marked by the 'EX' symbol to identify it as such, making it easier for you to identify products fit for their intended purpose and that adequate information is supplied to ensure its safe use.

A broad choice backed by application expertise is vital to end customers seeking a safe and effective solution to motion control in potentially explosive environments.

 

Learn more

Parker offers many components suitable for use in ATEX environments, such as cylinders (including rodless types), valves, filters/absorbers, air motors, logic controllers, pushbuttons, solenoids, coils, limit switches, and sensors. Download our catalogue to find out more.

 
 
How to achieve safe motion control in ATEX environments - Franck Roussillon - Parker Hannifin Pneumatic Division EuropeArticle contributed by Franck Roussillon, European product manager for actuators, Pneumatic Division Europe, Parker Hannifin Corporation
 
 
 
 
 

Related content

Know Your Pneumatics: Safety & Understanding Rod Locking Cylinders
Know Your Pneumatics: Specifying Cylinders for Size Restricted Spaces
3 Ways to Prevent Costly Downtime in Compressed Air Installations

Have a question about Parker products or services? We can help: Contact Us!

Comments for How to Achieve Safe Motion Control in ATEX Environments

Boom Lift
Thanks for sharing…

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha