Sealing Shielding

How to Apply Conductive Foil Masking Tape Before Painting

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Parker Chomerics CHO-MASK IIEMI (electromagnetic interference) is the disruption of the operation of an electronic device when it is near an electromagnetic field in the radio frequency spectrum that is caused by another electronic device. When used with a conductive EMI gasket, conductive foil tapes with a polyester paint masking provides a conductive, non-corroding surface on painted metal electronic enclosures that forms and effective EMI shielding solution.

But sometimes, applying conductive EMI foil masking tapes can be tricky and quite the hassle. Luckily, we’ve come up with five easy steps to make applying conductive tape easy and worry-free.

 

Step One: Prepare your surface

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Step One: Prepare Your SurfaceTo ensure maximum adhesion of your conductive foil tape with peel-off mask, remove all surface oils and dust. In large volume applications, proceed through your normal automated cabinet cleaning procedures. In small volume applications, clean cabinet flanges thoroughly with a cloth dampened with an industrial cleaner (acetone, toluene, or isopropyl alcohol).

Be sure to wear rubber gloves, because some cleaning agents tend to be nasty chemicals, and you do not want them to get on your skin. It is important to avoid contact with or handling of the adhesive on the back of the tape. Oils from the hand will affect adhesion. If oxidation or rust is present, abrade surface with sandpaper to expose clean metal before cleaning.

 

Step Two: Remove the release liner from the tape

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Step Two: Remove the Release Liner from the Tape

Still wearing your rubber gloves, peel away the release liner of the conductive tape and apply the tape to cabinet flanges, being careful to avoid wrinkles. Extend the tape beyond the corners and cut away excess. This prevents residual stress in the foil from lifting tape at ends. Run your finger along the mask to provide initial adhesion.

 

Step Three: Trim off excess

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Step Three: Trim Off Excess

The excess tape in each corner should now be trimmed, and it is not necessary to overlap the tape in the corners. It is recommended that a gap be left between the vertical and horizontal strips. The gap should measure about .080 in. (2.0 mm) wide (which is equivalent to the recessed edge of the tape). Later, when paint is applied to the cabinet, this gap will be filled and serve to edge seal the tape ends.

 

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Trim Off ExcessThen, using a precise cutting tool, cut about a .080 in. (2.0 mm) piece of the mask layer on each strip and remove. This will further ensure edge sealing when the cabinet is painted.

 

Step Four: Smooth over your surfaces

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Smooth Out Surfaces

Smooth over the surface of the conductive foil tape with a small rubber roller. Touch down the exposed tinned copper edges until they are flat and even. Note: Only moderate pressure is required (about 5 psi).

 

Step Five: Time to paint

Now your cabinet is ready for normal phosphatizing and painting. Follow the manufacturer’s instructions for paint application and curing. Note: Recommended paint thickness, including primer, is 4 mils (0.1 mm) or more.

 

Step Six: Remove your conductive masking tape

How to Apply Conductive Foil Masking Tape Before Painting, Chomerics Division, Remove Masking Tape

When the cabinet has reached room temperature, remove the mask of the conductive foil tape at a 180° angle from the foil tape leaving a clean, conductive grounding surface. The mask is easily removed at room temperature, with or without baking.

 

Looking for the perfect conductive foil tape with a peel-off mask? Check out Parker Chomerics CHO-MASK® II EMI Foil Tape now. CHO-MASK II tape provides
effective shielding performance and grounding points within the painted enclosure, and can accommodate a wide range of enclosure finishing processes, including powder coating.

Jarrod Cohen

 

 

This blog was contributed by Jarrod Cohen, marketing communications manager, Parker Chomerics Division.

 

 

 

Related content:

Calling All Puzzle Experts: Why Package Level EMI Shielding Makes Sense

Design Decisions Relating to EMC Shielding

Chomerics Division Honored with Boeing Award 

Categories
Recent Posts by Author

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...

Managing EMI and Lightning Strike Protection in Today’s Aircraft

Composite materials have been replacing metal structures throughout the aircraft industry primarily to save weight, improve fuel economy and reduce costs.  But the lack of electrical conductivity in...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for How to Apply Conductive Foil Masking Tape Before Painting


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha