Fluid Gas Handling

How to Dispense Small Volume Liquids With Precision

How to Dispense Small Volume Liquids - Smart Syringe Pump - Precision Fluidics Division - Parker HannifinThe trend to decrease volumes of liquids required for sample testing has led fluidics device OEMs to focus on new engineering solutions for better handling precision dispensing.

This is a complex problem: a small volume of liquid limits the velocity of the liquid being moved by stepper motor driven syringe pumps and does not create enough momentum and deceleration to overcome the surface tension that retains the droplet at the end of the probe.

An improvement over stepper motor driven pumps

To solve this problem, the Precision Fluidics Division at Parker developed the Smart Syringe Pump, capable of higher acceleration, running speed and deceleration than stepper motor driven pumps.

OEMs rely on two methods of precision dispensing --

  • air displacement
  • positive displacement

However, air displacement devices lack the precision of their positive displacement counterparts. They also generally require disposable tips, which add to the cost per sample and increase the amount of waste for disposal. Positive displacement devices utilize syringe and piston pumps, providing the best accuracy and precision. Typically they deliver larger volumes well with good ejection of liquid from the probe tip. However, in ranges around 10µL and lower stepper motor driven syringe and piston pumps begin to struggle because of the difficulty of completely clearing droplets off the probe.

Improving small volume performance

The strategy to improve small volume performance with these positive displacement systems has been to use a small volume syringe barrel or liquid head, the portion of the pump that is actually pumping liquid. Unfortunately, this leads to issues with successfully priming the pump, as bubbles tend to adhere to the small passageways inside the liquid head. Using small volumes of liquid limits the velocity of the liquid being moved and prevents enough momentum and deceleration to overcome the surface tension that adheres the droplet to the end of the probe, therefore, the accuracy and precision of the measurement is compromised as the reproducibility of the droplet clearing is compromised.

The reliable solution Parker developed, the Smart Syringe Pump, calls for using a larger volume syringe barrel or liquid head, along with changing the equipment design from using a stepper motor to a servo motor. Servo motors typically are capable of much higher acceleration, running speed and deceleration. This makes it possible to obtain sufficient flow velocity behind the dispense to reliably eject the droplet, while still having enough resolution to precisely and accurately deliver the right amount of low volume fluid to the desired site.

While the servo motor design is an important element behind a good solution, liquid volumes play a role as well. Typically a minimum 500µL or larger volume is required;  volumes of 1000µL are preferred. These larger volumes allow for enough fluid velocity behind the dispense, assuming the acceleration, running speed and deceleration of the motor is rapid enough to clear the droplet with high levels of precision.

 

View and Download the Smart Syringe Brochure.

How to dispense small volume liquids accurately - Introducing the Parker Smart Syringe Pump

 

 

 

 

 

 

 

 

 

 

 

Attending MDM West Show?

Parker representatives will be on-hand at the Medical Device and Manufacturing West Show (MDMWest),  February 6-8, in Anaheim, CA, at booth #2601.

 

How to dispense small volume liquids accurately - Don Mcneil Product managerArticle contributed by Donald S. McNeil, Sr. Product Manager, Parker Hannifin Corporation, Precision Fluidics Division

 

 

 

 

Other related articles by this contributor on this subject include:

Why Servo Motors Top Stepper Motors for Precision Liquid Dispensing

New Smart Syringe Pump Offers Greater Precision

High-Resolution, High-Speed Syringe Pumps Reduce Diagnostic Costs

Parker Announces Syringe Pump for Smarter, More Efficient Assays

Categories
Recent Posts by Author

Optimize Hydraulic Systems with Top Fluid & Gas Handling Blogs of 2017

As we look back on 2017, increased demand contributed to technology advancements and higher productivity across a range of industries including oil and gas, power generation, life...

Tapping Into Water Quality at a Public Facility

Having potable water at our fingertips is something many of us take for granted. For those in facility management, this can be a significant challenge. Water pressure, temperature,...

Dental Office Potable Water Case Study - Choosing the Right Connectors

Potable water systems, whether in water filtration, beverage dispensing, life science, bottling or semiconductor are much more than the sum of their individual parts. A thorough analysis of...
Comments

Comments for How to Dispense Small Volume Liquids With Precision


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha