Compressed Air Gas Treatment

How to Improve Coordinate Measuring Machine Reliability

Improving Reliability of Coordinate Measuring Machines - Parker HannifinA Coordinate Measuring Machine (CMM) is a highly sensitive instrument, used mainly for quality control applications, that locates point coordinates on three dimensional structures. A CMM measures parts down to a fraction of an inch and must be properly maintained and protected to ensure that accurate measurements are achieved. A CMM contains many delicate air bearings on which the measuring arm floats. Oil, moisture and particulate matter are commonly found in compressed air and can be extremely harmful to a CMM, often resulting in “drag” or resistance in the air bearings leading to hysteresis. These contaminants can also cause condensation and rust, resulting in poor machine performance and inaccurate measurements. Correcting the damage caused by contaminated compressed air is costly and requires production downtime.

The best way to protect a CMM from oil, moisture and particulate matter contained in compressed air is to install an air dryer/coalescing filter combination upstream of the CMM. Several different types of air dryers are available including membrane dryers, refrigerated dryers, chemical dryers and desiccant dryers. Choosing the Right Compressed Air Dryer for Your Application

Improving Reliability of Coordinate Measurement Machines - Membrane Air Dryers - Parker HannifinA membrane air dryer with a high efficiency coalescing filter is a smart choice for CMM applications. Membrane air dryers use specially formulated membrane microtubes that are selectively permeable to water vapor. The microtubes provide an excellent medium for producing dry air from standard compressed air. As the compressed air travels along the length of the membrane, water vapor diffuses through the membrane, producing clean, dry compressed air at the outlet. A small fraction of the dry air is then directed along the outside surface of the membrane to sweep the moisture-laden air away from the membrane. The illustration above shows how a membrane dryer operates.

Membrane dryers can reduce the dew point of compressed air to as low as -40°F/°C, and are designed with no moving parts and no requirement for electricity. They operate with very little noise output - just a small amount of purge air is emitted through small exhaust ports. Membrane dryers require minimal maintenance and are inherently explosion proof. They are ideal for water sensitive applications, remote areas, explosive environments, sub-freezing environments, and applications requiring a consistent dew point.

Improving Reliability of Coordinate Measuring Machines - Parker HannifinRead this marketing application for more information on membrane air dryers for coordinate measuring machines.

 

 

 

 

Related posts:

Facts You Need to Know About Drying Compressed Air

Compressed Air and Gas Technology Blog Team Member - Parker HannifinThis post was contributed by Judy Silva, Compressed Air and Gas Technology Blog Team Member, Parker Hannifin.

 

Categories
Recent Posts by Author

Air Preparation for High-Precision Manufacturing

Today's global manufacturing environment is uncompromising. To remain at the forefront, suppliers must meet a multitude of demands - shortest lead time, highest accuracy, zero rejects,...

Why Should I Change My Compressed Air Filter Element?

Often nicknamed manufacturing’s fourth utility alongside electricity, gas and water, compressed air is used in over 90% of the world’s manufacturing facilities. As with the other utilities, it is a...

How Oil Vapour in Ambient Air Affects Compressed Air Quality

Many companies, including those in the food and beverage, pharmaceutical, cosmetics, manufacturing and electronics industries, recognize the negative effects on quality created by oil contact with...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for How to Improve Coordinate Measuring Machine Reliability

jayesh chand
You have covered all the points from what is Coordinate Measuring Machine to how to improve Coordinate Measuring machine Reliability, very useful and excellent short content easy to understand not complex.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha