Fluid Gas Handling

How to Improve Steam Hose Safety in Petrochemical Refineries

How to Improve Steam Hose Safety in Petrochemical Refineries | Petrochemical facility | Industrial Hose Division | Parker HannifinDue to its size and complexity, a petrochemical refinery offers many potential safety hazards, one of which is rubber steam hose that blends into the scenery and presents many hidden-in-plain-sight risks. If a steam hose assembly fails, a potentially lethal hazard may be unleashed unexpectedly, quickly, and with overwhelming force upon defenseless workers.

Here is a simple, successful approach to converting a petrochemical refinery over to using crimped steam hose assemblies for a safer work environment.

 

Five steps to improving steam hose safety

  1. Get the “lay of the land”

The petrochemical refinery management team is usually not composed of “hose people.” So you (or they) may not be aware that steam service is one of the most rigorous applications for rubber hose, as heat is the arch-enemy of most synthetic rubber compounds. Large volumes of refinery steam are conveyed in fixed metal piping, with flexible hoses attached to allow the steam to be more easily deployed. The steam provides wet heat to lubricate and increase flow in applications such as tank and vessel cleaning, and to keep process equipment running smoothly and efficiently. When in service, the heat and moisture of the steam expand the rubber, and after use, the hose dries out and contracts. Each cycle jeopardizes the security of fittings installed with bolt-on clamps.

  1. Determine what type of fittings are currently installed on your steam hoses

  • Traditionally, rubber steam hose assemblies have been fabricated using re-attachable fittings installed using external bolt-on clamps.

  • More recently, rubber steam hose assemblies have been fabricated using hydraulic-style permanent crimp fittings installed using a high-pressure hydraulic crimper.

  1. Be aware of the significant differences in the two types of steam hose assemblies

Hose assemblies using traditional re-attachable fittings

  • How to Improve Steam Hose Safety in Petrochemical Refineries | steam hose clamped | Industrial Hose Division | Parker Hannifinthe components (hose, fittings, clamps) are usually produced by different manufacturers.

  • are not designed or tested as a bona fide system.

  • are attached by clamps that do not have contact with the entire circumference of the hose.

  • are susceptible to leakage at the hose/fitting interface.

  • because the hose is constantly expanding and contracting, the fittings/clamps need frequent maintenance.

  • require a visual inspection, tightening of the clamps using proper torque settings, etc.

  • clamps are heavy and bulky and present a tripping/bumping hazard.

  • over time, the clamps can no longer be tightened as much as needed, undermining the efficiency and safety of the hose assembly and requiring premature rework or replacement.

Hose assemblies using permanent crimped-on fittings

  • How to Improve Steam Hose Safety in Petrochemical Refineries | steam hose crimped | Industrial Hose Division | Parker Hannifincomponents (hose and fittings only) may or may not be produced by the same manufacturer (if different, the components may not have been tested/qualified as a bona fide system).
  • never need adjusting; they withstand the expansion and contraction of the hose during the service life of the hose.
  • provide equal gripping power around the entire circumference of the hose.
  • are not susceptible to leakage at the hose/fitting interface.
  • are streamlined and do not present a tripping/bumping hazard.
  1. Evaluate your plant

Perform a plant assessment or survey to determine

  • which type of steam hose assembly is deployed (there might be a mixture)?

  • is there a hose assembly visual tagging system? Or better yet, a hose assembly computer database such as the Parker Tracking System (PTS)?

  • if routine maintenance is being performed?

  • are clamp bolts being inspected/tightened? If so, are they being tightened according to the proper torque/spec?

  • what is the time/cost of maintenance?

  • what is the cost of steam loss/system inefficiency?

  • what is our steam hose safety record?

  1. Ask yourself: when is “Good Safety” ever good enough?

Never! Luckily, you know this and can take immediate action.

Finally, consider that Parker Hannifin pioneered steam hose crimped assembly technology and that we have validated steam hose assemblies with the same engineered care and precision used to qualify high-pressure hydraulic hose assemblies.

Take a look at our steam hose product offering to find the most suitable steam hose for your facility, and to locate the closest Parker hose distributor in your area to help you and your team develop a steam hose safety plan.

 

Dennis Daniel | Industrial Hose Division | Parker HannifinArticle contributed by Dennis Daniel, technical services manager for Hose Products Division, Parker Hannifin.

 

 

 

 

Related content

Working Together: Safety and Maintenance Tips to Ensure Hydraulic Hose Success

Best Practices for Hose Installation and Routing Rules

Top 8 Reasons Hydraulic Hoses Fail

How to Extend the Life of Your Surface Mining Hose

What is an Onsite Container?

Four Ways to Use Hose in a Wet Method Silica Dust Suppression System

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for How to Improve Steam Hose Safety in Petrochemical Refineries


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha