Providing miniature size, light weight and low power coupled with integration capabilities for pump and motor units in medical devices provide an ideal solution for design engineers. They are now able to design a more portable device that fits all the performance their customers demand into a package that takes up less space. The next challenge is to implement.
The four most common methods for controlling the motor/pump speed of Iron Core Permanent Magnet Direct Current (PMDC) motors (often called “brush motor,”), Coreless DC brush motors, and Brushless Direct Current (BLDC) motors are discussed in our recent post Mini Subcomponents for Medical Devices Make a Big Design Difference.
The following detailed descriptions will assist with properly integrating the motor speed control with whichever option is chosen. Although external PWM control is preferable when speed control is required, OEMs must decide the best control style for their application. The following detailed descriptions will assist with properly integrating the motor speed control with whichever option is chosen.
This technique often referred to as “2-wire” PWM, is one of the simplest methods for controlling pump speed in a device. The basic requirement from the customer device is a PWM signal, often generated from a microcontroller and a power transistor. The input voltage to the motor is turned on and off at a high frequency so that the average power to the motor is reduced. The following image illustrates an example of a “low side” PWM driver where the ground to the motor is being switched by the “customer PCBA” to reduce the speed.
For brush motors, 2-wire PWM is the most common method for control, and very effective. It is similarly effective with BLDC motors; however, it does present some limitations. Many BLDC motors have an internal controller that must maintain a minimum voltage to operate properly. When applying a PWM cycle to the input voltage, it is also reducing the effective voltage to the controller electronics; this limits the available speed control range. Using an external PWM control can provide more range in this situation.
This is the recommended method for controlling the speed of a BLDC diaphragm pump when possible. This method provides the most dynamic control of a pump, and can also simplify the engineer’s electrical circuit in some cases because only a low current transistor is required for the switching signal.
Most diaphragm pumps with external PWM require an “open-drain” or “open-collector” circuit on the OEM engineer’s device PCBA to provide the PWM signal. The BLDC motors have an internal pull-up resistor so the open-drain or open-collector circuits will actively bring this voltage to ground for the low part of the PWM signal. The following illustrations show examples of recommended circuits.
Open-Drain/Open-Collector Circuit Examples
In some applications, a PWM signal is not feasible or is not preferred by the system designer. Many BLDC motors offer an external analog DC signal input. In this case, the motor is provided a direct voltage to operate, but a separate low current 0 to 5 Vdc input (yellow wire) controls the speed of the pump.
The actual control voltage range may vary depending on the motor; however, the concept is the same: a 0 Vdc signal would disable the motor, 5 Vdc would represent full speed, and the range between 0 and 5Vdc would adjust the speed of the pump.
Many BLDC motors also have the ability to output a tachometer signal so the engineer’s device can monitor the actual pump speed. The signal is a digital pulse that can be used to determine the speed of the pump.
This is useful in applications where the pump will need to operate very slowly; with this information, the device controller could increase the speed if the pump begins to stall (that is, pump speed approaches zero). It also provides additional safety and/or diagnostics feedback for confirming proper system function.
The speed control signal to the motor can reduce or increase flow; however, it is not a direct linear relationship. For example, at a fixed 50% PWM signal, the speed of the pump will be reduced but not by exactly 50%. Also, as the load on the pump changes, the speed of the pump will also change, even while the PWM signal is fixed.
The maximum motor speed can be reduced by the pump configuration or the pressure/vacuum load on the pump in the application. Torque and speed have a linear relationship; when more torque is required to turn the pump, the motor will slow down.
Pump motors may be damaged if the pump stalls. When the motor’s rotor is locked in this position and power is being supplied to the motor, heat will increase and can damage the internal controller. When using speed control to reduce speed, a motor stall is more likely and should be closely monitored.
It is recommended that system designers implement a safety current limit or fuse to power the pump. This can help prevent damage to the pump motor and system if a stall event occurs.
Using any speed control method reduces the effective power to the motor. If the speed is reduced during restart, the starting torque will be reduced. Designers must ensure that the pump is capable of restarting under all conditions (such as pressure load and environmental temperature) when the speed is reduced.
When using a PWM speed control method, the recommended frequency is 20 kHz. Frequencies lower than 20 kHz may create an audible buzzing sound as the audible frequency range for humans is 20 Hz to 20 kHz. Using higher frequencies can limit the control range because of transistor rise and fall time; it is possible to switch so quickly that a low or high duty cycle signal appears as 0% or 100% because the transistor cannot switch fast enough. Also, with some motors and control circuits, PWM frequencies greater than 20 kHz can reduce efficiency.
In an era when engineering staffs are shrinking as much and as quickly as the instruments they design, it helps to work with multi-faceted and experienced component suppliers. For example, Parker is a pump supplier that builds most of its own brushless motors. This expertise in both motor and pump design speeds customization and prototype production, which can help shrink engineering timeframes and costs.
Article contributed by Jamie Campbell, applications engineer – Precision Fluidics Division, Parker Hannifin Co. and was originally published in DesignNews February 2016.
Other posts related to medical devices:
Mini Subcomponents for Medical Devices Make a Big Design Difference
How to Dispense Small Volume Liquids With Precision
Have a question about Parker products or services? We can help: Contact Us!
Comments for How to Integrate Motor Speed Control for Pump Motors in Medical Devices
Thanks!
Please contact us by email if you have any further questions at ppfinfo@parker.com
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.